TI-RTOS Drivers  tidrivers_cc32xx_2_16_01_13
Data Structures | Macros | Typedefs | Enumerations | Functions
PWM.h File Reference

Detailed Description

PWM driver interface.

============================================================================

The PWM header file should be included in an application as follows:

#include <ti/drivers/PWM.h>

Operation

The PWM driver in TI-RTOS facilitates the generation of Pulse Width Modulated signals via simple and portable APIs. A device's PWM peripheral pins must be configured before initializing the PWM driver. The application initializes the PWM driver by calling PWM_init(). PWM instances must be opened by calling PWM_open() while passing in a PWM index and a parameters data structure.

The driver APIs serve as an interface to a typical TI-RTOS application. The specific peripheral implementations are responsible of creating all SYS/BIOS specific primitives to allow for thread-safe operation.

When a PWM instance is opened, the period, units of the duty, and polarity can be set. The maximum period supported is device dependent; refer to the implementation specific documentation for values. A PWM instance can be configured to interpret the duty as one of three units: PWM_DUTY_COUNTS: The duty is in PWM timer ticks. PWM_DUTY_SCALAR: The duty is an integer scaled to the period where 0 corresponds to a duty of 0% and 65535 corresponds to 100% duty. PWM_DUTY_TIME: The duty is specified in microseconds. The driver calculates the appropriate amount of PWM timer ticks.

The polarity is used to set the output during the active duty portion of the period; it can be set to produce low output or a high output when active.

By default PWM output is set to a duty of 0. It is the applications responsability to set the duty for each PWM output used.

Opening the driver

PWM_Handle handle;
PWM_Params params;
PWM_Params_init(&params);
params.period = 20000; // Period in microseconds
params.dutyMode = PWM_DUTY_TIME; // Duty specified in microseconds
handle = PWM_open(Board_PWM0, &params);
if (handle == NULL) {
System_printf("PWM did not open");
}
// Update PWM to have a duty of 3000 microseconds
PWM_setDuty(handle, 3000);

Implementation

This module serves as the main interface for TI-RTOS applications. Its purpose is to redirect the module APIs to specific peripheral implementations specified by a pointer to a PWM_FxnTable.

The PWM driver interface module is joined (at link time) to a NULL-terminated array of PWM_Config data structures named PWM_config. PWM_config is implemented in the application with each entry being an instance of a PWM peripheral. Each entry in PWM_config contains a:

Calling Context

Function Hwi Swi Task Main
PWM_Params_init Y Y Y Y
PWM_close Y Y Y Y
PWM_control Y Y Y Y
PWM_getPeriodCounts Y Y Y Y
PWM_getPeriodMicroSecs Y Y Y Y
PWM_init Y Y Y Y
PWM_open Y Y Y Y
PWM_setDuty Y Y Y Y
  • Hwi: API is callable from Hwi context.
  • Swi: API is callable from Swi context.
  • Task: API is callable from a Task thread.
  • Main: API is callable from main().

Instrumentation

The PWM driver interface produces log statements if instrumentation is enabled.

Diagnostics Mask Log details
Diags_USER1 basic operations performed
Diags_USER2 detailed operations performed

#include <stdint.h>
#include <stddef.h>
Include dependency graph for PWM.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  PWM_Params
 PWM Parameters. More...
 
struct  PWM_FxnTable
 The definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation. More...
 
struct  PWM_Config
 PWM Global configuration. More...
 

Macros

#define PWM_CMD_RESERVED   32
 
#define PWM_STATUS_RESERVED   -32
 
#define PWM_STATUS_SUCCESS   0
 Successful status code returned by PWM_control(). More...
 
#define PWM_STATUS_ERROR   -1
 Generic error status code returned by PWM_control(). More...
 
#define PWM_STATUS_UNDEFINEDCMD   -2
 An error status code returned by PWM_control() for undefined command codes. More...
 

Typedefs

typedef struct PWM_ConfigPWM_Handle
 A handle that is returned from a PWM_open() call. More...
 
typedef enum PWM_DutyMode PWM_DutyMode
 Definitions for various units for specifying the PWM duty. More...
 
typedef enum PWM_Polarity PWM_Polarity
 Definitions for various PWM output polarity. More...
 
typedef struct PWM_Params PWM_Params
 PWM Parameters. More...
 
typedef void(* PWM_CloseFxn) (PWM_Handle handle)
 A function pointer to a driver specific implementation of PWM_close(). More...
 
typedef int(* PWM_ControlFxn) (PWM_Handle handle, unsigned int cmd, void *arg)
 A function pointer to a driver specific implementation of PWM_control(). More...
 
typedef unsigned int(* PWM_GetPeriodCountsFxn) (PWM_Handle handle)
 A function pointer to a driver specific implementation of PWM_getPeriodCounts(). More...
 
typedef unsigned int(* PWM_GetPeriodMicroSecsFxn) (PWM_Handle handle)
 A function pointer to a driver specific implementation of PWM_getPeriodMicroSecs(). More...
 
typedef void(* PWM_InitFxn) (PWM_Handle handle)
 A function pointer to a driver specific implementation of PWM_init(). More...
 
typedef PWM_Handle(* PWM_OpenFxn) (PWM_Handle handle, PWM_Params *params)
 A function pointer to a driver specific implementation of PWM_open(). More...
 
typedef void(* PWM_SetDutyFxn) (PWM_Handle handle, uint32_t duty)
 A function pointer to a driver specific implementation of PWM_setDuty(). More...
 
typedef struct PWM_FxnTable PWM_FxnTable
 The definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation. More...
 
typedef struct PWM_Config PWM_Config
 PWM Global configuration. More...
 

Enumerations

enum  PWM_DutyMode {
  PWM_DUTY_COUNTS = 0,
  PWM_DUTY_SCALAR,
  PWM_DUTY_TIME
}
 Definitions for various units for specifying the PWM duty. More...
 
enum  PWM_Polarity {
  PWM_POL_ACTIVE_HIGH = 0,
  PWM_POL_ACTIVE_LOW = 1
}
 Definitions for various PWM output polarity. More...
 

Functions

void PWM_close (PWM_Handle handle)
 Function to close a PWM peripheral specified by the PWM handle. More...
 
int PWM_control (PWM_Handle handle, unsigned int cmd, void *arg)
 Function performs implementation specific features on a given PWM_Handle. More...
 
unsigned int PWM_getPeriodCounts (PWM_Handle handle)
 Get the PWM handle period in timer counts. More...
 
unsigned int PWM_getPeriodMicroSecs (PWM_Handle handle)
 Get the PWM handle period in microseconds. More...
 
void PWM_init (void)
 This function initializes the PWM module. More...
 
PWM_Handle PWM_open (unsigned int index, PWM_Params *params)
 This function opens a given PWM peripheral. More...
 
void PWM_Params_init (PWM_Params *params)
 Function to initialize the PWM_Params struct to its defaults. More...
 
void PWM_setDuty (PWM_Handle handle, uint32_t duty)
 Function to set the duty cycle of the specified PWM handle. More...
 

Typedef Documentation

typedef struct PWM_Config* PWM_Handle

A handle that is returned from a PWM_open() call.

typedef enum PWM_DutyMode PWM_DutyMode

Definitions for various units for specifying the PWM duty.

typedef enum PWM_Polarity PWM_Polarity

Definitions for various PWM output polarity.

typedef struct PWM_Params PWM_Params

PWM Parameters.

PWM Parameters are used to with the PWM_open() call. Default values for these parameters are set using PWM_Params_init().

See also
PWM_Params_init()
typedef void(* PWM_CloseFxn) (PWM_Handle handle)

A function pointer to a driver specific implementation of PWM_close().

typedef int(* PWM_ControlFxn) (PWM_Handle handle, unsigned int cmd, void *arg)

A function pointer to a driver specific implementation of PWM_control().

typedef unsigned int(* PWM_GetPeriodCountsFxn) (PWM_Handle handle)

A function pointer to a driver specific implementation of PWM_getPeriodCounts().

typedef unsigned int(* PWM_GetPeriodMicroSecsFxn) (PWM_Handle handle)

A function pointer to a driver specific implementation of PWM_getPeriodMicroSecs().

typedef void(* PWM_InitFxn) (PWM_Handle handle)

A function pointer to a driver specific implementation of PWM_init().

typedef PWM_Handle(* PWM_OpenFxn) (PWM_Handle handle, PWM_Params *params)

A function pointer to a driver specific implementation of PWM_open().

typedef void(* PWM_SetDutyFxn) (PWM_Handle handle, uint32_t duty)

A function pointer to a driver specific implementation of PWM_setDuty().

typedef struct PWM_FxnTable PWM_FxnTable

The definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation.

typedef struct PWM_Config PWM_Config

PWM Global configuration.

The PWM_Config structure contains a set of pointers used to characterize the PWM driver implementation.

This structure needs to be defined before calling PWM_init() and it must not be changed thereafter.

See also
PWM_init()

Enumeration Type Documentation

Definitions for various units for specifying the PWM duty.

Enumerator
PWM_DUTY_COUNTS 
PWM_DUTY_SCALAR 
PWM_DUTY_TIME 

Definitions for various PWM output polarity.

Enumerator
PWM_POL_ACTIVE_HIGH 

PWM output active high

PWM_POL_ACTIVE_LOW 

PWM output active low

Function Documentation

void PWM_close ( PWM_Handle  handle)

Function to close a PWM peripheral specified by the PWM handle.

Precondition
PWM_open() has to be called first.
Parameters
handleA PWM handle returned from PWM_open()
See also
PWM_open()
int PWM_control ( PWM_Handle  handle,
unsigned int  cmd,
void *  arg 
)

Function performs implementation specific features on a given PWM_Handle.

Commands for PWM_control can originate from PWM.h or from implementation specific PWM*.h (PWMCC32XX.h, PWMTiva.h, etc.. ) files. While commands from PWM.h are API portable across driver implementations, not all implementations may support all these commands. Conversely, commands from driver implementation specific PWM*.h files add unique driver capabilities but are not API portable across all PWM driver implementations.

Commands supported by PWM.h follow a PWM_CMD_<cmd> naming convention.
Commands supported by PWM*.h follow a PWM*_CMD_<cmd> naming convention.
Each control command defines arg differently. The types of arg are documented with each command.

See PWM_control command codes for command codes.

See PWM_control return status codes for status codes.

Precondition
PWM_open() has to be called first.
Parameters
handleA PWM handle returned from PWM_open()
cmdPWM.h or PWM*.h commands.
argAn optional R/W (read/write) command argument accompanied with cmd
Returns
Implementation specific return codes. Negative values indicate unsuccessful operations.
See also
PWM_open()
unsigned int PWM_getPeriodCounts ( PWM_Handle  handle)

Get the PWM handle period in timer counts.

Parameters
handleA PWM_Handle
Returns
Period in timer counts.
See also
PWM_open
unsigned int PWM_getPeriodMicroSecs ( PWM_Handle  handle)

Get the PWM handle period in microseconds.

Parameters
handleA PWM_Handle
Returns
Period in microseconds.
See also
PWM_open
void PWM_init ( void  )

This function initializes the PWM module.

Precondition
The PWM_config structure must exist and be persistent before this function can be called. This function must also be called before any other PWM driver APIs. This function call does not modify any peripheral registers.
PWM_Handle PWM_open ( unsigned int  index,
PWM_Params params 
)

This function opens a given PWM peripheral.

Precondition
PWM controller has been initialized using PWM_init()
Parameters
indexLogical peripheral number for the PWM indexed into the PWM_config table
paramsPointer to an parameter block, if NULL it will use default values. All the fields in this structure are RO (read-only).
Returns
A PWM_Handle on success or a NULL on an error or if it has been opened already.
See also
PWM_init()
PWM_close()
void PWM_Params_init ( PWM_Params params)

Function to initialize the PWM_Params struct to its defaults.

Parameters
paramsAn pointer to PWM_Params structure for initialization

Defaults values are: period = 10000 (microseconds) dutyMode = PWM_DUTY_TIME polarity = PWM_POL_ACTIVE_HIGH

void PWM_setDuty ( PWM_Handle  handle,
uint32_t  duty 
)

Function to set the duty cycle of the specified PWM handle.

Parameters
handleA PWM_Handle
dutyPWM duty cycle.
See also
PWM_open
Copyright 2016, Texas Instruments Incorporated