IPC API
3.23.01.03
|
ti | |
grcm | |
RcmClient.h | Remote Command Message Client Module. An RcmClient is used for sending messages to an RcmServer for processing |
RcmServer.h | Remote Command Message Server Module. An RcmServer processes inbound messages received from an RcmClient |
RcmTypes.h | Remote Command Message Types |
ipc | |
mm | |
MmRpc.h | Multi-Media derived Remote Procedure Call |
MmServiceMgr.h | Multi-Media Service Manager |
MmType.h | Specific types to support the MmRpc and MmServiceMgr modules |
tests | |
gatempapp_rsc_table_vayu_dsp.h | |
GateMPAppCommon.h | |
Mx.h | Example of a host-side module which uses MmRpc to invoke functions on a remote processor |
MxServer.h | Example of a slave-side module which implements the Mx module functions. The functions in MxServer are invoked remotely by the Mx module running on the host processor |
GateMP.h | Multiple processor gate that provides local and remote context protection |
HeapBufMP.h | Multi-processor fixed-size buffer heap implementation |
HeapMemMP.h | Multi-processor variable size buffer heap implementation |
HeapMultiBufMP.h | Multiple fixed size buffer heap implementation |
Ipc.h | Ipc Manager |
ListMP.h | Multiple processor shared memory list |
MessageQ.h | MessageQ Manager |
MultiProc.h | Processor ID Manager |
NameServer.h | NameServer Manager |
Notify.h | Notification manager for IPC |
SharedRegion.h | Shared memory manager and address translator |