IRES_EDMA3CHAN_Obj Struct Reference
[IRES EDMA3 Protocol]

IRES_EDMA3CHAN_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource. More...

#include <ires_edma3Chan.h>

Collaboration diagram for IRES_EDMA3CHAN_Obj:
Collaboration graph
[legend]

Data Fields

IRES_Obj ires
IRES_EDMA3CHAN_PaRamStructshadowPaRams
unsigned int * assignedPaRamAddresses
short * assignedPaRamIndices
short * assignedTccIndices
short assignedNumPaRams
short assignedNumTccs
short assignedQdmaChannelIndex
short assignedEdmaChannelIndex
unsigned int esrBitMaskL
unsigned int esrBitMaskH
unsigned int iprBitMaskL
unsigned int iprBitMaskH

Detailed Description

IRES_EDMA3CHAN_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource.


Field Documentation

Actual programmed shadow paRam entries

Physical Addresses of assigned paRams

Assigned paRam Indices

Assigned Tcc Indices

Number of assigned paRams

Number of assigned tccs

Assigned qdma channel. Could be IRES_EDMA3CHAN_CHAN_NONE if no QDMA channel was requested

Assigned edma channel. Could be IRES_EDMA3CHAN_CHAN_NONE if no EDMA channel was requested

Event set register bit mask to trigger edma channel if requested.

Interrupt pending register bit mask to pend on transfer completion.


The documentation for this struct was generated from the following file:

Copyright 2010, Texas Instruments Incorporated