IRES_EDMA3CHAN_EDMA3DraeRegister Struct Reference
[IRES EDMA3 Protocol]

IRES_EDMA3CHAN_EDMA3DraeRegister defines the Region Enable register part of the EDMA3 CC Register Layer defined below. More...

#include <ires_edma3Chan.h>

Data Fields

volatile unsigned int DRAE
volatile unsigned int DRAEH

Detailed Description

IRES_EDMA3CHAN_EDMA3DraeRegister defines the Region Enable register part of the EDMA3 CC Register Layer defined below.


Field Documentation


The documentation for this struct was generated from the following file:

Copyright 2010, Texas Instruments Incorporated