DMAN3
Data Structures |
struct | DMAN3_Params |
| The module configuration structure for DMAN3 implementation. It is set at design time by the system integrator to ensure optimal sharing of DMA resources for the execution environment. More...
|
Defines |
#define | DMAN3_GTNAME "ti.sdo.fc.dman3" |
#define | DMAN3_MAXGROUPS 20 |
Typedefs |
typedef Bool(* | DMAN3_ScratchAllocFxn )(IALG_Handle alg, Int mutexId, IALG_MemRec *memTab, Int numRecs) |
| Function prototype for allocating IDMA3 Object's env from shared scratch memory. Algorithms might specify a particular IDMA3 protocol that provides custom DMA services. This protocol might require extra memory for the IDMA3 object's environment. DMAN3_ScratchAllocFxn might be used to allocate this memory. If this is NULL, then the env will be allocated from persistent memory.
|
typedef Void(* | DMAN3_ScratchFreeFxn )(Int mutexId, Void *addr, Uns size) |
| Function prototype for freeing IDMA3 Object's env from shared scratch memory. If this is NULL then env will be freed from persistent memory.
|
Functions |
Int | DMAN3_grantDmaChannels (Int groupId, IALG_Handle algHandle[], IDMA3_Fxns *dmaFxns[], Int numAlgs) |
| Add one or several algorithms to the DMA Manager. The DMA Manager will grant DMA resources to the algorithms as a result. This function is called when initializing XDAIS algorithm instances.
|
Void | DMAN3_exit (Void) |
| Finalization method of the DMAN module.
|
Int | DMAN3_createChannels (Int groupId, IDMA3_ChannelRec dmaTab[], Int numChans) |
| Allocate and initialize memory for one or several channel handles.
|
Void | DMAN3_init (Void) |
| Initialization method of the DMAN3 module. DMAN3_init() uses externally configured and provided DMAN3_PARAMS to initialize DMAN3 resources (QDMA channel map, memory heap...).
|
Int | DMAN3_releaseDmaChannels (IALG_Handle algHandle[], IDMA3_Fxns *dmaFxns[], Int numAlgs) |
| Remove logical channel resources from one or several algorithm instances.
|
Int | DMAN3_freeChannels (IDMA3_Handle channelTab[], Int numChans) |
| Free memory for array of channel handles.
|
Variables |
DMAN3_Params | DMAN3_PARAMS |
| Default module configuration structure (defined in dman3.c).
|
Uns | ti_sdo_fc_dman3_DMAN3_numQdmaGroup [20+1] |
| Array containing the number of Qdma channels that will be assigned to the algorithm groups for sharing.
|
Defines: DMAN3 Status Codes |
|
#define | DMAN3_SOK 0 |
#define | DMAN3_EOUTOFMEMORY -1 |
#define | DMAN3_EFAIL -2 |
#define | DMAN3_EFREE -3 |
#define | DMAN3_EOUTOFTCCS -4 |
#define | DMAN3_EOUTOFPARAMS -5 |
#define | DMAN3_ETCCCONFIG -6 |
#define | DMAN3_EPARAMCONFIG -7 |
Detailed Description
DMAN3 is an application interface to the 3rd generation DMA Manager. It provides routines for granting and reclaiming DMA resources used by algorithms or other non-algorithm users. This module is used by frameworks or applications which have XDAIS algorithms that implement the IDMA3 interface.
Define Documentation
#define DMAN3_GTNAME "ti.sdo.fc.dman3" |
Name to identify the GT module
#define DMAN3_MAXGROUPS 20 |
Maximum number of groups for sharing TCCs and parameter RAM.
DMAN3 Status Code: Successful.
#define DMAN3_EOUTOFMEMORY -1 |
DMAN3 Status Code: Failed to allocate memory for the handle.
DMAN3 Status Code: Unspecified error.
DMAN3 Status Code: Failed to free memory.
#define DMAN3_EOUTOFTCCS -4 |
DMAN3 Status Code: Insufficient number of TCCs available to create channels.
#define DMAN3_EOUTOFPARAMS -5 |
DMAN3 Status Code: Insufficient number of PaRams available to create channels.
#define DMAN3_ETCCCONFIG -6 |
DMAN3 Status Code: The number of TCCs configured for the scratchId is not enough to create the channels. This error can only be returned if allowUnshared
is set to FALSE.
#define DMAN3_EPARAMCONFIG -7 |
DMAN3 Status Code: The number of PaRams configured for the scratchId is not enough to create the channels. This error can only be returned if allowUnshared
is set to FALSE.
Typedef Documentation
Function prototype for allocating IDMA3 Object's env from shared scratch memory. Algorithms might specify a particular IDMA3 protocol that provides custom DMA services. This protocol might require extra memory for the IDMA3 object's environment. DMAN3_ScratchAllocFxn might be used to allocate this memory. If this is NULL, then the env will be allocated from persistent memory.
Function prototype for freeing IDMA3 Object's env from shared scratch memory. If this is NULL then env will be freed from persistent memory.
Function Documentation
Add one or several algorithms to the DMA Manager. The DMA Manager will grant DMA resources to the algorithms as a result. This function is called when initializing XDAIS algorithm instances.
- Parameters:
-
[in] | groupId | Group number for sharing TCCs and PaRAMs. Channels created with the same group number in a previous or subsequent call to this function will share the same TCCs and PaRam, as the channels created in this call, so they must be used simultaneously. The channels created in this function call, will not share TCCs and PaRam with eachother, even though they use the same group Id. When granting DMA resources for several algorithms (i.e. when numAlgs is greater than 1) these algorithms do not share TCCs and PaRAMs. If two algorithms can share TCCs and PaRAMs, two calls to DMAN3_grantDmaChannels() are needed. |
[in] | algHandle[] | Array of algorithm handles. |
[in] | dmaFxns[] | Array of IDMA3 Interfaces associated with each algorithm handle. |
[in] | numAlgs | Number of algorithms in algHandle array. |
- Return values:
-
| DMAN3_SOK | Success. |
| DMAN3_EOUTOFMEMORY | Failed to allocate logical handle. |
| DMAN3_EFAIL | Failed to initialize handle or dmaFxns dmaInit() failed. |
| DMAN3_EOUTOFTCCS | Not enough TCCs available for channels. |
| DMAN3_EOUTOFPARAMS | Not enough PaRams available for channels. |
- Precondition:
- groupId < DMAN3_MAXGROUPS.
-
Valid IALG_Handle.
-
Valid IDMA3_Fxns pointer.
-
IALG_Handle->fxns->implementationId == IDMA3_Fxns->implementationId
-
numberOfChannels returned by algorithm's dmaGetChannelCnt and dmaGetChannels is not greater than total number of Tccs allocated.
- Postcondition:
- DMAN3_SOK on successful allocation of IDMA3 logical handles.
Finalization method of the DMAN module.
Int DMAN3_createChannels |
( |
Int |
groupId, |
|
|
IDMA3_ChannelRec |
dmaTab[], |
|
|
Int |
numChans | |
|
) |
| | |
Allocate and initialize memory for one or several channel handles.
- Parameters:
-
[in] | groupId | Group number for sharing TCCs and PaRAMs. Channels created with the same group number in a previous or subsequent call to this function will share the same TCCs and PaRam, as the channels created in this call, so they must be used simultaneously. The channels created in this function call, will not share TCCs and PaRam with eachother, even though they use the same group Id. If two channels can share TCCs and PaRAMS then two calls to DMAN3_createChannels() are needed. |
[in] | dmaTab | Array of IDMA3 channel resource descriptors containing the parameters of the requested channels. |
[in] | numChans | Number of entries in dmaTab (ie, number of channels to create). |
[out] | dmaTab | On success assign valid and initialized IDMA3 logical DMA handle and environment (env, envSize) fields. |
- Return values:
-
| DMAN3_SOK | Success. |
| DMAN3_EOUTOFMEMORY | Failed to allocate logical handle. |
| DMAN3_EFAIL | Failed to initialize handle or dmaFxns dmaInit() failed. |
| DMAN3_EOUTOFTCCS | Not enough TCCs available for channels. |
| DMAN3_EOUTOFPARAMS | Not enough PaRams available for channels. |
- Precondition:
- Valid dmaTab structure.
-
numChans >= 0.
-
groupId < DMAN3_MAXGROUPS.
- Postcondition:
- On success, each handle in dmaTab[] will be set to a valid IDMA3_Handle. The 'env' field of the IDMA3_Handle will be set to newly allocated memory whose size is determined by the IDMA3_InitFxns passed in the dmaTab entry. On failure, the handle of each dmaTab[] entry will be NULL.
Initialization method of the DMAN3 module. DMAN3_init() uses externally configured and provided DMAN3_PARAMS to initialize DMAN3 resources (QDMA channel map, memory heap...).
- Precondition:
- DMAN3_PARAMS must be initialized
Remove logical channel resources from one or several algorithm instances.
- Parameters:
-
[in] | algHandle[] | Array of algorithm handles. |
[in] | dmaFxns[] | Array of IDMA3 Interfaces associated with the algorithm handles. |
[in] | numAlgs | Number of algorithm handles in algHandle[]. |
- Precondition:
- algHandle is an array of valid IALG_Handle
-
dmaFxns is an array of valid IDMA3_Fxns pointer
-
IALG_Handle->fxns->implementationId == IDMA2_Fxns->implementationId
-
numberOfChannels returned by algorithm's dmaGetChannelCnt and dmaGetChannels is >= 0 and not greater than number of Tccs allocated
- Postcondition:
- Handle and environment memory and allocated resources are freed/released.
Int DMAN3_freeChannels |
( |
IDMA3_Handle |
channelTab[], |
|
|
Int |
numChans | |
|
) |
| | |
Free memory for array of channel handles.
- Parameters:
-
[in] | channelTab | Array of IDMA3 handles representing logical dma channel state. |
[in] | numChans | Number of entries in channelTab (ie, number of channels to free). |
- Return values:
-
- Precondition:
numChans
>= 0.
-
Valid IDMA3 logical channel handles or numChans == 0.
- Postcondition:
- 'handle' and 'env' memory freed for each channel.
Variable Documentation
Default module configuration structure (defined in dman3.c).
Array containing the number of Qdma channels that will be assigned to the algorithm groups for sharing.