Framework Components Application Programming Interface (API)  fc-v02
Data Fields
_EdmaMgr_ConfigLarge Struct Reference

Configuration for a large channel. More...

#include <edmamgr.h>

Collaboration diagram for _EdmaMgr_ConfigLarge:
Collaboration graph

Data Fields

int32_t max_num_lines
 

Detailed Description

Configuration for a large channel.

Field Documentation

int32_t _EdmaMgr_ConfigLarge::max_num_lines

< Maximum number of lines which may be transfered by the channel.


The documentation for this struct was generated from the following file:
Copyright 2015, Texas Instruments Incorporated