Framework Components Application Programming Interface (API)  fc-v02
Functions | Macros | Data Structures | Typedefs
EdmaMgr

EDMA3 Functional library. More...

Functions

int32_t EdmaMgr_init (int32_t proc_id, void *edma3_config)
 Initialize EdmaMgr. More...
 
EdmaMgr_Handle EdmaMgr_alloc (int32_t max_linked_transfers)
 Allocate an EdmaMgr channel. More...
 
int32_t EdmaMgr_getSizesLarge (EdmaMgr_ConfigLarge *cfg, IALG_MemRec memTab[])
 Get buffer requirements for a large channel. More...
 
EdmaMgr_Handle EdmaMgr_allocLarge (EdmaMgr_ConfigLarge *cfg, IALG_MemRec memTab[])
 Allocate an EdmaMgr channel for "Large" 1D2D or 2D1D transfers which have a pitch outside the range [-32768,32768]. More...
 
int32_t EdmaMgr_free (EdmaMgr_Handle h)
 Frees an EdmaMgr channel. More...
 
void EdmaMgr_wait (EdmaMgr_Handle h)
 Wait for transfers to complete. More...
 
int32_t EdmaMgr_copy1D1D (EdmaMgr_Handle h, void *restrict src, void *restrict dst, int32_t num_bytes)
 Perform a single 1D->1D transfer. More...
 
int32_t EdmaMgr_copy1D2D (EdmaMgr_Handle h, void *restrict src, void *restrict dst, int32_t num_bytes, int32_t num_lines, int32_t pitch)
 Perform a 1D->2D transfer. More...
 
int32_t EdmaMgr_copy2D1D (EdmaMgr_Handle h, void *restrict src, void *restrict dst, int32_t num_bytes, int32_t num_lines, int32_t pitch)
 Perform a 2D->1D transfer. More...
 
int32_t EdmaMgr_copy2D2D (EdmaMgr_Handle h, void *restrict src, void *restrict dst, int32_t num_bytes, int32_t num_lines, int32_t pitch)
 Perform a 2D->2D transfer of buffers with the same pitch. More...
 
int32_t EdmaMgr_copy2D2DSep (EdmaMgr_Handle h, void *restrict src, void *restrict dst, int32_t num_bytes, int32_t num_lines, int32_t src_pitch, int32_t dst_pitch)
 Perform a 2D->2D transfer of buffers with different pitches. More...
 
int32_t EdmaMgr_copy1D1DLinked (EdmaMgr_Handle h, void *restrict src[], void *restrict dst[], int32_t num_bytes[], int32_t num_transfers)
 Perform a group of linked 1D->1D transfers. More...
 
int32_t EdmaMgr_copy1D2DLinked (EdmaMgr_Handle h, void *restrict src[], void *restrict dst[], int32_t num_bytes[], int32_t num_lines[], int32_t pitch[], int32_t num_transfers)
 Perform a group of linked 1D->2D transfers. More...
 
int32_t EdmaMgr_copy2D1DLinked (EdmaMgr_Handle h, void *restrict src[], void *restrict dst[], int32_t num_bytes[], int32_t num_lines[], int32_t pitch[], int32_t num_transfers)
 Perform a group of linked 2D->1D transfers. More...
 
int32_t EdmaMgr_copy2D2DLinked (EdmaMgr_Handle h, void *restrict src[], void *restrict dst[], int32_t num_bytes[], int32_t num_lines[], int32_t pitch[], int32_t num_transfers)
 Perform a group of linked 2D->2D transfers. More...
 
int32_t EdmaMgr_copy2D2DSepLinked (EdmaMgr_Handle h, void *restrict src[], void *restrict dst[], int32_t num_bytes[], int32_t num_lines[], int32_t src_pitch[], int32_t dst_pitch[], int32_t num_transfers)
 Perform a group of linked 2D->2D transfers with different pitches. More...
 
int32_t EdmaMgr_copy1D2DLarge (EdmaMgr_Handle h, void *restrict src, void *restrict dst, int32_t num_bytes, int32_t num_lines, int32_t pitch)
 Perform a 1D->2D large transfer. More...
 
int32_t EdmaMgr_copy2D1DLarge (EdmaMgr_Handle h, void *restrict src, void *restrict dst, int32_t num_bytes, int32_t num_lines, int32_t pitch)
 Perform a 2D->1D large transfer. More...
 
int32_t EdmaMgr_copyFast (EdmaMgr_Handle h, void *restrict src, void *restrict dst)
 Perform a fast copy. This API inherits the transfer configuration of a previous transfer and only modifies the src and dst addresses. More...
 
int32_t EdmaMgr_copyLinkedFast (EdmaMgr_Handle h, void *restrict src[], void *restrict dst[], int32_t num_transfers)
 Perform a linked fast copy. This API inherits the transfer configuration of a previous transfer and only modifies the src and dst addresses. More...
 

Macros

#define EdmaMgr_SUCCESS   0
 
#define EdmaMgr_ERROR_INVARG   -1
 
#define EdmaMgr_ERROR_INVCFG   -2
 
#define EdmaMgr_ERROR_RMANINIT   -3
 
#define EdmaMgr_ERROR_INVHANDLE   -4
 
#define EdmaMgr_ERROR_FREE   -5
 
#define EdmaMgr_MAX_NUM_MEMRECS_LARGE   1
 

Data Structures

struct  _EdmaMgr_ConfigLarge
 Configuration for a large channel. More...
 

Typedefs

typedef void * EdmaMgr_Handle
 Handle to an EdmaMgr instance. More...
 
typedef struct _EdmaMgr_ConfigLarge EdmaMgr_ConfigLarge
 Configuration for a large channel. More...
 

Detailed Description

EDMA3 Functional library.

Function Documentation

int32_t EdmaMgr_init ( int32_t  proc_id,
void *  edma3_config 
)

Initialize EdmaMgr.

Parameters
[in]proc_idProcessor ID. This ID is used to index into the EDMA3_InstanceInitConfig array pointed to by the ti_sdo_fc_edmamgr_edma3RegionConfig variable.
[in]edma3_configOptional edma3_config which will override the configuration which is pointed to by ti_sdo_fc_edmamgr_edma3RegionConfig.
Return values
EdmaMgr_SUCCESSSuccess
EdmaMgr_ERROR_INVARGFailure, Invalid Argument
EdmaMgr_ERROR_INVCFGFailure, Invalid Configuration
EdmaMgr_ERROR_RMANINITFailure, RMAN initialization
Remarks
edma3_config may be NULL to accept default values.
The FC product includes an example (ex23_edmamgr) which demonstrates how to set up a ti_sdo_fc_edma3RegionConfig variable.
EdmaMgr_Handle EdmaMgr_alloc ( int32_t  max_linked_transfers)

Allocate an EdmaMgr channel.

Parameters
[in]max_linked_transfersMaximum linked transfers
Return values
NULLFailure to allocate the channel
non-NULLSuccess
Precondition
EdmaMgr_init() must have first been called.
int32_t EdmaMgr_getSizesLarge ( EdmaMgr_ConfigLarge cfg,
IALG_MemRec  memTab[] 
)

Get buffer requirements for a large channel.

Parameters
[in]cfgConfiguration for a large channel.
[out]memTabBuffer requirements for a large channel.
Return values
EdmaMgr_SUCCESSSuccess
EdmaMgr_ERROR_INVCFGFailure, Invalid Configuration
Remarks
These buffers must be provided to EdmaMgr_allocLarge() along with the corresponding EdmaMgr_ConfigLarge structure.
EdmaMgr_Handle EdmaMgr_allocLarge ( EdmaMgr_ConfigLarge cfg,
IALG_MemRec  memTab[] 
)

Allocate an EdmaMgr channel for "Large" 1D2D or 2D1D transfers which have a pitch outside the range [-32768,32768].

Parameters
[in]cfgConfiguration for a large channel.
[in]memTabBuffer requirements along with allocated buffers for a large channel.
Return values
NULLFailure to allocate the channel
non-NULLSuccess
Precondition
EdmaMgr_init() must have first been called.
EdmaMgr_getSizesLarge() must have been called and buffers allocated satisfying the requirements in memTab.
int32_t EdmaMgr_free ( EdmaMgr_Handle  h)

Frees an EdmaMgr channel.

Parameters
[in]hHandle returned from EdmaMgr_alloc().
Return values
EdmaMgr_SUCCESSSuccess
EdmaMgr_ERROR_INVHANDLEFailure, Invalid Handle
EdmaMgr_ERROR_FREEFailure to free a resource
Precondition
h must be a handle successfully returned from EdmaMgr_alloc().
void EdmaMgr_wait ( EdmaMgr_Handle  h)

Wait for transfers to complete.

Parameters
[in]hHandle returned from EdmaMgr_alloc().
Precondition
h must be a handle successfully returned from EdmaMgr_alloc().
Remarks
This function waits for all transfers on a specific channel to complete. It is a blocking call.
int32_t EdmaMgr_copy1D1D ( EdmaMgr_Handle  h,
void *restrict  src,
void *restrict  dst,
int32_t  num_bytes 
)

Perform a single 1D->1D transfer.

Parameters
[in]hHandle returned from EdmaMgr_alloc().
[in]srcSource address
[in]dstDestination address
[in]num_bytesNumber of bytes to transfer
Precondition
h must be a handle successfully returned from EdmaMgr_alloc().
Remarks
Perform a single 1D->1D transfer of num_bytes bytes from src address to dst address.
See also
EdmaMgr_copy1D1DLinked
int32_t EdmaMgr_copy1D2D ( EdmaMgr_Handle  h,
void *restrict  src,
void *restrict  dst,
int32_t  num_bytes,
int32_t  num_lines,
int32_t  pitch 
)

Perform a 1D->2D transfer.

Parameters
[in]hHandle returned from EdmaMgr_alloc().
[in]srcSource address
[in]dstDestination address
[in]num_bytesNumber of bytes to transfer
[in]num_linesNumber of lines
[in]pitchPitch
Precondition
h must be a handle successfully returned from EdmaMgr_alloc().
Remarks
Perform a 1D->2D transfer of num_bytes bytes. The source is one dimensional, and the destination is two dimensional.
After every line of num_bytes is transferred, the src address is incremented by num_bytes and the dst address is incremented by pitch bytes.
int32_t EdmaMgr_copy2D1D ( EdmaMgr_Handle  h,
void *restrict  src,
void *restrict  dst,
int32_t  num_bytes,
int32_t  num_lines,
int32_t  pitch 
)

Perform a 2D->1D transfer.

Parameters
[in]hHandle returned from EdmaMgr_alloc().
[in]srcSource address
[in]dstDestination address
[in]num_bytesNumber of bytes to transfer
[in]num_linesNumber of lines
[in]pitchPitch
Precondition
h must be a handle successfully returned from EdmaMgr_alloc().
Remarks
Perform a 2D->1D transfer of num_bytes bytes. The source is two dimensional, and the destination is one dimensional.
After every line of num_bytes is transferred, the src address is incremented by pitch and the dst address is incremented by num_bytes bytes.
int32_t EdmaMgr_copy2D2D ( EdmaMgr_Handle  h,
void *restrict  src,
void *restrict  dst,
int32_t  num_bytes,
int32_t  num_lines,
int32_t  pitch 
)

Perform a 2D->2D transfer of buffers with the same pitch.

Parameters
[in]hHandle returned from EdmaMgr_alloc().
[in]srcSource address
[in]dstDestination address
[in]num_bytesNumber of bytes to transfer
[in]num_linesNumber of lines
[in]pitchPitch
Precondition
h must be a handle successfully returned from EdmaMgr_alloc().
Remarks
Perform a 2D->2D transfer of num_bytes bytes. The source and destination are two dimensional.
After every line of num_bytes is transferred, the src address and dst address is incremented by pitch bytes.
int32_t EdmaMgr_copy2D2DSep ( EdmaMgr_Handle  h,
void *restrict  src,
void *restrict  dst,
int32_t  num_bytes,
int32_t  num_lines,
int32_t  src_pitch,
int32_t  dst_pitch 
)

Perform a 2D->2D transfer of buffers with different pitches.

Parameters
[in]hHandle returned from EdmaMgr_alloc().
[in]srcSource address
[in]dstDestination address
[in]num_bytesNumber of bytes to transfer
[in]num_linesNumber of lines
[in]src_pitchSource buffer pitch
[in]dst_pitchDestination buffer pitch
Precondition
h must be a handle successfully returned from EdmaMgr_alloc().
Remarks
Perform a 2D->2D transfer of num_bytes bytes. The source and destination are two dimensional.
After every line of num_bytes is transferred, the src address is incremented by src_pitch bytes and the dst address is incremented by dst_pitch bytes.
int32_t EdmaMgr_copy1D1DLinked ( EdmaMgr_Handle  h,
void *restrict  src[],
void *restrict  dst[],
int32_t  num_bytes[],
int32_t  num_transfers 
)

Perform a group of linked 1D->1D transfers.

Parameters
[in]hHandle returned from EdmaMgr_alloc().
[in]src[]Array of source addresses
[in]dst[]Array of destination addresses
[in]num_bytes[]Array of number of bytes to transfer
[in]num_transfersNumber of transfers
Precondition
h must be a handle successfully returned from EdmaMgr_alloc().
See also
EdmaMgr_copy1D1D
int32_t EdmaMgr_copy1D2DLinked ( EdmaMgr_Handle  h,
void *restrict  src[],
void *restrict  dst[],
int32_t  num_bytes[],
int32_t  num_lines[],
int32_t  pitch[],
int32_t  num_transfers 
)

Perform a group of linked 1D->2D transfers.

Parameters
[in]hHandle returned from EdmaMgr_alloc().
[in]src[]Array of source addresses
[in]dst[]Array of destination addresses
[in]num_bytes[]Array of number of bytes to transfer
[in]num_lines[]Array of lines to transfer
[in]pitch[]Array of pitches
[in]num_transfersNumber of transfers
Precondition
h must be a handle successfully returned from EdmaMgr_alloc().
See also
EdmaMgr_copy1D2D
int32_t EdmaMgr_copy2D1DLinked ( EdmaMgr_Handle  h,
void *restrict  src[],
void *restrict  dst[],
int32_t  num_bytes[],
int32_t  num_lines[],
int32_t  pitch[],
int32_t  num_transfers 
)

Perform a group of linked 2D->1D transfers.

Parameters
[in]hHandle returned from EdmaMgr_alloc().
[in]src[]Array of source addresses
[in]dst[]Array of destination addresses
[in]num_bytes[]Array of number of bytes to transfer
[in]num_lines[]Array of lines to transfer
[in]pitch[]Array of pitches
[in]num_transfersNumber of transfers
Precondition
h must be a handle successfully returned from EdmaMgr_alloc().
See also
EdmaMgr_copy2D1D
int32_t EdmaMgr_copy2D2DLinked ( EdmaMgr_Handle  h,
void *restrict  src[],
void *restrict  dst[],
int32_t  num_bytes[],
int32_t  num_lines[],
int32_t  pitch[],
int32_t  num_transfers 
)

Perform a group of linked 2D->2D transfers.

Parameters
[in]hHandle returned from EdmaMgr_alloc().
[in]src[]Array of source addresses
[in]dst[]Array of destination addresses
[in]num_bytes[]Array of number of bytes to transfer
[in]num_lines[]Array of lines to transfer
[in]pitch[]Array of pitches
[in]num_transfersNumber of transfers
Precondition
h must be a handle successfully returned from EdmaMgr_alloc().
See also
EdmaMgr_copy2D2D
int32_t EdmaMgr_copy2D2DSepLinked ( EdmaMgr_Handle  h,
void *restrict  src[],
void *restrict  dst[],
int32_t  num_bytes[],
int32_t  num_lines[],
int32_t  src_pitch[],
int32_t  dst_pitch[],
int32_t  num_transfers 
)

Perform a group of linked 2D->2D transfers with different pitches.

Parameters
[in]hHandle returned from EdmaMgr_alloc().
[in]src[]Array of source addresses
[in]dst[]Array of destination addresses
[in]num_bytes[]Array of number of bytes to transfer
[in]num_lines[]Array of lines to transfer
[in]src_pitch[]Array of source pitches
[in]dst_pitch[]Array of destination pitches
[in]num_transfersNumber of transfers
Precondition
h must be a handle successfully returned from EdmaMgr_alloc().
See also
EdmaMgr_copy2D2DSep
int32_t EdmaMgr_copy1D2DLarge ( EdmaMgr_Handle  h,
void *restrict  src,
void *restrict  dst,
int32_t  num_bytes,
int32_t  num_lines,
int32_t  pitch 
)

Perform a 1D->2D large transfer.

Parameters
[in]hHandle returned from EdmaMgr_alloc().
[in]srcSource address
[in]dstDestination address
[in]num_bytesNumber of bytes to transfer
[in]num_linesNumber of lines
[in]pitchPitch
Precondition
h must be a handle successfully returned from EdmaMgr_allocLarge().
Remarks
Perform a 1D->2D transfer of num_bytes bytes. The source is one dimensional, and the destination is two dimensional.
After every line of num_bytes is transferred, the src address is incremented by num_bytes and the dst address is incremented by pitch bytes.
This should be used when the pitch is outside the range of [-32768,32767].
int32_t EdmaMgr_copy2D1DLarge ( EdmaMgr_Handle  h,
void *restrict  src,
void *restrict  dst,
int32_t  num_bytes,
int32_t  num_lines,
int32_t  pitch 
)

Perform a 2D->1D large transfer.

Parameters
[in]hHandle returned from EdmaMgr_alloc().
[in]srcSource address
[in]dstDestination address
[in]num_bytesNumber of bytes to transfer
[in]num_linesNumber of lines
[in]pitchPitch
Precondition
h must be a handle successfully returned from EdmaMgr_allocLarge().
Remarks
Perform a 2D->1D transfer of num_bytes bytes. The source is two dimensional, and the destination is one dimensional.
After every line of num_bytes is transferred, the src address is incremented by pitch and the dst address is incremented by num_bytes bytes.
This should be used when the pitch is outside the range of [-32768,32767].
int32_t EdmaMgr_copyFast ( EdmaMgr_Handle  h,
void *restrict  src,
void *restrict  dst 
)

Perform a fast copy. This API inherits the transfer configuration of a previous transfer and only modifies the src and dst addresses.

Parameters
[in]hHandle returned from EdmaMgr_alloc().
[in]srcSource address
[in]dstDestination address
Precondition
h must be a handle successfully returned from EdmaMgr_alloc().
A non-linked transfer must have been completed on handle h before calling this function.
See also
EdmaMgr_copyLinkedFast
int32_t EdmaMgr_copyLinkedFast ( EdmaMgr_Handle  h,
void *restrict  src[],
void *restrict  dst[],
int32_t  num_transfers 
)

Perform a linked fast copy. This API inherits the transfer configuration of a previous transfer and only modifies the src and dst addresses.

Parameters
[in]hHandle returned from EdmaMgr_alloc().
[in]src[]Array of source addresses
[in]dst[]Array of destination addresses
[in]num_transfersNumber of transfers
Precondition
h must be a handle successfully returned from EdmaMgr_alloc().
A linked transfer must have been completed on handle h before calling this function.
See also
EdmaMgr_copyLinkedFast

Macro Definition Documentation

#define EdmaMgr_SUCCESS   0

Success

#define EdmaMgr_ERROR_INVARG   -1

Failure, Invalid Argument

#define EdmaMgr_ERROR_INVCFG   -2

Failure, Invalid Configuration

#define EdmaMgr_ERROR_RMANINIT   -3

Failure, RMAN initialization

#define EdmaMgr_ERROR_INVHANDLE   -4

Failure, Invalid Handle

#define EdmaMgr_ERROR_FREE   -5

Failure to free a resource

#define EdmaMgr_MAX_NUM_MEMRECS_LARGE   1

Maximum number of buffers required to allocate a large channel.

Typedef Documentation

typedef void* EdmaMgr_Handle

Handle to an EdmaMgr instance.

Configuration for a large channel.

Copyright 2015, Texas Instruments Incorporated