RMAN_Params Struct Reference
[Resource Manager for IRES-based resources]

The module configuration structure for RMAN. It is set at design time by the system integrator to register the specific Resource Managers(IRESMAN implementations). More...

#include <rman.h>

Data Fields

short numRegistries
IRESMAN_PersistentAllocFxnallocFxn
IRESMAN_PersistentFreeFxnfreeFxn
IRES_YieldFxn yieldFxn
Bool yieldSamePriority

Detailed Description

The module configuration structure for RMAN. It is set at design time by the system integrator to register the specific Resource Managers(IRESMAN implementations).

Remarks:
Typically, system integrators configure these settings using XDC config scripts. System integrators that use that method of configuration can ignore this structure definition. It's auto-generated during the config step by the XDC Tools.

Field Documentation


The documentation for this struct was generated from the following file:

Copyright 2009, Texas Instruments Incorporated