Resource Manager for IRES-based resources

Data Structures

struct  RMAN_Params
 The module configuration structure for RMAN. It is set at design time by the system integrator to register the specific Resource Managers(IRESMAN implementations). More...
struct  RMAN_YieldArgs
 Yield Arguments passed to the algorithm if RMAN's useDSKT2 flag is set. These arguments are used by the yield function set/get context and release/acquire locks for a particular scratch group. More...

Defines

#define RMAN_GTNAME   "ti.sdo.fc.rman"
 Name used to identify the GT module.
#define RMAN_PROTOCOLNAMESIZE   200
 Size of the Protocol Name in the Resource Registry Table.

Typedefs

typedef struct Sem_Obj * RMAN_SemHandle
 Declare abstract handle for Semaphore object.

Functions

IRES_Status RMAN_init (Void)
 Initialize the RMAN object with static information from the headers/configuration etc. This function has to return successfully before the other APIs are called.
IRES_Status RMAN_exit (Void)
 Delete the generic IRES RMAN and release memory back.
IRES_Status RMAN_register (IRESMAN_Fxns *resmanFxns, IRESMAN_Params *initArgs)
 Register the IRESMAN protocol/protocol revision i.e., device specific resource manager implementation with the Resource Registry of RMAN. RMAN logs these entries in an internal table that is uses to satisfy requests for different IRES resources.
IRES_Status RMAN_unregister (IRESMAN_Fxns *resmanFxns)
 Unregisters the protocol and the corresponding resource manager implementation from RMAN's Resource Registry. This API is called when this resource no longer needs to be managed by RMAN.
IRES_Status RMAN_assignResources (IALG_Handle algHandle, IRES_Fxns *resFxns, Int scratchGroupId)
 Assign IRES resources to the algorithm indicated by algHandle. Algorithm could request multiple IRES resources of same/ different type through its IRES implementation. RMAN would identify which IRESMAN implementation (that is registered with it) to query and then request resources from that, to satisfy the individual IRES requests. Non-algorithm users of this API can obtain resources by passing * NULL as the algHandle. Resources will still be assigned to the IRES_Fxns::initResources API.
IRES_Status RMAN_freeResources (IALG_Handle algHandle, IRES_Fxns *resFxns, Int scratchGroupId)
 Free resources held by the algorithm resource handle.
IRES_Status RMAN_activateResource (IALG_Handle algHandle, IRES_Handle resourceHandle, IRES_Fxns *resFxns, Int scratchGroupId)
 Activate resource identified by the resourceHandle held by the algorithm.
IRES_Status RMAN_activateAllResources (IALG_Handle algHandle, IRES_Fxns *resFxns, Int scratchGroupId)
 Activate all resources held by the algorithm.
IRES_Status RMAN_deactivateResource (IALG_Handle algHandle, IRES_Handle resourceHandle, IRES_Fxns *resFxns, Int scratchGroupId)
 Deactivate resource identified by the resourceHandle held by the algorithm.
IRES_Status RMAN_deactivateAllResources (IALG_Handle algHandle, IRES_Fxns *resFxns, Int scratchGroupId)
 Deactivate all resources held by the algorithm.
void RMAN_yield (IRES_YieldResourceType resource, IRES_YieldContextHandle algYieldContext, IRES_YieldArgs yieldArgs)
 Yield function specifically for use when DSKT2 based algorithms need cooperative preemption and multi-tasking support This function is called by the algorithm at pre-determined points during its execution, to allow another algorithm of same, or higher prioirty to preempt its execution.

Variables

__FAR__ RMAN_Params RMAN_PARAMS
__FAR__ IRESMAN_FxnsRMAN_TABLE []
__FAR__ short RMAN_FREE_ENTRIES []
__FAR__ short RMAN_numRegistryEntries
__FAR__ IRESMAN_Fxns ** RMAN_registryEntries
__FAR__ IRESMAN_Params ** RMAN_registryResmanArgs

Detailed Description

IRES generic Resource Manager RMAN Definitions - Generic Resource Manager that manages resource allocation for algorithms that implement the IRES interface


Define Documentation

#define RMAN_GTNAME   "ti.sdo.fc.rman"

Name used to identify the GT module.

#define RMAN_PROTOCOLNAMESIZE   200

Size of the Protocol Name in the Resource Registry Table.


Typedef Documentation

typedef struct Sem_Obj* RMAN_SemHandle

Declare abstract handle for Semaphore object.


Function Documentation

IRES_Status RMAN_init ( Void   ) 

Initialize the RMAN object with static information from the headers/configuration etc. This function has to return successfully before the other APIs are called.

Return values:
IRES_OK IRES RMAN created successfully
IRES_ENORESOURCE One of the calls to the device specific Resource Manager failed
IRES_Status RMAN_exit ( Void   ) 

Delete the generic IRES RMAN and release memory back.

Return values:
IRES_OK IRES RMAN exited successfully
IRES_EFAIL Error closing device specific RESMAN
IRES_Status RMAN_register ( IRESMAN_Fxns resmanFxns,
IRESMAN_Params initArgs 
)

Register the IRESMAN protocol/protocol revision i.e., device specific resource manager implementation with the Resource Registry of RMAN. RMAN logs these entries in an internal table that is uses to satisfy requests for different IRES resources.

Parameters:
[in] resmanFxns Device-specific implementation of the IRESMAN interfaces
[in] initArgs Arguments to the initialization interface of the RESMAN interfaces
Return values:
IRES_OK Registered successfully
IRES_EEXISTS Protocol already exists
IRES_ENORESOURCE Device specific Resman failed to initialize Resource Manager failed
IRES_EFAIL Error closing device specific RESMAN
IRES_Status RMAN_unregister ( IRESMAN_Fxns resmanFxns  ) 

Unregisters the protocol and the corresponding resource manager implementation from RMAN's Resource Registry. This API is called when this resource no longer needs to be managed by RMAN.

Parameters:
[in] resmanFxns Device-specific implementation of the RESMAN interfaces
Return values:
IRES_OK Unregistered successfully
IRES_ENOTFOUND Entry not found in the RMAN Table
IRES_EFAIL Error closing device specific RESMAN
IRES_Status RMAN_assignResources ( IALG_Handle  algHandle,
IRES_Fxns resFxns,
Int  scratchGroupId 
)

Assign IRES resources to the algorithm indicated by algHandle. Algorithm could request multiple IRES resources of same/ different type through its IRES implementation. RMAN would identify which IRESMAN implementation (that is registered with it) to query and then request resources from that, to satisfy the individual IRES requests. Non-algorithm users of this API can obtain resources by passing * NULL as the algHandle. Resources will still be assigned to the IRES_Fxns::initResources API.

Parameters:
[in] algHandle Handle to the algorithm
[in] resFxns Handle to the IRES implementation
[in] scratchGroupId Id of the scratch group in which resources are requested from -1 if persistent resources are requested. Note: If performing cooperative preemption, use the same scratchGroupId * to request resources and to create algorithm. Failure to do so, will lead to unexpected behaviour.
Return values:
IRES_OK Resources assigned successfully
IRES_EALG One of the calls to the IRES interfaces of the algorithm failed
IRES_ENOMEM Not enough memory
IRES_ENOTFOUND Entry not found
IRES_ENORESOURCE Resources unavailable
IRES_EFAIL Error freeing handles etc
IRES_Status RMAN_freeResources ( IALG_Handle  algHandle,
IRES_Fxns resFxns,
Int  scratchGroupId 
)

Free resources held by the algorithm resource handle.

Parameters:
[in] algHandle Handle to the algorithm, could be NULL for non-algorithm requests.
[in] resFxns Handle to the IRES implementation
[in] scratchGroupId Id of the scratch group in which resources were requested -1 if persistent resources are requested
Return values:
IRES_OK Resources freed successfully
IRES_EALG One of the calls to the IRES interfaces of the algorithm failed
IRES_ENOMEM Not enough memory
IRES_ENOTFOUND Entry not found
IRES_ENORESOURCE Error obtaining resource information
IRES_EFAIL Error freeing handles etc
IRES_ENOMEM Out of memory
IRES_Status RMAN_activateResource ( IALG_Handle  algHandle,
IRES_Handle  resourceHandle,
IRES_Fxns resFxns,
Int  scratchGroupId 
)

Activate resource identified by the resourceHandle held by the algorithm.

Parameters:
[in] algHandle Handle to the algorithm
[in] resourceHandle Handle to the resource
[in] resFxns Handle to the IRES implementation
[in] scratchGroupId Id of the scratch group in which resources are requested from
Return values:
IRES_OK Resource activated successfully
IRES_Status RMAN_activateAllResources ( IALG_Handle  algHandle,
IRES_Fxns resFxns,
Int  scratchGroupId 
)

Activate all resources held by the algorithm.

Parameters:
[in] algHandle Handle to the algorithm
[in] resFxns Handle to the IRES implementation
[in] scratchGroupId Id of the scratch group in which resources are requested from
Return values:
IRES_OK All resources activated successfully
IRES_Status RMAN_deactivateResource ( IALG_Handle  algHandle,
IRES_Handle  resourceHandle,
IRES_Fxns resFxns,
Int  scratchGroupId 
)

Deactivate resource identified by the resourceHandle held by the algorithm.

Parameters:
[in] algHandle Handle to the algorithm
[in] resourceHandle Handle to the resource
[in] resFxns Handle to the IRES implementation
[in] scratchGroupId Id of the scratch group in which resources are requested from
Return values:
IRES_OK Resource deactivated successfully
IRES_Status RMAN_deactivateAllResources ( IALG_Handle  algHandle,
IRES_Fxns resFxns,
Int  scratchGroupId 
)

Deactivate all resources held by the algorithm.

Parameters:
[in] algHandle Handle to the algorithm
[in] resFxns Handle to the IRES implementation
[in] scratchGroupId Id of the scratch group in which resources are requested from
Return values:
IRES_OK Resources deactivated successfully
void RMAN_yield ( IRES_YieldResourceType  resource,
IRES_YieldContextHandle  algYieldContext,
IRES_YieldArgs  yieldArgs 
)

Yield function specifically for use when DSKT2 based algorithms need cooperative preemption and multi-tasking support This function is called by the algorithm at pre-determined points during its execution, to allow another algorithm of same, or higher prioirty to preempt its execution.

Parameters:
[in] resource Enum identifying type of resource (ALL, Scratch Memory, Scratch DMA, IRES Resource)
[in] algYieldContext Handle to the yield context that contains information supplied by the algorithm including the algorithm handle, the corresponding context save/restore fxns and arguments with which to call these fxns.
[in] yieldArgs Framework supplied yield arguments that are passed to the algorithm at the time of granting resource handles. These should be passed back unmodified to this function.

Variable Documentation

__FAR__ short RMAN_FREE_ENTRIES[]
__FAR__ short RMAN_numRegistryEntries

Copyright 2009, Texas Instruments Incorporated