IVIDENC_Fxns Struct Reference
[XDM IVIDENC Video Encoder Interface]

Defines all of the operations on IVIDENC objects. More...

#include <ividenc.h>

Collaboration diagram for IVIDENC_Fxns:
Collaboration graph
[legend]

Data Fields

IALG_Fxns ialg
XDAS_Int32(* process )(IVIDENC_Handle handle, XDM_BufDesc *inBufs, XDM_BufDesc *outBufs, IVIDENC_InArgs *inArgs, IVIDENC_OutArgs *outArgs)
 Basic video encoding call.
XDAS_Int32(* control )(IVIDENC_Handle handle, IVIDENC_Cmd id, IVIDENC_DynamicParams *params, IVIDENC_Status *status)
 Control behavior of an algorithm.

Detailed Description

Defines all of the operations on IVIDENC objects.


Field Documentation

XDAIS algorithm interface.

See also:
IALG_Fxns

Basic video encoding call.

Parameters:
[in] handle Handle to an algorithm instance.
[in] inBufs Input buffer descriptors.
[in,out] outBufs Output buffer descriptors. The algorithm may modify the output buffer pointers.
[in] inArgs Input arguments. This is a required parameter.
[out] outArgs Ouput results. This is a required parameter.
Remarks:
process() is a blocking call. When process() returns, the algorithm's processing is complete.
Precondition:
inArgs must not be NULL, and must point to a valid IVIDENC_InArgs structure.
outArgs must not be NULL, and must point to a valid IVIDENC_OutArgs structure.
The buffers in inBufs and outBufs are physically contiguous and owned by the calling application.
Postcondition:
The algorithm must not modify the contents of inArgs.
The buffers in inBufs are owned by the calling application.
Return values:
IALG_EOK Success.
IALG_EFAIL Failure. See IVIDENC_OutArgs::extendedError for more detailed further error conditions.

Control behavior of an algorithm.

Parameters:
[in] handle Handle to an algorithm instance.
[in] id Command id. See XDM_CmdId.
[in] params Dynamic parameters. This is a required parameter.
[out] status Output results. This is a required parameter.
Precondition:
handle must be a valid algorithm instance handle.
params must not be NULL, and must point to a valid IVIDENC_DynamicParams structure.
status must not be NULL, and must point to a valid IVIDENC_Status structure.
Postcondition:
The algorithm must not modify the contents of params. That is, the data pointed to by this parameter must be treated as read-only.
Return values:
IALG_EOK Success.
IALG_EFAIL Failure. See IVIDENC_Status::extendedError for more detailed further error conditions.

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated