IVIDDEC2_OutArgs Struct Reference
[XDM IVIDDEC2 Video Decoder Interface]

Defines the run time output arguments for all IVIDDEC2 instance objects. More...

#include <ividdec2.h>

Collaboration diagram for IVIDDEC2_OutArgs:
Collaboration graph
[legend]

Data Fields

XDAS_Int32 size
XDAS_Int32 bytesConsumed
XDAS_Int32 outputID [20]
IVIDEO1_BufDesc decodedBufs
IVIDEO1_BufDesc displayBufs [20]
XDAS_Int32 outputMbDataID
XDM1_SingleBufDesc mbDataBuf
XDAS_Int32 freeBufID [20]
XDAS_Int32 outBufsInUseFlag

Detailed Description

Defines the run time output arguments for all IVIDDEC2 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC2_Fxns::process()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Number of bytes consumed during the process() call.

Output ID corresponding to displayBufs[].

Remarks:
A value of zero (0) indicates an invalid ID. The first zero entry in array will indicate end of valid outputIDs within the array. Hence the application can stop reading the array when it encounters the first zero entry.
See also:
IVIDDEC2_OutArgs::displayBufs
IVIDDEC2_InArgs::inputID

The decoder fills this structure with buffer pointers to the decoded frame. Related information fields for the decoded frame are also populated.

When frame decoding is not complete, as indicated by outBufsInUseFlag, the frame data in this structure will be incomplete. However, the algorithm will provide incomplete decoded frame data in case application may choose to use it for error recovery purposes.

See also:
IVIDDEC2_OutArgs::outBufsInUseFlag

Array containing display frames corresponding to valid ID entries in the outputID[] array.

Remarks:
Entries in the array corresponding to invalid ID values (zero) in outputID[] will set zero value for the following fields in the IVIDEO1_BufDesc structure: numBufs, frameWidth, frameHeight, and framePitch.
Implied by the previous remark, as this array corresponds to buffer IDs indicated by outputID[], elements of this array are undefined if the corresponding outputID[] element is zero (0).

Output ID corresponding with the MB Data

Remarks:
This will be set to zero when there is no MB Data Buffer

The decoder populates the last buffer among the buffers supplied within outBufs->bufs[] with the decoded MB data generated by the ECD module. The pointer buffer along with the buffer size is output via this buffer descriptor.

This is an array of inputID's corresponding to the buffers that have been unlocked in the current process call.

Remarks:
Buffers returned to the application for display (via IVIDDEC2_OutArgs::displayBufs) continue to be owned by the algorithm until they are released - indicated by the ID being returned in this freeBuf array.
The buffers released by the algorithm are indicated by their non-zero ID (previously provided via IVIDDEC2_InArgs::inputID).
A value of zero (0) indicates an invalid ID. The first zero entry in array will indicate end of valid freeBufIDs within the array. Hence the application can stop searching the array when it encounters the first zero entry.
If no buffer was unlocked in the process call, freeBufID[0] will have a value of zero.
See also:
IVIDDEC2_InArgs::inputID
IVIDDEC2_OutArgs::displayBufs

Flag to indicate that the outBufs provided with the process() call are in use. No outBufs are required to be supplied with the next process() call.

Remarks:
Valid values are XDAS_TRUE and XDAS_FALSE.

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated