ISPHENC_Status Struct Reference
[XDM ISPHENC Speech/Voice Encoder Interface]

Defines instance status parameters (read-only). More...

#include <isphenc.h>

Collaboration diagram for ISPHENC_Status:
Collaboration graph
[legend]

Data Fields

XDAS_Int32 size
XDAS_Int32 extendedError
XDAS_Int32 frameSize
XDAS_Int32 bitRate
XDAS_Int32 mode
XDAS_Int32 vadFlag
XDAS_Int32 noiseSuppressionMode
XDAS_Int32 ttyTddMode
XDAS_Int32 dtmfMode
XDAS_Int32 dataTransmit
XDAS_Int32 homingMode
XDM_AlgBufInfo bufInfo

Detailed Description

Defines instance status parameters (read-only).

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
ISPHENC_Fxns::control()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Extended error information.

Remarks:
When an internal error occurs, the algorithm will return an error return value (e.g. EFAIL, EUNSUPPORTED)
The value of each enum is the bit which is set.
Bits 31-16 are reserved. Bits 7-0 are codec and implementation specific.
The algorithm can set multiple bits to 1 based on conditions. e.g. it will set bits XDM_FATALERROR (fatal) and XDM_UNSUPPORTEDPARAM (unsupported params) in case of unsupported run time parameters.
This enumeration data type should not be used for storage, but rather only for its constant values.

See also:
XDM_ErrorBit

Input frame size in bytes for sample based codecs

Rate selection for multi_rate codecs

Mode selection for multi_mode codecs

VAD_On =1, VAD_OFF = 0

0 - OFF, 1 = NS-A, 2 = NS-B etc

0 = TTY OFF, 1 = 45.45bauds 2 = 50 bauds

0 = DTMF_OFF, 1 = DTMF_ON

1 = ON, 0 = OFF

0 - DISABLED; 1 - ENABLED

Input and output buffer information.

See also:
XDM_AlgBufInfo.

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated