Defines all of the operations on IIMGDEC1 objects.
More...
#include <iimgdec1.h>
Detailed Description
Defines all of the operations on IIMGDEC1 objects.
Field Documentation
XDAIS algorithm interface.
- See also:
- IALG_Fxns
Basic image decoding call.
- Parameters:
-
[in] | handle | Handle to an algorithm instance. |
[in,out] | inBufs | Input buffer descriptors. |
[in,out] | outBufs | Output buffer descriptors. The algorithm may modify the output buffer pointers. |
[in] | inArgs | Input arguments. This is a required parameter. |
[out] | outArgs | Ouput results. This is a required parameter. |
- Precondition:
handle
must be a valid algorithm instance handle.
-
inArgs
must not be NULL, and must point to a valid IIMGDEC1_InArgs structure.
-
outArgs
must not be NULL, and must point to a valid IIMGDEC1_OutArgs structure.
-
inBufs
must not be NULL, and must point to a valid XDM1_BufDesc structure.
-
inBufs->descs
[0].buf must not be NULL, and must point to a valid buffer of data that is at least inBufs->descs
[0].bufSize bytes in length.
-
outBufs
must not be NULL, and must point to a valid XDM1_BufDesc structure.
-
outBufs->descs
[0].buf must not be NULL, and must point to a valid buffer of data that is at least outBufs->descs
[0].bufSize bytes in length.
-
The buffers in
inBufs
and outBufs
are physically contiguous and owned by the calling application.
- Postcondition:
- The algorithm must not modify the contents of
inArgs
.
-
The algorithm must not modify the contents of
inBufs
, with the exception of inBufs.descs
[].accessMask. That is, the data and buffers pointed to by these parameters must be treated as read-only.
-
The algorithm must appropriately set/clear the
XDM1_BufDesc::descs
[].accessMask field in both inBufs
and outBufs
. For example, if the algorithm only read from inBufs.descs
[0].buf using the algorithm processor, it could utilize XDM_SETACCESSMODE_READ to update the appropriate accessMask
fields. The application may utilize these returned values to appropriately manage cache.
-
The buffers in
inBufs
and outBufs
are owned by the calling application.
- Return values:
-
| IIMGDEC1_EOK | Success. |
| IIMGDEC1_EFAIL | General failure. See IIMGDEC1_Status::extendedError for more detailed further error conditions. |
| IIMGDEC1_EUNSUPPORTED | Request is unsupported. |
Control behaviour of an algorithm.
- Parameters:
-
[in] | handle | Handle to an algorithm instance. |
[in] | id | Command id. See XDM_CmdId. |
[in] | params | Dynamic parameters. This is a required parameter. |
[out] | status | Output results. This is a required parameter. |
- Precondition:
handle
must be a valid algorithm instance handle.
-
params
must not be NULL, and must point to a valid IIMGDEC1_DynamicParams structure.
-
status
must not be NULL, and must point to a valid IIMGDEC1_Status structure.
-
If a buffer is provided in the
status->data
field, it must be physically contiguous and owned by the calling application.
- Postcondition:
- The algorithm must not modify the contents of
params
. That is, the data pointed to by this parameter must be treated as read-only.
-
If a buffer was provided in the
status->data
field, it is owned by the calling application.
- Return values:
-
| IIMGDEC1_EOK | Success. |
| IIMGDEC1_EFAIL | General failure. See IIMGDEC1_Status::extendedError for more detailed further error conditions. |
| IIMGDEC1_EUNSUPPORTED | Request is unsupported. |
The documentation for this struct was generated from the following file: