Defines the creation time parameters for all IAUDENC1 instance objects. More...
#include <iaudenc1.h>
Defines the creation time parameters for all IAUDENC1 instance objects.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details. Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Sampling Frequency in Hz. For example, if the sampling frequency is 44.1 kHz, this field will be 44100.
Average bit rate, in bits per second.
Input Channel Mode.
Endianness of input data.
Encoding mode.
Input format block/interleaved.
Number of input bits per output sample. For example, if there are 16 bits per PCM input sample, this should be set to 16.
Maximum bit rate in case of VBR. Some of the encoders allow you to specify max bit rate in case of VBR mode
Mode to indicate type of Dual Mono. Applicable only if channelMode is dualMono
Flag indicating whether the encoder should insert CRC bits into the bitstream or not.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.
Ancillary Data Flag.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.
Flag indicating whether LFE channel data is present or not in the input.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.