IAUDDEC1_InArgs Struct Reference
[XDM IAUDDEC1 Audio Decoder Interface]

Defines the input arguments for all IAUDDEC1 instance process function. More...

#include <iauddec1.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 numBytes
XDAS_Int32 desiredChannelMode
XDAS_Int32 lfeFlag

Detailed Description

Defines the input arguments for all IAUDDEC1 instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IAUDDEC1_Fxns::process()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Size of input data in bytes, provided to the algorithm for decoding.

Desired Channel Configuration.

See also:
IAUDIO_ChannelMode

Flag indicating whether LFE channel data is desired in the output.

Valid values for this field are XDAS_TRUE and XDAS_FALSE.


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated