IMGENC Image Encoder Interface

Data Structures

struct  IIMGENC_CodecClassConfig
 Definition of IIMGENC codec class configurable parameters. More...

Defines

#define IMGENC_EOK   IIMGENC_EOK
#define IMGENC_EFAIL   IIMGENC_EFAIL
#define IMGENC_ERUNTIME   IIMGENC_ERUNTIME
#define IMGENC_ETIMEOUT   VISA_ETIMEOUT
#define IMGENC_FOREVER   VISA_FOREVER

Typedefs

typedef IIMGENC_Status IMGENC_Status
typedef VISA_Handle IMGENC_Handle
 Opaque handle to a IMGENC codec.
typedef struct IIMGENC_Params IMGENC_Params
 This structure defines the parameters necessary to create an instance of an image encoder object.
typedef IIMGENC_InArgs IMGENC_InArgs
typedef IIMGENC_OutArgs IMGENC_OutArgs
typedef IIMGENC_Cmd IMGENC_Cmd
typedef IIMGENC_DynamicParams IMGENC_DynamicParams

Functions

IMGENC_Handle IMGENC_create (Engine_Handle e, String name, IMGENC_Params *params)
 Create an instance of an image encoder algorithm.
Int32 IMGENC_process (IMGENC_Handle handle, XDM_BufDesc *inBufs, XDM_BufDesc *outBufs, IMGENC_InArgs *inArgs, IMGENC_OutArgs *outArgs)
 Execute the process() method in this instance of an image encoder algorithm.
Int32 IMGENC_control (IMGENC_Handle handle, IMGENC_Cmd id, IMGENC_DynamicParams *params, IMGENC_Status *status)
 Execute the control() method in this instance of an image encoder algorithm.
Void IMGENC_delete (IMGENC_Handle handle)
 Delete the instance of an image encoder algorithm.
XDAS_Int32 IMGENC_processAsync (IMGENC_Handle handle, XDM_BufDesc *inBufs, XDM_BufDesc *outBufs, IIMGENC_InArgs *inArgs, IIMGENC_OutArgs *outArgs)
 Perform asynchronous submission to this instance of an image encoder algorithm.
XDAS_Int32 IMGENC_processWait (IMGENC_Handle handle, XDM_BufDesc *inBufs, XDM_BufDesc *outBufs, IIMGENC_InArgs *inArgs, IIMGENC_OutArgs *outArgs, UInt timeout)
 Wait for a return message from a previous invocation of IMGENC_processAsync() in this instance of an image encoder algorithm.

Detailed Description

This is the IMGENC image encoder interface. Several of the data types in this API are specified by the XDM interface; please see the XDM documentation for those details.


Define Documentation

#define IMGENC_EOK   IIMGENC_EOK

Success.

#define IMGENC_EFAIL   IIMGENC_EFAIL

General failure.

#define IMGENC_ERUNTIME   IIMGENC_ERUNTIME

General runtime failure.

#define IMGENC_ETIMEOUT   VISA_ETIMEOUT

Timeout occurred.

#define IMGENC_FOREVER   VISA_FOREVER

Special value for timeout parameter indicating never timeout.


Typedef Documentation

Defines instance status parameters (read-only).

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IIMGENC_Fxns::control()

Opaque handle to a IMGENC codec.

typedef struct IIMGENC_Params IMGENC_Params

This structure defines the parameters necessary to create an instance of an image encoder object.

Defines the input arguments for all IIMGENC instance process() function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IIMGENC_Fxns::process()

Defines the run time output arguments for all IIMGENC instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IIMGENC_Fxns::process()

Defines the control commands for the IIMGENC module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId
IIMGENC_Fxns::control()

This structure defines the algorithm parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IIMGENC_Fxns::control()


Function Documentation

IMGENC_Handle IMGENC_create ( Engine_Handle  e,
String  name,
IMGENC_Params params 
)

Create an instance of an image encoder algorithm.

Instance handles must not be concurrently accessed by multiple threads; each thread must either obtain its own handle (via IMGENC_create()) or explicitly serialize access to a shared handle.

Parameters:
[in] e Handle to an opened engine.
[in] name String identifier of the type of image encoder to create.
[in] params Creation parameters.
Return values:
NULL An error has occurred.
non-NULL The handle to the newly created image encoder instance.
Remarks:
params is optional. If it's not supplied, codec-specific default params will be used.
Depending on the configuration of the engine opened, this call may create a local or remote instance of the image encoder.
In general, name is the name of the codec configured by the system integrator. However, an optional "argument string" may be appended to the codec name, to allow the codec's configured priority and/or the heaps where its memory will be allocated and/or the number of VISA messages to allocate, to be overridden. This optional argument string is of the form ":priority:flag:number-of-messages", and can be specified with an empty field for any element that you don't want to be overridden, e.g. "mp3:::3" to cause 3 messages to be allocated while using the default values for priority and the heap flag.
priority is the new priority to create the codec with.
The flag must be either 0 or 1, and if 1, all memory allocated for the codec will be in the heap that corresponds to IALG_EXTERNAL. If flag is 0, the memory for the codec will be allocated from the heaps it has requested. For example, if a codec named "mp3" has been configured into the system, setting name to "mp3:4" would cause the codec to be created at priority 4, instead of whatever priority was configured. This feature is useful if more than one instance of the codec are to be created at different priorities.
The flag can be used to prevent the codec from using any internal memory, for example, if it is to be run at the same time as another codec that must use internal memory, and there is insufficient internal memory for both.
The number-of-messages overrides the default of 1 message, and is useful (or required, practically speaking) for when the "asynchronous" process method is used, i.e. "AUDENC1_processAsync()"
See also:
Engine_open()
IMGENC_delete()
Int32 IMGENC_process ( IMGENC_Handle  handle,
XDM_BufDesc inBufs,
XDM_BufDesc outBufs,
IMGENC_InArgs inArgs,
IMGENC_OutArgs outArgs 
)

Execute the process() method in this instance of an image encoder algorithm.

Parameters:
[in] handle Handle to a created image encoder instance.
[in] inBufs A buffer descriptor containing input buffers.
[out] outBufs A buffer descriptor containing output buffers.
[in] inArgs Input Arguments.
[out] outArgs Output Arguments.
Precondition:
handle is a valid (non-NULL) image encoder handle and the image encoder is in the created state.
Return values:
IMGENC_EOK Success.
IMGENC_EFAIL Failure.
IMGENC_ERUNTIME Internal Runtime Error.
Remarks:
Since the IMGENC encoder contains support for asynchronous buffer submission and retrieval, this API becomes known as synchronous in nature.
This is a blocking call, and will return after the data has been encoded.
The buffers supplied to IMGENC_process() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
If an error is returned, outArgs->extendedError may indicate further details about the error. See IMGENC_OutArgs::extendedError for details.
See also:
IMGENC_create()
IMGENC_delete()
IMGENC_control()
IMGENC_processAsync()
IMGENC_processWait()
IIMGENC_Fxns::process() - the reflected algorithm interface, which may contain further usage details.
Int32 IMGENC_control ( IMGENC_Handle  handle,
IMGENC_Cmd  id,
IMGENC_DynamicParams params,
IMGENC_Status status 
)

Execute the control() method in this instance of an image encoder algorithm.

Parameters:
[in] handle Handle to a created image encoder instance.
[in] id Command id for XDM control operation.
[in] params Runtime control parameters used for encoding.
[out] status Status info upon completion of encode operation.
Precondition:
handle is a valid (non-NULL) image encoder handle and the image encoder is in the created state.
Return values:
IMGENC_EOK Success.
IMGENC_EFAIL Failure.
IMGENC_ERUNTIME Internal Runtime Error.
Remarks:
This is a blocking call, and will return after the control command has been executed.
If an error is returned, status->extendedError may indicate further details about the error. See IMGENC_Status::extendedError for details.
See also:
IMGENC_create()
IMGENC_delete()
IIMGENC_Fxns::control() - the reflected algorithm interface, which may contain further usage details.
Void IMGENC_delete ( IMGENC_Handle  handle  ) 

Delete the instance of an image encoder algorithm.

Parameters:
[in] handle Handle to a created image encoder instance.
Remarks:
Depending on the configuration of the engine opened, this call may delete a local or remote instance of the image encoder.
Precondition:
handle is a valid (non-NULL) handle which is in the created state.
Postcondition:
All resources allocated as part of the IMGENC_create() operation (memory, DMA channels, etc.) are freed.
See also:
IMGENC_create()
XDAS_Int32 IMGENC_processAsync ( IMGENC_Handle  handle,
XDM_BufDesc inBufs,
XDM_BufDesc outBufs,
IIMGENC_InArgs inArgs,
IIMGENC_OutArgs outArgs 
)

Perform asynchronous submission to this instance of an image encoder algorithm.

Parameters:
[in] handle Handle to a created image encoder instance.
[in] inBufs A buffer descriptor containing input buffers.
[out] outBufs A buffer descriptor containing output buffers.
[in] inArgs Input Arguments.
[out] outArgs Output Arguments.
Precondition:
handle is a valid (non-NULL) image encoder handle and the image encoder is in the created state.
Return values:
IMGENC_EOK Success.
IMGENC_EFAIL Failure.
IMGENC_ERUNTIME Internal Runtime Error.
Remarks:
This API is the asynchronous counterpart to the process() method. It allows for buffer and argument submission without waiting for retrieval. A response is retrieved using the IMGENC_processWait() API.
The buffers supplied to IMGENC_processAsync() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
See also:
IMGENC_create()
IMGENC_delete()
IMGENC_control()
IMGENC_process()
IMGENC_processWait()
IIMGENC_Fxns::process() - the reflected algorithm interface, which may contain further usage details.
XDAS_Int32 IMGENC_processWait ( IMGENC_Handle  handle,
XDM_BufDesc inBufs,
XDM_BufDesc outBufs,
IIMGENC_InArgs inArgs,
IIMGENC_OutArgs outArgs,
UInt  timeout 
)

Wait for a return message from a previous invocation of IMGENC_processAsync() in this instance of an image encoder algorithm.

Parameters:
[in] handle Handle to a created image encoder instance.
[in] inBufs A buffer descriptor containing input buffers.
[out] outBufs A buffer descriptor containing output buffers.
[in] inArgs Input Arguments.
[out] outArgs Output Arguments.
[in] timeout Amount of "time" to wait (from 0 -> IMGENC_FOREVER)
Precondition:
handle is a valid (non-NULL) image encoder handle and the image encoder is in the created state.
Return values:
IMGENC_EOK Success.
IMGENC_EFAIL Failure.
IMGENC_ERUNTIME Internal Runtime Error.
IMGENC_ETIMEOUT Operation timed out.
Remarks:
This is a blocking call, and will return after the data has been decoded.
"Polling" is supported by using a timeout of 0. Waiting forever is supported by using a timeout of IMGENC_EFOREVER.
There must have previously been an invocation of the IMGENC_processAsync() API.
The buffers supplied to IMGENC_processAsync() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
See also:
IMGENC_create()
IMGENC_delete()
IMGENC_control()
IMGENC_process()
IMGENC_processAsync()
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated