Data Structures | Defines | Typedefs | Enumerations | Functions | Variables

Codec Engine Runtime

Data Structures

struct  Engine_Attrs
 Attributes of an Engine. More...
struct  Engine_AlgInfo
 Properties of an Engine algorithm. More...
struct  Engine_AlgInfo2
 Properties of an Engine algorithm. More...
struct  Engine_AlgDesc
 Descriptor for an alg. This object can be passed to Engine_addAlg(), to dynamically add an alg to an engine. More...
struct  Engine_DllAlgDesc
 Descriptor for a dynamically loaded alg. A dynamic library for a codec must export a function that fills in a structure of this type. More...
struct  Engine_Desc
 This structure is passed to Engine_add(), and contains parameters to specify an engine. More...

Defines

#define Engine_MODNAME   "ti.sdo.ce.Engine"
 Name to pass to Diags_setMask() to enable logging for Engine functions.
#define Engine_EOK   0
#define Engine_EEXIST   1
#define Engine_ENOMEM   2
#define Engine_EDSPLOAD   3
#define Engine_ENOCOMM   4
#define Engine_ENOSERVER   5
#define Engine_ECOMALLOC   6
#define Engine_ERUNTIME   7
#define Engine_ECODECCREATE   8
#define Engine_ECODECSTART   9
#define Engine_EINVAL   10
#define Engine_EBADSERVER   11
#define Engine_ENOTAVAIL   12
#define Engine_EWRONGSTATE   13
#define Engine_EINUSE   14
#define Engine_ENOTFOUND   15
#define Engine_ETIMEOUT   16
#define Engine_GETALGDESCFXN   "GetEngineAlgDesc"
 Name of function that a dynamically loaded codec must supply.

Typedefs

typedef struct Engine_Obj * Engine_Handle
 Opaque handle to an engine.
typedef Int Engine_Error
 Engine error code.
typedef struct Engine_Attrs Engine_Attrs
 Attributes of an Engine.
typedef struct Engine_AlgInfo Engine_AlgInfo
 Properties of an Engine algorithm.
typedef struct Engine_AlgInfo2 Engine_AlgInfo2
 Properties of an Engine algorithm.
typedef enum Engine_CachedMemType Engine_CachedMemType
 Engine Cacheable Memory types.
typedef struct Engine_AlgDesc Engine_AlgDesc
 Descriptor for an alg. This object can be passed to Engine_addAlg(), to dynamically add an alg to an engine.
typedef struct Engine_DllAlgDesc Engine_DllAlgDesc
 Descriptor for a dynamically loaded alg. A dynamic library for a codec must export a function that fills in a structure of this type.
typedef Int(* Engine_GetAlgDescFxn )(Engine_DllAlgDesc *dllAlgDesc)
 Prototype of function that must be supplied by a dynamic codec library to fill in a Engine_DllAlgDesc structure.
typedef struct Engine_Desc Engine_Desc
 This structure is passed to Engine_add(), and contains parameters to specify an engine.

Enumerations

enum  Engine_CachedMemType {
  Engine_USECACHEDMEM_DEFAULT = -1,
  Engine_USECACHEDMEM_NONCACHED = 0,
  Engine_USECACHEDMEM_CACHED = 1
}
 

Engine Cacheable Memory types.

More...

Functions

Engine_Error Engine_addStubFxns (String fxnsName, IALG_Fxns *fxns)
 Register stub functions through which a remote algorithm can be called.
Engine_Error Engine_add (Engine_Desc *pDesc)
 Add an Engine to the database of engines that can be opened with Engine_open()
Engine_Error Engine_addAlg (String name, Engine_Handle engine, String location, Engine_AlgDesc *pAlgDesc)
 Dynamically add an algorithm to an Engine.
Engine_Error Engine_removeAlg (String name, Engine_Handle engine, String algName)
 Dynamically remove an algorithm that was added to an Engine with Engine_addAlg().
Void Engine_close (Engine_Handle engine)
 Close an Engine.
Void Engine_initAlgDesc (Engine_AlgDesc *pAlgDesc)
 Initialize an Engine_AlgDesc structure with default values.
Void Engine_initAttrs (Engine_Attrs *pAttrs)
 Initialize an Engine_Attrs structure with default values.
Void Engine_initDesc (Engine_Desc *pDesc)
 Initialize an Engine_Desc structure with default values.
Engine_Handle Engine_open (String name, Engine_Attrs *attrs, Engine_Error *ec)
 Open an Engine.
Int Engine_fwriteTrace (Engine_Handle engine, String prefix, FILE *out)
 Write Server's trace buffer to specifed file stream.
Engine_Error Engine_getAlgInfo (String name, Engine_AlgInfo *algInfo, Int index)
 Get details of an algorithm configured into an engine.
Engine_Error Engine_getAlgInfo2 (String name, Engine_Handle engine, Engine_AlgInfo2 *algInfo2, Int index)
 Get details of an algorithm.
Engine_Error Engine_getDesc (String name, Engine_Desc *desc)
 Fill in an Engine_Desc structure with the values of the Engine descriptor for an Engine.
Engine_Error Engine_getLastError (Engine_Handle engine)
 Get error code of the last failed operation.
String Engine_getName (Engine_Handle engine)
 Get the name of an opened engine.
Engine_Error Engine_getNumAlgs (String name, Int *numAlgs)
 Get the number of algorithms configured into an Engine.
Engine_Error Engine_getNumAlgs2 (String name, Engine_Handle engine, Int *numAlgs)
 Get the number of algorithms statically configured into an engine or the total number of algorithms both statically configured and dynamically added through server information when the engine was opened.
Server_Handle Engine_getServer (Engine_Handle engine)
 Get handle to an Engine's Server.
UInt32 Engine_getUsedMem (Engine_Handle engine)
 Get Server's total memory usage.
Engine_Error Engine_remove (String engineName)
 Remove an engine from the list of engines that can be opened.
Engine_Error Engine_setDesc (String name, Engine_Desc *desc)
 Set values for an Engine's descriptor. This function should only be called when the Engine has not yet been opened.
Int Engine_setTrace (Engine_Handle engine, String mask)
 Set Server's trace mask.

Variables

Engine_Attrs Engine_ATTRS
 Default engine attributes.

Define Documentation

#define Engine_MODNAME   "ti.sdo.ce.Engine"

Name to pass to Diags_setMask() to enable logging for Engine functions.

Example Usage:
The following code turns on all Log statements in the Engine module.
     Diags_setMask(Engine_MODNAME "+EX1234567");
Remarks:
Using Diags_setMask() to enable Engine Logging must be called after CERuntime_init() (which creates and initializes the Engine trace mask) to have any effect.
#define Engine_EOK   0

Success.

#define Engine_EEXIST   1

Name does not exist.

#define Engine_ENOMEM   2

Unable to allocate memory.

#define Engine_EDSPLOAD   3

Unable to load the DSP.

#define Engine_ENOCOMM   4

Unable to create a comm connection to the DSP.

#define Engine_ENOSERVER   5

Unable to locate the server on the DSP.

#define Engine_ECOMALLOC   6

Unable to allocate communication buffer.

#define Engine_ERUNTIME   7

Internal engine runtime failure.

#define Engine_ECODECCREATE   8

Creation of the Codec failed.

#define Engine_ECODECSTART   9

Start of the Codec failed. For codecs which are implemented as a thread, this implies that the codec thread of execution failed to start.

#define Engine_EINVAL   10

Bad paramater passed to method.

#define Engine_EBADSERVER   11

Incompatible server specified.

#define Engine_ENOTAVAIL   12

Service not available.

#define Engine_EWRONGSTATE   13

Call can not be made at this time.

#define Engine_EINUSE   14

Call can't be made at this time because a required name/resource is in use.

#define Engine_ENOTFOUND   15

Entity was not found.

#define Engine_ETIMEOUT   16

Timeout-based operation timed out.

#define Engine_GETALGDESCFXN   "GetEngineAlgDesc"

Name of function that a dynamically loaded codec must supply.


Typedef Documentation

typedef struct Engine_Obj* Engine_Handle

Opaque handle to an engine.

typedef Int Engine_Error

Engine error code.

typedef struct Engine_Attrs Engine_Attrs

Attributes of an Engine.

See also:
Engine_initAttrs().
Engine_open().

Properties of an Engine algorithm.

See also:
Engine_getAlgInfo()

Properties of an Engine algorithm.

Remarks:
This structure is identical to Engine_AlgInfo except that the typeTab array of strings is replaced by a single string called types. The string, types, represents a ';' separated list of inheritance hierarchies of the algorithm, for example, "ti.sdo.ce.video.IVIDDEC;ti.sdo.ce.test.xvideo.IVIDE".
See also:
Engine_getAlgInfo2()

Engine Cacheable Memory types.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.

Descriptor for an alg. This object can be passed to Engine_addAlg(), to dynamically add an alg to an engine.

See also:
Engine_initAlgDesc()
Engine_addAlg()

Descriptor for a dynamically loaded alg. A dynamic library for a codec must export a function that fills in a structure of this type.

See also:
Engine_GetAlgDescFxn
typedef Int(* Engine_GetAlgDescFxn)(Engine_DllAlgDesc *dllAlgDesc)

Prototype of function that must be supplied by a dynamic codec library to fill in a Engine_DllAlgDesc structure.

Remarks:
This function will be called by Engine_addAlg() to fill in the dynamic codec's descriptor.
See also:
Engine_DllAlgDesc
typedef struct Engine_Desc Engine_Desc

This structure is passed to Engine_add(), and contains parameters to specify an engine.

See also:
Engine_add()
Engine_open()

Enumeration Type Documentation

Engine Cacheable Memory types.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
Enumerator:
Engine_USECACHEDMEM_DEFAULT 

Use default cache setting

Engine_USECACHEDMEM_NONCACHED 

Use non-cached memory

Engine_USECACHEDMEM_CACHED 

Use cached memory


Function Documentation

Engine_Error Engine_addStubFxns ( String  fxnsName,
IALG_Fxns fxns 
)

Register stub functions through which a remote algorithm can be called.

Parameters:
[in]fxnsNameThe name of the stub function table (e.g. "UNIVERSAL_STUBS")
[in]fxnsAddress of stub function table (e.g. &UNIVERSAL_STUBS)
Precondition:
As with all Codec Engine API's, CERuntime_init() must have previously been called.
Remarks:
This service is not necessary if you configure your Engine at build/config time using Engine.createFromServer(). When using Engine.createFromServer(), the appropriate alg-specific stubs are added to the system automatically.
When on an RTOS (e.g. SYS/BIOS), the stubs registered are available to all Engines in the system. When on a HLOS (e.g. Linux, WinCE), the stubs registered are available to all Engines in the calling application's process.
The symbol passed to the fxns argument can often be found in the class-specific VISA header file (e.g. UNIVERSAL_STUBS is declared in ti/sdo/ce/universal/universal.h).
For example, to register "UNIVERSAL_STUBS" for use by an IUNIVERSAL-compliant algorithm at runtime, you can do the following:
      #include <ti/sdo/ce/Engine.h>
      #include <ti/sdo/ce/universal/universal.h>

      Engine_register("UNIVERSAL_STUBS",
              (IALG_Fxns *)&UNIVERSAL_STUBS);
Return values:
Engine_EOKSuccess.
Engine_ENOMEMMemory allocation failed.
See also:
Engine_open()
Engine_Error Engine_add ( Engine_Desc pDesc )

Add an Engine to the database of engines that can be opened with Engine_open()

Parameters:
[in]pDescThe handle of an Engine Descriptor object. Before setting the fields of pDesc, it must first be initialized with Engine_initDesc().
Return values:
Engine_EINVALBad parameter passed, such as pDesc = NULL, or pDesc->name = NULL.
Engine_EINUSEAn engine with the name pDesc->name already exists.
Engine_ENOMEMA memory allocation failed.
Engine_EOKSuccess.
Precondition:
As with all Codec Engine API's, CERuntime_init() must have previously been called.
Postcondition:
If the return value is Engine_EOK, Engine_open() can be called with pDesc->name.
Example Usage:
      #include <ti/sdo/ce/Engine.h>

      Engine_Desc desc;

      Engine_initDesc(&desc);

      desc.name = "myEngine";
      desc.remoteName = "myServer.x64P";
      Engine_add(&desc);
See also:
Engine_remove()
Engine_open()
Engine_Error Engine_addAlg ( String  name,
Engine_Handle  engine,
String  location,
Engine_AlgDesc pAlgDesc 
)

Dynamically add an algorithm to an Engine.

Remarks:
If the Engine has not been opened, the name of the Engine is used, otherwise, a handle to the opened Engine. If the Engine has been opened, the added alg will only be accessible to the caller of this function. Either one or the other, but not both, of name and engine should be non-NULL.
Parameters:
[in]nameThe name of the engine. name is specified in the engine configuration, or the name of an engine added with Engine_add(). This can only be non-NULL if the engine is not opened, otherwise, use an engine handle and set name to NULL.
[in]engineThe handle of an engine returned by Engine_open(). If engine is non-NULL, set name to NULL.
[in]locationString identifying the location of the algorithm. Often this is a file name, but for systems without a file system, it may be a system-specific string identifier. This may be NULL if the algorithm is built into the executable.
[in]pAlgDescParameters describing the algorithm being added. Before setting the fields of this structure, it should first be initialized with Engine_initAlgDesc(), to set all fields to default values. If location is non-NULL (a dynamic library), then the following fields of pAlgDesc must be specified: pAlgDesc->name pAlgDesc->isLocal pAlgDesc->groupId All other Engine_AlgDesc fields will be from the dynamic library. If location is NULL (not a dynamic library), the user must set the following fields of pAlgDesc: pAlgDesc->name pAlgDesc->fxns pAlgDesc->idmaFxns, if applicable pAlgDesc->iresFxns, if applicable pAlgDesc->isLocal pAlgDesc->groupId pAlgDesc->types
Precondition:
As with all Codec Engine API's, CERuntime_init() must have previously been called.
engine is a valid (non-NULL) engine handle which is in the open state.
Remarks:
If there is an existing algorithm in the engine already named name, an error will be returned.
Return values:
Engine_EOKSuccess.
Engine_EINUSEThe Engine name is non-NULL, and the Engine is open.
Engine_EINVALpAlgDesc or pAlgDesc->name is NULL.
Engine_EINVALBoth name and engine are NULL. Ensure one of these is non-NULL.
Engine_EINVALBoth name and engine are non-NULL. Ensure that one of these is NULL.
Engine_EEXISTThere is no engine with the given name.
Engine_EINUSEThe name of the alg in pAlgDesc->name is already in use.
Example Usage:
      #include <ti/sdo/ce/Engine.h>

      Engine_AlgDesc desc;

      Engine_initAlgDesc(&desc);

      desc.groupId = 2;
      desc.isLocal = TRUE;
      desc.fxns = &UNIVERSALCOPY_TI_IUNIVERSALCOPY;
      desc.idmaFxns = NULL;
      desc.iresFxns = NULL;
      desc.memType = Engine_USECACHEDMEM_DEFAULT;
      desc.types = UNIVERSAL_VISATYPE;

      status = Engine_addAlg("myEngine", NULL, NULL, &desc);
See also:
Engine_initAlgDesc()
Engine_open()
Engine_removeAlg()
Engine_Error Engine_removeAlg ( String  name,
Engine_Handle  engine,
String  algName 
)

Dynamically remove an algorithm that was added to an Engine with Engine_addAlg().

Remarks:
The same values of the parameters name and engine that were passed to Engine_addAlg() should be used here. In particular, if name was used to add the alg, all handles to the engine must be closed before calling Engine_removeAlg().
Parameters:
[in]nameThe name of the engine or NULL, that was passed to Engine_addAlg().
[in]engineThe handle to an engine, previously acquired by a call to Engine_open(), or NULL, that was used in Engine_addAlg().
[in]algNameName of the algorithm to remove.
Return values:
Engine_EOKSuccess.
Engine_EEXISTThe engine name does not exist.
Engine_ENOTFOUNDalgName could not be found in engine.
Engine_EINUSEThe Engine name is still open.
See also:
Engine_open()
Engine_addAlg()
Void Engine_close ( Engine_Handle  engine )

Close an Engine.

Parameters:
[in]engineThe handle to an engine, previously acquired by a call to Engine_open().
Precondition:
engine must not be referenced by any algorithm instance objects; i.e., you must first delete all algorithm instances associated with engine before closing it.
engine is a valid (non-NULL) engine handle which is in the open state.
See also:
Engine_open()
Void Engine_initAlgDesc ( Engine_AlgDesc pAlgDesc )

Initialize an Engine_AlgDesc structure with default values.

Parameters:
[in]pAlgDescLocation of Engine_AlgDesc object to initialize. The fields of pAlgDesc will be set to the following:

pAlgDesc->name = NULL; pAlgDesc->uuid.data = 0; pAlgDesc->fxns = NULL; pAlgDesc->idmaFxns = NULL; pAlgDesc->typeTab = NULL; pAlgDesc->isLocal = TRUE; pAlgDesc->groupId = 0; pAlgDesc->rpcProtocolVersion = 0; pAlgDesc->iresFxns = NULL; pAlgDesc->codecClassConfig = NULL; pAlgDesc->memType = Engine_USECACHEDMEM_DEFAULT; pAlgDesc->types = NULL;

See also:
Engine_addAlg()
Void Engine_initAttrs ( Engine_Attrs pAttrs )

Initialize an Engine_Attrs structure with default values.

Parameters:
[in]pAttrsLocation of Engine_Attrs object to initialize.
See also:
Engine_open()
Void Engine_initDesc ( Engine_Desc pDesc )

Initialize an Engine_Desc structure with default values.

Parameters:
[in]pDescLocation of Engine_Desc object to initialize. The fields of pDesc will be set to the following:

pDesc->name = NULL; pDesc->remoteName = NULL; pDesc->heapId = 0;

See also:
Engine_add()
Engine_Handle Engine_open ( String  name,
Engine_Attrs attrs,
Engine_Error ec 
)

Open an Engine.

The handle returned may be used to create one or more instances of an algorithm contained in the specified Engine.

An Engine may be opened more than once; each open returns a unique handle that can be used to create algorithm instances or get status of the Engine.

Engine handles must not be concurrently accessed by multiple threads; each thread must either obtain its own handle (via Engine_open()) or explicitly serialize access to a shared handle.

Parameters:
[in]nameThe name of the engine to open. name is specified in the engine configuration.
[in]attrsAttributes for the open engine.
[out]ecOptional output error code
Return values:
NULLAn error has occurred.
non-NULLThe handle to the opened engine.
Precondition:
name is a non-NULL string.
name is a valid, pre-configured name of an engine.
As with all Codec Engine API's, CERuntime_init() must have previously been called.
Postcondition:
If the return handle is NULL and ec is non-NULL, *ec is set to a non-zero value indicating the cause of the failure.
If ec is non-NULL, the Engine_Error value is set to one of the following values:
See also:
Engine_close()
Engine_add()
Engine_remove()
Int Engine_fwriteTrace ( Engine_Handle  engine,
String  prefix,
FILE *  out 
)

Write Server's trace buffer to specifed file stream.

Parameters:
[in]engineThe handle to the opened engine.
[in]prefixA string to prepend to each line output; this allows one to easily identify trace from the server from the application's trace, for example.
[in]outA open FILE stream used to output the Server's trace characters.
Return values:
Integernumber of characters copied to the specified FILE stream.
Precondition:
engine is a valid (non-NULL) engine handle and the engine is in the open state.
Postcondition:
In the event a negative value is returned, Engine_getLastError() will return one of the following values:
  • Engine_ERUNTIME Either an internal runtime error occured or the underlying server error occured.
  • Engine_EINUSE Server trace resource is already in use.
Engine_Error Engine_getAlgInfo ( String  name,
Engine_AlgInfo algInfo,
Int  index 
)

Get details of an algorithm configured into an engine.

Parameters:
[in]nameThe name of the engine. name is specified in the engine configuration.
[out]algInfoStructure to store algorithm details. The algInfoSize field of this structure must be set to sizeof(Engine_AlgInfo) by the application.
[out]indexThe index of the algorithm to get the information.
Return values:
Engine_EOKSuccess.
Engine_EEXISTThere is no engine with the given name.
Engine_ENOTFOUNDindex is greater than or equal to the total number of algorithms configured for the engine, or index < 0.
Engine_EINVALThe value of algInfoSize passed to this function does not match the CE library's sizeof(Engine_AlgInfo).
Precondition:
name is a non-NULL string.
algInfo is non-NULL.
As with all Codec Engine API's, CERuntime_init() must have previously been called.
Postcondition:
If name is a valid engine name and 0 <= index < the total number of algorithms configured for the engine, then algInfo will contain the information for the engine's ith (i = index) algorithm.
See also:
Engine_getNumAlgs()
Engine_Error Engine_getAlgInfo2 ( String  name,
Engine_Handle  engine,
Engine_AlgInfo2 algInfo2,
Int  index 
)

Get details of an algorithm.

Parameters:
[in]nameThe name of the engine. name is specified in the engine configuration. This may be NULL if engine contains a valid engine handle.
[in]engineThe handle of an engine returned by Engine_open(). If this is NULL, only information for a static alg can be obtained.
[out]algInfo2Structure to store algorithm details. The algInfoSize field of this structure must be set to sizeof(Engine_AlgInfo2) by the application.
[out]indexThe index of the algorithm to get the information.
Return values:
Engine_EOKSuccess.
Engine_EEXISTThere is no engine with the given name.
Engine_ENOTFOUNDindex is greater than or equal to the total number of algorithms configured for the engine, or index < 0.
Engine_EINVALThe value of algInfoSize passed to this function does not match the CE library's sizeof(Engine_AlgInfo2).
Precondition:
name is a non-NULL string or engine is non-NULL.
algInfo2 is non-NULL.
As with all Codec Engine API's, CERuntime_init() must have previously been called.
Postcondition:
If name is a valid engine name and 0 <= index < the total number of algorithms configured for the engine, then algInfo2 will contain the information for the engine's ith (i = index) algorithm.
Remarks:
This service supports algorithms statically configured into an Engine at build/config time, or algorithms that have been dynamically added to an opened engine. If the Engine has not been opened yet, the name of the Engine is used to get the statically configured alg. If the Engine has been opened, the Engine handle can be used to get either information for a statically configured alg, or a remote alg that was added when the server was queried during Engine_open().
See also:
Engine_getNumAlgs2().
Engine_Error Engine_getDesc ( String  name,
Engine_Desc desc 
)

Fill in an Engine_Desc structure with the values of the Engine descriptor for an Engine.

Parameters:
[in]nameThe name of the Engine. name is specified in the engine configuration or a a name that was passed to Engine_add().
[out]descThe structure where the descriptor of the Engine specified by name will be copied to.
Return values:
Engine_EOKSuccess.
Engine_EEXISTThere is no engine with the given name.
Precondition:
name is a non-NULL string.
desc is non-NULL.
As with all Codec Engine API's, CERuntime_init() must have previously been called.
Postcondition:
If name is a valid engine name, then desc will contain the descriptor of the engine name.
See also:
Engine_setDesc().
Engine_Error Engine_getLastError ( Engine_Handle  engine )

Get error code of the last failed operation.

Parameters:
[in]engineThe handle to the opened engine.
Return values:
errorcode (Engine_Error) of the last failed engine operation.
Precondition:
As with all Codec Engine API's, CERuntime_init() must have previously been called.
engine is a valid (non-NULL) engine handle and the engine is in the open state.
String Engine_getName ( Engine_Handle  engine )

Get the name of an opened engine.

Parameters:
[in]engineThe handle to the opened engine.
Precondition:
As with all Codec Engine API's, CERuntime_init() must have previously been called.
Return values:
NULLAn error has occurred.
non-NULLThe name of the opened engine.
Engine_Error Engine_getNumAlgs ( String  name,
Int *  numAlgs 
)

Get the number of algorithms configured into an Engine.

Parameters:
[in]nameThe name of the Engine. name is specified in the engine configuration.
[out]numAlgsThe number of algorithms that are configured in the given engine.
Return values:
Engine_EOKSuccess.
Engine_EEXISTThere is no engine with the given name.
Precondition:
name is a non-NULL string.
numAlgs is non-NULL.
As with all Codec Engine API's, CERuntime_init() must have previously been called.
Postcondition:
If name is a valid engine name, then numAlgs will contain the number of algorithms configured for the given engine.
See also:
Engine_getAlgs().
Engine_Error Engine_getNumAlgs2 ( String  name,
Engine_Handle  engine,
Int *  numAlgs 
)

Get the number of algorithms statically configured into an engine or the total number of algorithms both statically configured and dynamically added through server information when the engine was opened.

Parameters:
[in]nameThe name of the engine. name is specified in the engine configuration. name can be NULL, if engine is a valid Engine_Handle.
[in]engineThe handle of an engine returned by Engine_open(). If engine is NULL, name must be non-NULL, and only the number of statically configured algorithms will be returned in numAlgs. specified in the engine configuration.
[out]numAlgsThe number of algorithms that are configured in the given engine.
Return values:
Engine_EOKSuccess.
Engine_EEXISTThere is no engine with the given name.
Precondition:
name is a non-NULL string or engine is non-NULL.
numAlgs is non-NULL.
As with all Codec Engine API's, CERuntime_init() must have previously been called.
Postcondition:
If name is a valid engine name, then numAlgs will contain the number of algorithms configured for the given engine.
Remarks:
If the engine has a server, but was not configured with Engine.createFromServer() number of remote algorithms (if any) that were statically configured into the engine, will be counted twice: once for the static alg table, and once for the information queried from the server.
See also:
Engine_getAlgs().
Server_Handle Engine_getServer ( Engine_Handle  engine )

Get handle to an Engine's Server.

This function returns the handle to an Engines server, that can be used with Server APIs to obtain information from and control the remote DSP server.

Parameters:
[in]engineThe handle to the opened engine.
Return values:
Handleto engine's server.
Precondition:
As with all Codec Engine API's, CERuntime_init() must have previously been called.
engine is a valid (non-NULL) engine handle and the engine is in the open state.
UInt32 Engine_getUsedMem ( Engine_Handle  engine )

Get Server's total memory usage.

Deprecated:
This service has been replaced by Server_getMemStat() to better indicate that this API is not intended for obtaining the current processor's memory statistics, rather it obtains the memory statistics of a remote Server. Also, Server_getMemStat() provides more granularity than Engine_getUsedMem().
Parameters:
[in]engineThe handle to the opened engine.
Return values:
Totalamount of used memory (in MAUs). If the amount is not available, 0 is returned and the reason can be retrieved via Engine_getLastError().
Precondition:
As with all Codec Engine API's, CERuntime_init() must have previously been called.
engine is a valid (non-NULL) engine handle and the engine is in the open state.
Postcondition:
in the event that 0 is returned, Engine_getLastError() will return one of the following values:
Engine_Error Engine_remove ( String  engineName )

Remove an engine from the list of engines that can be opened.

Parameters:
[in]engineNameThe name of the engine to be removed.
Precondition:
As with all Codec Engine API's, CERuntime_init() must have previously been called.
engineName is non-NULL.
Return values:
Engine_EINUSEThe engine cannot be removed because an instance of it is still opened.
Engine_EEXISTNo engine by this name exists.
Engine_EOKSuccess.
See also:
Engine_add()
Engine_Error Engine_setDesc ( String  name,
Engine_Desc desc 
)

Set values for an Engine's descriptor. This function should only be called when the Engine has not yet been opened.

Parameters:
[in]nameThe name of the Engine. name is specified in the engine configuration or a a name that was passed to Engine_add().
[in]descThe structure where descriptor values for the Engine specified by name will be copied from.
Return values:
Engine_EOKSuccess.
Engine_EEXISTThere is no engine with the given name.
Engine_EINUSEThe Engine name has already been opened.
Precondition:
name is a non-NULL string.
desc is non-NULL.
As with all Codec Engine API's, CERuntime_init() must have previously been called.
Postcondition:
If name is a valid engine name, then the desscriptor for the engine name will have been updated with values from desc.
Remarks:
Use Engine_getDesc() to fill in the descriptor, override the fields you want to change, and then pass the descriptor to Engine_setDesc(). Only the following fields of the Engine_Desc are allowed to be modified: memMap useExtLoader heapId
See also:
Engine_getDesc().
Int Engine_setTrace ( Engine_Handle  engine,
String  mask 
)

Set Server's trace mask.

Parameters:
[in]engineThe handle to the opened engine.
[in]maskTrace mask, e.g. "*=01234567"
Return values:
Engine_ENOSERVERNo server for this engine.
Engine_EINUSETrace resource is already in use.
Engine_ERUNTIMEInternal runtime error has occurred.
Precondition:
As with all Codec Engine API's, CERuntime_init() must have previously been called.
engine is a valid (non-NULL) engine handle and the engine is in the open state.
Remarks:
This only sets the trace for a remote server. To change the trace mask for the application-side of the framework, use Diags_setMask(), or Diags_setMaskMeta().
See also:
xdc.runtime.Diags

Variable Documentation

Default engine attributes.

Deprecated:
Engine_ATTRS is no longer recommended. Please use Engine_initAttrs() instead.
See also:
Engine_initAttrs() Default attrs.
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated