Data Structures | Defines | Typedefs

IVIDTRANSCODE - XDM Video Transcoder Interface

Data Structures

struct  IVIDTRANSCODE_Obj
 This must be the first field of all IVIDTRANSCODE instance objects. More...
struct  IVIDTRANSCODE_Params
 Defines the creation time parameters for all IVIDTRANSCODE instance objects. More...
struct  IVIDTRANSCODE_DynamicParams
 This structure defines the codec parameters that can be modified after creation via control() calls. More...
struct  IVIDTRANSCODE_InArgs
 Defines the input arguments for all IVIDTRANSCODE instance process function. More...
struct  IVIDTRANSCODE_Status
 Defines instance status parameters. More...
struct  IVIDTRANSCODE_OutArgs
 Defines the run time output arguments for all IVIDTRANSCODE instance objects. More...
struct  IVIDTRANSCODE_Fxns
 Defines all of the operations on IVIDTRANSCODE objects. More...

Defines

#define IVIDTRANSCODE_EOK   XDM_EOK
#define IVIDTRANSCODE_EFAIL   XDM_EFAIL
#define IVIDTRANSCODE_EUNSUPPORTED   XDM_EUNSUPPORTED
#define IVIDTRANSCODE_MAXOUTSTREAMS   2

Typedefs

typedef struct IVIDTRANSCODE_Obj IVIDTRANSCODE_Obj
 This must be the first field of all IVIDTRANSCODE instance objects.
typedef struct IVIDTRANSCODE_ObjIVIDTRANSCODE_Handle
 Opaque handle to an IVIDTRANSCODE objects.
typedef struct IVIDTRANSCODE_Params IVIDTRANSCODE_Params
 Defines the creation time parameters for all IVIDTRANSCODE instance objects.
typedef struct
IVIDTRANSCODE_DynamicParams 
IVIDTRANSCODE_DynamicParams
 This structure defines the codec parameters that can be modified after creation via control() calls.
typedef struct IVIDTRANSCODE_InArgs IVIDTRANSCODE_InArgs
 Defines the input arguments for all IVIDTRANSCODE instance process function.
typedef struct IVIDTRANSCODE_Status IVIDTRANSCODE_Status
 Defines instance status parameters.
typedef struct
IVIDTRANSCODE_OutArgs 
IVIDTRANSCODE_OutArgs
 Defines the run time output arguments for all IVIDTRANSCODE instance objects.
typedef IALG_Cmd IVIDTRANSCODE_Cmd
 Defines the control commands for the IVIDTRANSCODE module.
typedef struct IVIDTRANSCODE_Fxns IVIDTRANSCODE_Fxns
 Defines all of the operations on IVIDTRANSCODE objects.

Detailed Description

This is the XDM IVIDENC2 Video Transcoder Interface.


Define Documentation

#define IVIDTRANSCODE_EOK   XDM_EOK

Success.

#define IVIDTRANSCODE_EFAIL   XDM_EFAIL

General failure.

#define IVIDTRANSCODE_EUNSUPPORTED   XDM_EUNSUPPORTED

Request is unsupported.

#define IVIDTRANSCODE_MAXOUTSTREAMS   2
Todo:
Document this.

Typedef Documentation

This must be the first field of all IVIDTRANSCODE instance objects.

Opaque handle to an IVIDTRANSCODE objects.

Defines the creation time parameters for all IVIDTRANSCODE instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.

This structure defines the codec parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that a given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDTRANSCODE_Fxns::control()

Defines the input arguments for all IVIDTRANSCODE instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDTRANSCODE_Fxns::process()

Defines instance status parameters.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDTRANSCODE_Fxns::control()

Defines the run time output arguments for all IVIDTRANSCODE instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDTRANSCODE_Fxns::process()

Defines the control commands for the IVIDTRANSCODE module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId
IVIDTRANSCODE_Fxns::control()

Defines all of the operations on IVIDTRANSCODE objects.

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated