Data Structures | Defines | Typedefs | Enumerations

IVIDDEC2 - XDM Video Decoder Interface

Data Structures

struct  IVIDDEC2_Obj
 This must be the first field of all IVIDDEC2 instance objects. More...
struct  IVIDDEC2_Params
 Defines the creation time parameters for all IVIDDEC2 instance objects. More...
struct  IVIDDEC2_DynamicParams
 This structure defines the codec parameters that can be modified after creation via control() calls. More...
struct  IVIDDEC2_InArgs
 Defines the input arguments for all IVIDDEC2 instance process function. More...
struct  IVIDDEC2_Status
 Defines instance status parameters. More...
struct  IVIDDEC2_OutArgs
 Defines the run time output arguments for all IVIDDEC2 instance objects. More...
struct  IVIDDEC2_Fxns
 Defines all of the operations on IVIDDEC2 objects. More...

Defines

#define IVIDDEC2_MAX_IO_BUFFERS   IVIDEO2_MAX_IO_BUFFERS
 Maximum I/O Buffers.
#define IVIDDEC2_EOK   XDM_EOK
#define IVIDDEC2_EFAIL   XDM_EFAIL
#define IVIDDEC2_EUNSUPPORTED   XDM_EUNSUPPORTED

Typedefs

typedef struct IVIDDEC2_Obj IVIDDEC2_Obj
 This must be the first field of all IVIDDEC2 instance objects.
typedef struct IVIDDEC2_ObjIVIDDEC2_Handle
 Opaque handle to an IVIDDEC2 objects.
typedef struct IVIDDEC2_Params IVIDDEC2_Params
 Defines the creation time parameters for all IVIDDEC2 instance objects.
typedef struct
IVIDDEC2_DynamicParams 
IVIDDEC2_DynamicParams
 This structure defines the codec parameters that can be modified after creation via control() calls.
typedef struct IVIDDEC2_InArgs IVIDDEC2_InArgs
 Defines the input arguments for all IVIDDEC2 instance process function.
typedef struct IVIDDEC2_Status IVIDDEC2_Status
 Defines instance status parameters.
typedef struct IVIDDEC2_OutArgs IVIDDEC2_OutArgs
 Defines the run time output arguments for all IVIDDEC2 instance objects.
typedef IALG_Cmd IVIDDEC2_Cmd
 Defines the control commands for the IVIDDEC2 module.
typedef struct IVIDDEC2_Fxns IVIDDEC2_Fxns
 Defines all of the operations on IVIDDEC2 objects.

Enumerations

enum  IVIDDEC2_FrameOrder {
  IVIDDEC2_DISPLAY_ORDER = 0,
  IVIDDEC2_DECODE_ORDER = 1,
  IVIDDEC2_FRAMEORDER_DEFAULT = IVIDDEC2_DISPLAY_ORDER
}
 

Video decoder output frame order.

More...

Detailed Description

This is the XDM IVIDDEC2 Video Decoder Interface.


Define Documentation

#define IVIDDEC2_MAX_IO_BUFFERS   IVIDEO2_MAX_IO_BUFFERS

Maximum I/O Buffers.

Remarks:
This IVIDDEC2-specific definition has been replaced with IVIDEO2_MAX_IO_BUFFERS. It has been kept for backward compatibility, but users are encouraged to use IVIDEO2_MAX_IO_BUFFERS instead.
See also:
IVIDEO2_MAX_IO_BUFFERS
#define IVIDDEC2_EOK   XDM_EOK

Success.

#define IVIDDEC2_EFAIL   XDM_EFAIL

General failure.

#define IVIDDEC2_EUNSUPPORTED   XDM_EUNSUPPORTED

Request is unsupported.


Typedef Documentation

typedef struct IVIDDEC2_Obj IVIDDEC2_Obj

This must be the first field of all IVIDDEC2 instance objects.

typedef struct IVIDDEC2_Obj* IVIDDEC2_Handle

Opaque handle to an IVIDDEC2 objects.

Defines the creation time parameters for all IVIDDEC2 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.

This structure defines the codec parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that a given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC2_Fxns::control()

Defines the input arguments for all IVIDDEC2 instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC2_Fxns::process()

Defines instance status parameters.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
All fields correspond to latest IVIDDEC2_Fxns::process() call on the particular instance of the decoder.
See also:
IVIDDEC2_Fxns::control()

Defines the run time output arguments for all IVIDDEC2 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC2_Fxns::process()

Defines the control commands for the IVIDDEC2 module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId
IVIDDEC2_Fxns::control()
typedef struct IVIDDEC2_Fxns IVIDDEC2_Fxns

Defines all of the operations on IVIDDEC2 objects.


Enumeration Type Documentation

Video decoder output frame order.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
See also:
IVIDDEC2_DynamicParams::frameOrder
Enumerator:
IVIDDEC2_DISPLAY_ORDER 

The decoder provides decoded output in in the actual order of displaying the output buffer. The codec assumes the responsibility of reordering the frames.

Remarks:
The output buffer will be delayed by one frame, regardless of whether the frame contains I/P or I/P/B frames.
This is the default mode.
This mode is required to be supported by all video decoder codecs.
IVIDDEC2_DECODE_ORDER 

The decoder provides decoded output in the the order of decoding. There will be no delay in the output buffers.

Remarks:
It is the application's responsibility to handle the frame re-ordering.
This mode is optional. If it is not supported by the decoder, IVIDDEC_EUNSUPPORTED will be returned.
IVIDDEC2_FRAMEORDER_DEFAULT 

Default setting.

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated