Data Structures | Typedefs | Functions

VIDDEC2FRONT/VIDDEC2BACK - Split video decoder interface

Data Structures

struct  IVIDDEC2BACK_CodecClassConfig
 Definition of IVIDDEC2BACK codec class configurable parameters. More...

Typedefs

typedef IVIDDEC2FRONT_Status VIDDEC2FRONT_Status
typedef VISA_Handle VIDDEC2FRONT_Handle
 Opaque handle to a VIDDEC2FRONT codec.
typedef VISA_Handle VIDDEC2BACK_Handle
 Opaque handle to a VIDDEC2BACK codec.
typedef IVIDDEC2FRONT_OutArgs VIDDEC2FRONT_OutArgs
typedef struct
IVIDDEC2BACK_CodecClassConfig 
IVIDDEC2BACK_CodecClassConfig
 Definition of IVIDDEC2BACK codec class configurable parameters.

Functions

VIDDEC2BACK_Handle VIDDEC2BACK_create (Engine_Handle e, String name, VIDDEC2_Params *params)
 Create an instance of the BACK end of a split video decoder algorithm.
Int32 VIDDEC2BACK_process (VIDDEC2BACK_Handle handle, XDM_Context *context, VIDDEC2_OutArgs *outArgs)
 Execute the process() method in this instance of a BACK side split video decoder algorithm.
Int32 VIDDEC2BACK_control (VIDDEC2BACK_Handle handle, XDM_Context *context, VIDDEC2_Status *status)
 Execute the control() method in this instance of a video decoder algorithm.
Void VIDDEC2BACK_delete (VIDDEC2BACK_Handle handle)
 Delete the instance of a video decoder algorithm.
VIDDEC2FRONT_Handle VIDDEC2FRONT_create (Engine_Handle e, String name, VIDDEC2_Params *params)
 Create an instance of the FRONT end of a split video decoder algorithm.
Int32 VIDDEC2FRONT_process (VIDDEC2FRONT_Handle handle, VIDDEC2_InArgs *inArgs, XDM_Context *context, VIDDEC2FRONT_OutArgs *outArgs)
 Execute the process() method in this instance of a FRONT side split video decoder algorithm.
Int32 VIDDEC2FRONT_control (VIDDEC2FRONT_Handle handle, VIDDEC2_Cmd id, VIDDEC2_DynamicParams *params, XDM_Context *context, VIDDEC2FRONT_Status *status)
 Execute the control() method in this instance of a video decoder algorithm.
Void VIDDEC2FRONT_delete (VIDDEC2FRONT_Handle handle)
 Delete the instance of a video decoder algorithm.

Detailed Description

This is the split VIDDEC2 video decoder interface. Several of the data types in this API are specified by the XDM interface; please see the XDM documentation for those details.


Typedef Documentation

Defines instance status parameters.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
All fields correspond to latest IVIDDEC2_Fxns::process() call on the particular instance of the decoder.
See also:
IVIDDEC2_Fxns::control()

Opaque handle to a VIDDEC2FRONT codec.

Opaque handle to a VIDDEC2BACK codec.

Defines the run time output arguments for all IVIDDEC2FRONT instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC2FRONT_Fxns::process()

Definition of IVIDDEC2BACK codec class configurable parameters.


Function Documentation

VIDDEC2BACK_Handle VIDDEC2BACK_create ( Engine_Handle  e,
String  name,
VIDDEC2_Params params 
)

Create an instance of the BACK end of a split video decoder algorithm.

Instance handles must not be concurrently accessed by multiple threads; each thread must either obtain its own handle (via VIDDEC2BACK_create) or explicitly serialize access to a shared handle.

Parameters:
[in]eHandle to an opened engine.
[in]nameString identifier of the type of video decoder to create.
[in]paramsCreation parameters.
Return values:
NULLAn error has occurred.
non-NULLThe handle to the newly created video decoder instance.
Remarks:
Depending on the configuration of the engine opened, this call may create a local or remote instance of the video decoder.
In general, name is the name of the codec configured by the system integrator. However, an optional "argument string" may be appended to the codec name, to allow the codec's configured priority and/or the heaps where its memory will be allocated, to be overridden. This optional argument string is of the form ":priority", ":priority:flag", or "::flag".
priority is the new priority to create the codec with.
The flag must be either 0 or 1, and if 1, all memory allocated for the codec will be in the heap that corresponds to IALG_EXTERNAL. If flag is 0, the memory for the codec will be allocated from the heaps it has requested. For example, if a codec named "mp3" has been configured into the system, setting name to "mp3:4" would cause the codec to be created at priority 4, instead of whatever priority was configured. This feature is useful if more than one instance of the codec are to be created at different priorities.
The flag can be used to prevent the codec from using any internal memory, for example, if it is to be run at the same time as another codec that must use internal memory, and there is insufficient internal memory for both.
See also:
Engine_open()
Int32 VIDDEC2BACK_process ( VIDDEC2BACK_Handle  handle,
XDM_Context context,
VIDDEC2_OutArgs outArgs 
)

Execute the process() method in this instance of a BACK side split video decoder algorithm.

Parameters:
[in]handleHandle to a created video decoder instance.
[in,out]contextContext provided to, and managed by, the split codec.
[out]outArgsOutput results. This is a required parameter
Precondition:
handle is a valid (non-NULL) video decoder handle and the video decoder is in the created state.
Return values:
VIDDEC2_EOKSuccess.
VIDDEC2_EFAILFailure.
Remarks:
Since the VIDDEC2BACK decoder contains support for asynchronous buffer submission and retrieval, this API becomes known as synchronous in nature.
This is a blocking call, and will return after the data has been decoded.
The buffers supplied to VIDDEC2BACK_process() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
See also:
VIDDEC2BACK_create()
VIDDEC2BACK_delete()
VIDDEC2BACK_control()
VIDDEC2BACK_processAsync()
VIDDEC2BACK_processWait()
IVIDDEC2BACK_Fxns::process()
VIDDEC2FRONT_create()
VIDDEC2FRONT_delete()
VIDDEC2FRONT_control()
IVIDDEC2FRONT_Fxns::process()
Int32 VIDDEC2BACK_control ( VIDDEC2BACK_Handle  handle,
XDM_Context context,
VIDDEC2_Status status 
)

Execute the control() method in this instance of a video decoder algorithm.

Parameters:
[in]handleHandle to a created video decoder instance.
[in,out]contextContext provided to, and managed by, the split codec.
[out]statusStatus info upon completion of decode operation.
Precondition:
handle is a valid (non-NULL) video decoder handle and the video decoder is in the created state.
Return values:
VIDDEC2_EOKSuccess.
VIDDEC2_EFAILFailure.
Remarks:
This is a blocking call, and will return after the control command has been executed.
See also:
VIDDEC2FRONT_create()
VIDDEC2FRONT_delete()
IVIDDEC2FRONT_Fxns::process()
VIDDEC2BACK_create()
VIDDEC2BACK_delete()
IVIDDEC2BACK_Fxns::process()
Void VIDDEC2BACK_delete ( VIDDEC2BACK_Handle  handle )

Delete the instance of a video decoder algorithm.

Parameters:
[in]handleHandle to a created video decoder instance.
Remarks:
Depending on the configuration of the engine opened, this call may delete a local or remote instance of the video decoder.
Precondition:
handle is a valid (non-NULL) handle which is in the created state.
Postcondition:
All resources allocated as part of the VIDDEC2BACK_create() operation (memory, DMA channels, etc.) are freed.
See also:
VIDDEC2BACK_create()
VIDDEC2FRONT_Handle VIDDEC2FRONT_create ( Engine_Handle  e,
String  name,
VIDDEC2_Params params 
)

Create an instance of the FRONT end of a split video decoder algorithm.

Instance handles must not be concurrently accessed by multiple threads; each thread must either obtain its own handle (via VIDDEC2FRONT_create) or explicitly serialize access to a shared handle.

Parameters:
[in]eHandle to an opened engine.
[in]nameString identifier of the type of video decoder to create.
[in]paramsCreation parameters.
Return values:
NULLAn error has occurred.
non-NULLThe handle to the newly created video decoder instance.
Remarks:
Depending on the configuration of the engine opened, this call may create a local or remote instance of the video decoder.
In general, name is the name of the codec configured by the system integrator. However, an optional "argument string" may be appended to the codec name, to allow the codec's configured priority and/or the heaps where its memory will be allocated, to be overridden. This optional argument string is of the form ":priority", ":priority:flag", or "::flag".
priority is the new priority to create the codec with.
The flag must be either 0 or 1, and if 1, all memory allocated for the codec will be in the heap that corresponds to IALG_EXTERNAL. If flag is 0, the memory for the codec will be allocated from the heaps it has requested. For example, if a codec named "mp3" has been configured into the system, setting name to "mp3:4" would cause the codec to be created at priority 4, instead of whatever priority was configured. This feature is useful if more than one instance of the codec are to be created at different priorities.
The flag can be used to prevent the codec from using any internal memory, for example, if it is to be run at the same time as another codec that must use internal memory, and there is insufficient internal memory for both.
See also:
Engine_open()
Int32 VIDDEC2FRONT_process ( VIDDEC2FRONT_Handle  handle,
VIDDEC2_InArgs inArgs,
XDM_Context context,
VIDDEC2FRONT_OutArgs outArgs 
)

Execute the process() method in this instance of a FRONT side split video decoder algorithm.

Parameters:
[in]handleHandle to a created video decoder instance.
[in]inArgsInput Arguments.
[in,out]contextContext provided to, and managed by, the split codec.
[out]outArgsOutput results. This is a required parameter
Precondition:
handle is a valid (non-NULL) video decoder handle and the video decoder is in the created state.
Return values:
VIDDEC2_EOKSuccess.
VIDDEC2_EFAILFailure.
Remarks:
Since the VIDDEC2FRONT decoder contains support for asynchronous buffer submission and retrieval, this API becomes known as synchronous in nature.
This is a blocking call, and will return after the data has been decoded.
The buffers supplied to VIDDEC2FRONT_process() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
See also:
VIDDEC2FRONT_create()
VIDDEC2FRONT_delete()
VIDDEC2FRONT_control()
IVIDDEC2FRONT_Fxns::process()
VIDDEC2BACK_create()
VIDDEC2BACK_delete()
VIDDEC2BACK_control()
VIDDEC2BACK_processAsync()
VIDDEC2BACK_processWait()
IVIDDEC2BACK_Fxns::process()
Int32 VIDDEC2FRONT_control ( VIDDEC2FRONT_Handle  handle,
VIDDEC2_Cmd  id,
VIDDEC2_DynamicParams params,
XDM_Context context,
VIDDEC2FRONT_Status status 
)

Execute the control() method in this instance of a video decoder algorithm.

Parameters:
[in]handleHandle to a created video decoder instance.
[in]idCommand id for xDM control operation.
[in]paramsRuntime control parameters used for decoding.
[in,out]contextContext provided to, and managed by, the split codec.
[out]statusStatus info upon completion of decode operation.
Precondition:
handle is a valid (non-NULL) video decoder handle and the video decoder is in the created state.
Return values:
VIDDEC2_EOKSuccess.
VIDDEC2_EFAILFailure.
Remarks:
This is a blocking call, and will return after the control command has been executed.
See also:
VIDDEC2FRONT_create()
VIDDEC2FRONT_delete()
IVIDDEC2FRONT_Fxns::process()
VIDDEC2BACK_create()
VIDDEC2BACK_delete()
IVIDDEC2BACK_Fxns::process()
Void VIDDEC2FRONT_delete ( VIDDEC2FRONT_Handle  handle )

Delete the instance of a video decoder algorithm.

Parameters:
[in]handleHandle to a created video decoder instance.
Remarks:
Depending on the configuration of the engine opened, this call may delete a local or remote instance of the video decoder.
Precondition:
handle is a valid (non-NULL) handle which is in the created state.
Postcondition:
All resources allocated as part of the VIDDEC2FRONT_create() operation (memory, DMA channels, etc.) are freed.
See also:
VIDDEC2FRONT_create()
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated