Detailed Description
The TraceUtil module provides services to manage trace output.
Define Documentation
#define TRACEUTIL_SUCCESS 0 |
#define TRACEUTIL_FAILURE -1 |
Function Documentation
Int TraceUtil_start |
( |
String |
engineName ) |
|
Begin using the TraceUtil module; create thread that periodically collects DSP trace.
- Parameters:
-
[in] | engineName | Name of the engine. This uses the same name conventions as Engine_open()'s name. |
- Return values:
-
TRACEUTIL_SUCCESS | Success. |
TRACEUTIL_FAILURE | Failed to initialize the necessary tracing resources. |
- See also:
- TraceUtil_stop()
Int TraceUtil_stop |
( |
Void |
) |
|
Finish using the TraceUtil module, stop the collecting thread.
- Return values:
-
TRACEUTIL_SUCCESS | Success. |
TRACEUTIL_FAILURE | Failed to free the necessary tracing resources. |
- See also:
- TraceUtil_start()