![]() |
![]() |
Defines the input arguments for all IAUDDEC1 instance process function. More...
#include <iauddec1.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | numBytes |
XDAS_Int32 | desiredChannelMode |
XDAS_Int32 | lfeFlag |
Defines the input arguments for all IAUDDEC1 instance process function.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Size of input data in bytes, provided to the algorithm for decoding.
Desired Channel Configuration.
Flag indicating whether LFE channel data is desired in the output.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.