![]() |
![]() |
Data Structures | |
struct | IAUDDEC1_Obj |
This must be the first field of all IAUDDEC1 instance objects. More... | |
struct | IAUDDEC1_Params |
Defines the creation time parameters for all IAUDDEC1 instance objects. More... | |
struct | IAUDDEC1_DynamicParams |
This structure defines the codec parameters that can be modified after creation via control() calls. More... | |
struct | IAUDDEC1_InArgs |
Defines the input arguments for all IAUDDEC1 instance process function. More... | |
struct | IAUDDEC1_Status |
Defines instance status parameters (read-only). More... | |
struct | IAUDDEC1_OutArgs |
Defines the run time output arguments for all IAUDDEC1 instance objects. More... | |
struct | IAUDDEC1_Fxns |
Defines all of the operations on IAUDDEC1 objects. More... | |
Defines | |
#define | IAUDDEC1_EOK XDM_EOK |
#define | IAUDDEC1_EFAIL XDM_EFAIL |
#define | IAUDDEC1_EUNSUPPORTED XDM_EUNSUPPORTED |
Typedefs | |
typedef struct IAUDDEC1_Obj | IAUDDEC1_Obj |
This must be the first field of all IAUDDEC1 instance objects. | |
typedef struct IAUDDEC1_Obj * | IAUDDEC1_Handle |
Opaque handle to an IAUDDEC1 objects. | |
typedef struct IAUDDEC1_Params | IAUDDEC1_Params |
Defines the creation time parameters for all IAUDDEC1 instance objects. | |
typedef struct IAUDDEC1_DynamicParams | IAUDDEC1_DynamicParams |
This structure defines the codec parameters that can be modified after creation via control() calls. | |
typedef struct IAUDDEC1_InArgs | IAUDDEC1_InArgs |
Defines the input arguments for all IAUDDEC1 instance process function. | |
typedef struct IAUDDEC1_Status | IAUDDEC1_Status |
Defines instance status parameters (read-only). | |
typedef struct IAUDDEC1_OutArgs | IAUDDEC1_OutArgs |
Defines the run time output arguments for all IAUDDEC1 instance objects. | |
typedef IALG_Cmd | IAUDDEC1_Cmd |
Defines the control commands for the IAUDDEC1 module. | |
typedef struct IAUDDEC1_Fxns | IAUDDEC1_Fxns |
Defines all of the operations on IAUDDEC1 objects. |
This is the XDM IAUDDEC1 Audio Decoder Interface.
#define IAUDDEC1_EOK XDM_EOK |
Success.
#define IAUDDEC1_EFAIL XDM_EFAIL |
General failure.
#define IAUDDEC1_EUNSUPPORTED XDM_EUNSUPPORTED |
Request is unsupported.
typedef struct IAUDDEC1_Obj IAUDDEC1_Obj |
This must be the first field of all IAUDDEC1 instance objects.
typedef struct IAUDDEC1_Obj* IAUDDEC1_Handle |
Opaque handle to an IAUDDEC1 objects.
typedef struct IAUDDEC1_Params IAUDDEC1_Params |
Defines the creation time parameters for all IAUDDEC1 instance objects.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details. typedef struct IAUDDEC1_DynamicParams IAUDDEC1_DynamicParams |
This structure defines the codec parameters that can be modified after creation via control() calls.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.typedef struct IAUDDEC1_InArgs IAUDDEC1_InArgs |
Defines the input arguments for all IAUDDEC1 instance process function.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.typedef struct IAUDDEC1_Status IAUDDEC1_Status |
Defines instance status parameters (read-only).
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.typedef struct IAUDDEC1_OutArgs IAUDDEC1_OutArgs |
Defines the run time output arguments for all IAUDDEC1 instance objects.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.typedef IALG_Cmd IAUDDEC1_Cmd |
Defines the control commands for the IAUDDEC1 module.
typedef struct IAUDDEC1_Fxns IAUDDEC1_Fxns |
Defines all of the operations on IAUDDEC1 objects.