Data Structures | Defines | Typedefs | Functions

VIDDEC3 - Video Decoder Interface

Data Structures

struct  IVIDDEC3_CodecClassConfig
 Definition of IVIDDEC3 codec class configurable parameters. More...

Defines

#define VIDDEC3_EOK   IVIDDEC3_EOK
#define VIDDEC3_EFAIL   IVIDDEC3_EFAIL
#define VIDDEC3_EUNSUPPORTED   IVIDDEC3_EUNSUPPORTED
#define VIDDEC3_ETIMEOUT   VISA_ETIMEOUT
#define VIDDEC3_FOREVER   VISA_FOREVER

Typedefs

typedef VISA_Handle VIDDEC3_Handle
 Opaque handle to a VIDDEC3 codec.
typedef struct IVIDDEC3_Params VIDDEC3_Params
typedef IVIDDEC3_InArgs VIDDEC3_InArgs
typedef IVIDDEC3_OutArgs VIDDEC3_OutArgs
typedef IVIDDEC3_Cmd VIDDEC3_Cmd
typedef IVIDDEC3_DynamicParams VIDDEC3_DynamicParams
typedef IVIDDEC3_Status VIDDEC3_Status
typedef struct
IVIDDEC3_CodecClassConfig 
IVIDDEC3_CodecClassConfig
 Definition of IVIDDEC3 codec class configurable parameters.

Functions

Int32 VIDDEC3_control (VIDDEC3_Handle handle, VIDDEC3_Cmd id, VIDDEC3_DynamicParams *params, VIDDEC3_Status *status)
 Execute the control() method in this instance of a video decoder algorithm.
VIDDEC3_Handle VIDDEC3_create (Engine_Handle e, String name, VIDDEC3_Params *params)
 Create an instance of a video decoder algorithm.
Void VIDDEC3_delete (VIDDEC3_Handle handle)
 Delete the instance of a video decoder algorithm.
Int32 VIDDEC3_process (VIDDEC3_Handle handle, XDM2_BufDesc *inBufs, XDM2_BufDesc *outBufs, VIDDEC3_InArgs *inArgs, VIDDEC3_OutArgs *outArgs)
 Execute the process() method in this instance of a video decoder algorithm.

Detailed Description

This is the VIDDEC3 video decoder interface. Several of the data types in this API are specified by the XDM IVIDDEC3 interface; please see the XDM documentation for those details.


Define Documentation

#define VIDDEC3_EOK   IVIDDEC3_EOK

Success.

#define VIDDEC3_EFAIL   IVIDDEC3_EFAIL

General failure.

Request is unsupported.

#define VIDDEC3_EUNSUPPORTED   IVIDDEC3_EUNSUPPORTED
#define VIDDEC3_ETIMEOUT   VISA_ETIMEOUT

Timeout occurred.

#define VIDDEC3_FOREVER   VISA_FOREVER

Special value for timeout parameter indicating never timeout.


Typedef Documentation

Opaque handle to a VIDDEC3 codec.

Defines the creation time parameters for all IVIDDEC3 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.

Defines the input arguments for all IVIDDEC3 instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC3_Fxns::process()

Defines the run time output arguments for all IVIDDEC3 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
The size of this struct may vary when IVIDDEC3_OutArgs.displayBufsMode is set to IVIDDEC3_DISPLAYBUFS_EMBEDDED (see details in IVIDDEC3_OutArgs.displayBufs.bufDesc).
When IVIDDEC3_OutArgs.displayBufsMode is set to IVIDDEC3_DISPLAYBUFS_EMBEDDED, the number of elements in the IVIDDEC3_OutArgs.displayBufs.bufDesc array is a constant (and can be acquired by calling IVIDDEC3_Fxns.control() and looking in the IVIDDEC3_Status.maxOutArgsDisplayBufs field. Note that any extended fields follow the IVIDDEC3_OutArgs.displayBufs.bufDesc array.
See also:
IVIDDEC3_Fxns.process()

Defines the control commands for the IVIDDEC3 module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId
IVIDDEC3_Fxns::control()

This structure defines the algorithm parameters that can be modified after creation via IVIDDEC3_Fxns.control() calls.

Remarks:
It is not necessary that a given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC3_Fxns::control()

Defines instance status parameters.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC3_Fxns::control()

Definition of IVIDDEC3 codec class configurable parameters.

See also:
VISA_getCodecClassConfig()

Function Documentation

Int32 VIDDEC3_control ( VIDDEC3_Handle  handle,
VIDDEC3_Cmd  id,
VIDDEC3_DynamicParams params,
VIDDEC3_Status status 
)

Execute the control() method in this instance of a video decoder algorithm.

Parameters:
[in]handleHandle to a created video decoder instance.
[in]idCommand id for XDM control operation.
[in]paramsRuntime control parameters used for decoding.
[out]statusStatus info upon completion of decode operation.
Precondition:
handle is a valid (non-NULL) video decoder handle and the video decoder is in the created state.
Return values:
VIDDEC3_EOKSuccess.
VIDDEC3_EFAILFailure.
VIDDEC3_EUNSUPPORTEDUnsupported request.
Remarks:
This is a blocking call, and will return after the control command has been executed.
If an error is returned, status->extendedError may indicate further details about the error. See XDM_ErrorBit for details.
See also:
VIDDEC3_create()
VIDDEC3_delete()
IVIDDEC3_Fxns::process()
VIDDEC3_Handle VIDDEC3_create ( Engine_Handle  e,
String  name,
VIDDEC3_Params params 
)

Create an instance of a video decoder algorithm.

Instance handles must not be concurrently accessed by multiple threads; each thread must either obtain its own handle (via VIDDEC3_create) or explicitly serialize access to a shared handle.

Parameters:
[in]eHandle to an opened engine.
[in]nameString identifier of the type of video decoder to create.
[in]paramsCreation parameters.
Return values:
NULLAn error has occurred.
non-NULLThe handle to the newly created video decoder instance.
Remarks:
params is optional. If it's not supplied, codec-specific default params will be used.
Depending on the configuration of the engine opened, this call may create a local or remote instance of the video decoder.
In general, name is the name of the codec configured by the system integrator. However, an optional "argument string" may be appended to the codec name, to allow the codec's configured priority and/or the heaps where its memory will be allocated, to be overridden. This optional argument string is of the form ":priority", ":priority:flag", or "::flag".
priority is the new priority to create the codec with.
The flag must be either 0 or 1, and if 1, all memory allocated for the codec will be in the heap that corresponds to IALG_EXTERNAL. If flag is 0, the memory for the codec will be allocated from the heaps it has requested. For example, if a codec named "mp3" has been configured into the system, setting name to "mp3:4" would cause the codec to be created at priority 4, instead of whatever priority was configured. This feature is useful if more than one instance of the codec are to be created at different priorities.
The flag can be used to prevent the codec from using any internal memory, for example, if it is to be run at the same time as another codec that must use internal memory, and there is insufficient internal memory for both.
See also:
Engine_open()
VIDENC3_delete()
Void VIDDEC3_delete ( VIDDEC3_Handle  handle )

Delete the instance of a video decoder algorithm.

Parameters:
[in]handleHandle to a created video decoder instance.
Remarks:
Depending on the configuration of the engine opened, this call may delete a local or remote instance of the video decoder.
Precondition:
handle is a valid (non-NULL) handle which is in the created state.
Postcondition:
All resources allocated as part of the VIDDEC3_create() operation (memory, DMA channels, etc.) are freed.
See also:
VIDDEC3_create()
Int32 VIDDEC3_process ( VIDDEC3_Handle  handle,
XDM2_BufDesc inBufs,
XDM2_BufDesc outBufs,
VIDDEC3_InArgs inArgs,
VIDDEC3_OutArgs outArgs 
)

Execute the process() method in this instance of a video decoder algorithm.

Parameters:
[in]handleHandle to a created video decoder instance.
[in]inBufsA buffer descriptor containing input buffers.
[out]outBufsA buffer descriptor containing output buffers.
[in]inArgsInput Arguments.
[out]outArgsOutput Arguments.
Precondition:
handle is a valid (non-NULL) video decoder handle and the video decoder is in the created state.
Return values:
VIDDEC3_EOKSuccess.
VIDDEC3_EFAILFailure.
VIDDEC3_EUNSUPPORTEDUnsupported request.
Remarks:
Since the VIDDEC3 decoder contains support for asynchronous buffer submission and retrieval, this API becomes known as synchronous in nature.
This is a blocking call, and will return after the data has been decoded.
The buffers supplied to VIDDEC3_process() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
If an error is returned, outArgs->extendedError may indicate further details about the error. See XDM_ErrorBit for details.
See also:
VIDDEC3_create()
VIDDEC3_delete()
VIDDEC3_control()
VIDDEC3_processAsync()
VIDDEC3_processWait()
IVIDDEC3_Fxns::process()
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated