The Codec Engine System Programming Interface. Provides system developers with services necessary to implement stubs and skeletons.
#include <stddef.h>
#include <ti/sdo/ce/node/node.h>
#include <ti/xdais/ialg.h>
#include <ti/sdo/ce/Engine.h>
Go to the source code of this file.
Data Structures | |
struct | VISA_MsgHeader |
VISA message header. More... | |
Defines | |
#define | VISA_EOK 0 |
Success. | |
#define | VISA_ERUNTIME -1 |
Internal runtime error. | |
#define | VISA_EFAIL -2 |
General system error. | |
#define | VISA_ETIMEOUT -100 |
Timeout occurred. | |
#define | VISA_FOREVER Engine_FOREVER |
Special value for timeout parameter indicating never timeout. | |
#define | VISA_MODNAME "ti.sdo.ce.VISA" |
Name to pass to Diags_setMask() to enable logging for VISA functions. For example, Diags_setMask(VISA_MODNAME"+EX1234567"); turns on all Log statements in this module. Diags_setMask() must be called after initialization to take effect. | |
Typedefs | |
typedef Int | VISA_Status |
VISA result data type. | |
typedef struct VISA_Obj * | VISA_Handle |
Opaque handle to a node. | |
typedef struct VISA_MsgHeader | VISA_MsgHeader |
VISA message header. | |
typedef VISA_MsgHeader * | VISA_Msg |
Functions | |
VISA_Msg | VISA_allocMsg (VISA_Handle visa) |
Obtain an algorithm instance's message. | |
VISA_Status | VISA_call (VISA_Handle visa, VISA_Msg *msg) |
Invoke the operation specified in the message and wait for it to complete. | |
VISA_Status | VISA_callAsync (VISA_Handle visa, VISA_Msg *msg) |
Invoke the operation specified in the message and return without waiting for it to complete. | |
VISA_Status | VISA_wait (VISA_Handle visa, VISA_Msg *msg, UInt timeout) |
Wait for the oldest operation from a command specified with VISA_callAsync() to complete. | |
Void | VISA_freeMsg (VISA_Handle visa, VISA_Msg msg) |
Release an algorithm instance's message. | |
VISA_Status | VISA_getAlgMemRecs (VISA_Handle visa, IALG_MemRec *memTab, Int size, Int *numRecs) |
Get the IALG_MemRec memory assigned to an algorithm instance. | |
VISA_Status | VISA_getAlgNumRecs (VISA_Handle visa, Int *numRecs) |
Get the number of IALG_MemRecs assigned to an algorithm. | |
Void | VISA_getContext (VISA_Handle visa, UInt32 *pContext) |
Get optional context parameter. | |
Ptr | VISA_getCodecClassConfig (VISA_Handle visa) |
Get codec-specific values for the VISA class-specific (or codec-specific if the codec doesn't extend VISA) stub-and/ or-skeleton configuration data (that some classes have) | |
UInt | VISA_getMaxMsgSize (VISA_Handle visa) |
Returns max size of messages allocated by VISA_allocMsg() | |
Void | VISA_setContext (VISA_Handle visa, UInt32 context) |
Set optional context parameter. | |
Bool | VISA_isLocal (VISA_Handle visa) |
Indicates whether VISA codecs run on a remote or local CPU. | |
VISA_Handle | VISA_create (Engine_Handle engine, String name, IALG_Params *params, size_t msgSize, String type) |
Create a new instance of an algorithm. | |
Void | VISA_delete (VISA_Handle visa) |
Delete an instance of an algorithm. | |
VISA_Handle | VISA_create2 (Engine_Handle engine, String name, IALG_Params *params, Int paramsSize, size_t msgSize, String type) |
Create a new instance of an algorithm. | |
Void | VISA_enter (VISA_Handle visa) |
Enter an algorithm's critical section. This must be called before any of the algorithm's IALG_Fxns are invoked. | |
Void | VISA_exit (VISA_Handle visa) |
Leave an algorithm's critical section. This must be called after the API has completed calling an algorithm's IALG_Fxns. | |
Ptr | VISA_getAlgHandle (VISA_Handle visa) |
Obtains an algorithm's handle. This is the handle required to be passed to the algorithm's IALG_Fxns. | |
Ptr | VISA_getAlgorithmHandle (VISA_Handle visa) |
Obtains an algorithm's handle. If the algorithm is local, this is the handle that can be passed to Algorithm APIs, not to the IALG_Fxns. | |
IALG_Fxns * | VISA_getAlgFxns (VISA_Handle visa) |
Get implementation functions for this algorithm. |
#define VISA_MODNAME "ti.sdo.ce.VISA" |
Name to pass to Diags_setMask() to enable logging for VISA functions. For example, Diags_setMask(VISA_MODNAME"+EX1234567"); turns on all Log statements in this module. Diags_setMask() must be called after initialization to take effect.
typedef struct VISA_Obj* VISA_Handle |
Opaque handle to a node.
typedef VISA_MsgHeader* VISA_Msg |