VISA

Defines

#define VISA_EOK   0
 Success.
#define VISA_ERUNTIME   -1
 Internal runtime error.
#define VISA_EFAIL   -2
 General system error.
#define VISA_ETIMEOUT   -100
 Timeout occurred.
#define VISA_FOREVER   Engine_FOREVER
 Special value for timeout parameter indicating never timeout.

Typedefs

typedef Int VISA_Status
 VISA result data type.

Functions

VISA_Status VISA_getAlgMemRecs (VISA_Handle visa, IALG_MemRec *memTab, Int size, Int *numRecs)
 Get the IALG_MemRec memory assigned to an algorithm instance.
VISA_Status VISA_getAlgNumRecs (VISA_Handle visa, Int *numRecs)
 Get the number of IALG_MemRecs assigned to an algorithm.
Ptr VISA_getCodecClassConfig (VISA_Handle visa)
 Get codec-specific values for the VISA class-specific (or codec-specific if the codec doesn't extend VISA) stub-and/ or-skeleton configuration data (that some classes have).
UInt VISA_getMaxMsgSize (VISA_Handle visa)
 Returns max size of messages allocated by VISA_allocMsg().
Bool VISA_isLocal (VISA_Handle visa)
 Indicates whether VISA codecs run on a remote or local CPU.

Detailed Description

Codec Engine Algorithm-independent shared definitions and services.


Define Documentation

#define VISA_EOK   0

Success.

#define VISA_ERUNTIME   -1

Internal runtime error.

#define VISA_EFAIL   -2

General system error.

#define VISA_ETIMEOUT   -100

Timeout occurred.

#define VISA_FOREVER   Engine_FOREVER

Special value for timeout parameter indicating never timeout.


Typedef Documentation

typedef Int VISA_Status

VISA result data type.


Function Documentation

VISA_Status VISA_getAlgMemRecs ( VISA_Handle  visa,
IALG_MemRec memTab,
Int  size,
Int *  numRecs 
)

Get the IALG_MemRec memory assigned to an algorithm instance.

Parameters:
[in] visa Handle to an algorithm instance.
[out] memTab Location to store the IALG_MemRecs.
[in] size Maximum number of IALG_MemRecs to put in memTab array.
[out] numRecs Actual number of IALG_MemRecs copied into memTab array.
Remarks:
Any algorithm instance handle (e.g. VIDDEC2_Handle, AUDDEC1_Handle, etc), can be cast to a visa handle.
Example:
      AUDDEC1_Handle decoder;

      decoder = AUDDEC1_create(...);

      ... likely use VISA_getAlgNumRecs() to alloc enough mem...

      VISA_getAlgMemRecs((VISA_Handle)decoder, ...);
Return values:
VISA_EOK Success.
VISA_EFAIL Failure.
See also:
VISA_getAlgNumRecs()
VISA_Status VISA_getAlgNumRecs ( VISA_Handle  visa,
Int *  numRecs 
)

Get the number of IALG_MemRecs assigned to an algorithm.

Parameters:
[in] visa Handle to an algorithm instance.
[out] numRecs Location to store the number of IALG_MemRecs used.
Remarks:
Any algorithm instance handle (e.g. VIDDEC2_Handle, AUDDEC1_Handle, etc), can be cast to a visa handle.
Example:
      Int numRecs;
      AUDDEC1_Handle decoder;

      decoder = AUDDEC1_create(...);

      VISA_getAlgNumRecs((VISA_Handle)decoder, &numRecs);
Return values:
VISA_EOK Success.
VISA_EFAIL Failure.
See also:
VISA_getAlgMemRecs()
Ptr VISA_getCodecClassConfig ( VISA_Handle  visa  ) 

Get codec-specific values for the VISA class-specific (or codec-specific if the codec doesn't extend VISA) stub-and/ or-skeleton configuration data (that some classes have).

Parameters:
[in] visa Handle to an algorithm instance.
Return values:
address of the codec class config data structure, or NULL if codec class config data not defined for the codec; the format of the structure is class-specific, and the data in it is codec- specific
Precondition:
visa must be a valid algorithm instance handle.
UInt VISA_getMaxMsgSize ( VISA_Handle  visa  ) 

Returns max size of messages allocated by VISA_allocMsg().

Return values:
maxMsgSize Max size of messages allocated by VISA_allocMsg()
Remarks:
This is typically called by an algorithm class' stub.
See also:
VISA_allocMsg()
Bool VISA_isLocal ( VISA_Handle  visa  ) 

Indicates whether VISA codecs run on a remote or local CPU.

Return values:
FALSE VISA codecs run on remote CPU
TRUE VISA codecs run on local CPU
Remarks:
This is typically called by an algorithm class' stub.
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2009, Texas Instruments Incorporated