#include <que.h>
#include <pool.h>
#include <platform.h>
#include <version.h>
Go to the source code of this file.
Defines | |
#define | IN |
Argument specification syntax ============================================================================. | |
#define | OUT |
#define | CONST const |
#define | DSP_MAX_STRLEN 32 |
Maximum length of string. ============================================================================. | |
#define | MAX_IPS 16 |
#define | DSPLINK_TERMINATE_EVT (-1) |
#define | DSPLINK_DRIVER_NAME "/dsplink" |
DSPLINK driver name ============================================================================. | |
#define | MAX_DRIVER_NAME_LEN 16 |
Maximum length of the driver name. ============================================================================. | |
Typedefs | |
typedef Void(* | DSPLINK_TerminateFxn )(Void) |
Variables | |
far DSPLINK_TerminateFxn | DSPLINK_terminateFxn |
POOL | |
POOL variable defined by MSGQ module. This is temporary until this definition is exported by DSP/BIOS configuration tool. ============================================================================ ============================================================================ | |
POOL_Config * | POOL |
Void | DSPLINK_init (Void) |
This function initializes DSP/BIOS LINK. |
#define IN |
Argument specification syntax ============================================================================.
============================================================================
#define OUT |
#define CONST const |
#define DSP_MAX_STRLEN 32 |
Maximum length of string. ============================================================================.
============================================================================
#define MAX_IPS 16 |
#define DSPLINK_TERMINATE_EVT (-1) |
#define DSPLINK_DRIVER_NAME "/dsplink" |
DSPLINK driver name ============================================================================.
============================================================================
#define MAX_DRIVER_NAME_LEN 16 |
Maximum length of the driver name. ============================================================================.
============================================================================
typedef Void(* DSPLINK_TerminateFxn)(Void) |
Void DSPLINK_init | ( | Void | ) |
This function initializes DSP/BIOS LINK.
============================================================================
None. |
POOL_Config* POOL |