Contact Us     Buy      About TI      TI Worldwide     my.TI  
Texas Instruments
Real World Signal Processing
  Search TI  > Advanced Search 
  
  
 
Update Advisor: Code Composer Studio v3.3 Service Releases

Update Information

A Service Release contains bug fixes and updated device support.  A service release contains all the content from all previous service releases.  i.e. service release 2 is a superset of service release 1.  A service release can be installed on any previous CCStudio v3.3 release.  If you are using a 3rd Party emulator please check the company's website to obtain the appropriate drivers.    We will indicate in description below if there is a change introduced that requires a driver update (remember to check see if previous releases required an update). 

The release notes will provide the complete listing of the bugs addressed in each service release.   Links to previous service releases are provided, however it is recommended that you install the latest service release.

Important Note: Some new devices may require updates to DSP/BIOS or the Code Generation tools in addition to the Code Composer Studio service release.  These Updates are also available from the Update Advisor.


Attention Windows Vista Users

There are some known issues with Code Composer Studio operating on Microsoft Windows Vista. If you are a user of Code Composer Studio on Windows Vista please refer to the following page. 

 

Latest Service Release
Service Release 12.1 (3.3.82.13) Release Notes This is an updated version of the older Release 12. 
Bug fixes (see release notes). 
Chip Support Packages for the following devices have been added: F2823x RevA, C6474, TCI6484, DA830, c6747, c6745, OMAP-L137, F28027, and CortexM & CortexR Peripheral Register.
Note: This package contains an updated USCIF which may require you to update your 3rd party emulation drivers.  Spectrum Digital XDS560R drivers are not available, however the 510 products are fine.  Blackhawk has drivers available for their emulators.
Previous Service Releases
Service Release 11 (3.3.81.6.2) Release Notes Bug fixes (see release notes). 
NOTE: A previous version of an SR may have removed some older documents. Newer updated documents are posted on the web. If you require the older documents, they are backed up in <install_dir>\Uninstall\UpdateAdvisorBackup\docs).
Service Release 10 (3.3.80) Release Notes Bug fixes (see release notes).  ARM users should update their Spectrum Digital Drivers.  DM646x, F2823x, DM643x and C642x support added.
Service Release 9 (3.3.79) Release Notes Bug fixes (see release notes). 
Service Release 8 (3.3.77) Release Notes Bug fixes (see release notes). 
Advanced event triggering is now moved into the breakpoint manager.  XDS560T(Trace) support has also been updated with numerous fixes and usability improvements.
Service Release 7 (3.3.67) Release Notes Bug fixes (see release notes). 
Includes the following chip support packages: OMAP3430 ES2.0, Cortex M3/R4 and F283xx. 
Service Release 6 (3.3.57)
F283xx Chip Support Package
Release Notes Bug fixes (see release notes)
F283xx CSP will be rolled into SR7
Service Release 5 (3.3.54.1)
DM648 Chip Support Package
Release Notes Bug fixes (see release notes)
DM648/647 CSP will be rolled into SR6
Service Release 4 (3.3.50.2) Release Notes Bug fixes (see release notes)
Service Release 3 (3.3.49.1) Release Notes Bug fixes (see release notes), TCI6488 and TCI6486 CSPs
Service Release 2 (3.3.46.1) Release Notes Bug fixes (see release notes), OMAP3430 CSP. 

Note: Update to 3rd party 560 drivers required.

Important Workaround: Board configuration names longer than 20 characters may cause CCS to crash on startup. To prevent this, please use CCS Setup to modify the board name to be less than equal to 20 characters in length. This issue is resolved in newer service releases.

Service Release 1 (3.3.42.1) Release Notes Bug fixes (see release notes)

 

For additional information, contact support@ti.com

Products  |  Applications  |  Support  |  Site Map
© Copyright 1995-2003 Texas Instruments Incorporated. All rights reserved. Trademarks  |  Privacy Policy  |  Terms of Use