Code Composer Studio ™ IDE v3.3 Service Release 2 Release Notes
These Code Composer Studio (CCStudio) release notes contain valuable
information which may not be included in other product documentation. This
information will assist you in the use of CCStudio.
To keep up-to-date on specific items in this list please visit our
Tools and Software Bug Search site. Use the unique
identifier (SDSCM number) to find what you are looking for.
Please note the content of each Service Release is cumulative: each Service Release of the content of all previous Service Releases plus the content of the new release.
InstallShield and DemoShield are registered trademarks and service marks of InstallShield Software Corporation.
C2000, C5000, C54x, C55x, C6000, C6x, OMAP, TMS320, TMS320C54x,
TMS470, Code Composer Studio, DSP/BIOS, eXpressDSP, XDS560,
and XDS510 are trademarks of Texas Instruments.
This service release includes the contents of the following Chip Support Packages (CSPs):
Users of Blackhawk and Spectrum Digital Emulators will need to update their 560 drivers after installing SR2.
General Information
Release notes specific to CCS' XDS560 Trace functionality can be found here.
Identifier |
Headline |
Component |
Target |
---|---|---|---|
SDSCM00014761 | .tprof file is not generated while disabling profile in Halt Collection state. | Profiler | All |
SDSCM00016161 | Cortex Disassembly window shows no labels for some particlular .out files | Object File Server | TMS470 |
SDSCM00015388 | callstack only shows one entry when using gcc created executable | Object File Server | TMS470 |
SDSCM00015914 | Loading with program offset's affects data offsets | Object File Server | All |
SDSCM00015564 | Step out does not always work in thum mode programs | Object File Server | TMS470 |
SDSCM00015676 | Labels in thumb code have wrong address when compiled with TI ARM 4.4 codegen w/EABI | Object File Server | TMS470 |
SDSCM00015864 | Memory Window does not display min & max signed long values correctly on C64x and C64x+ | Watch Window | C6000 |
SDSCM00016102 | Program load progress bar disappears before load completes | Program/Symbol Loader | All |
SDSCM00016041 | local variable is wrong | Object File Server | All |
SDSCM00012654 | Resetting counter on Run | Breakpoint Manager | TMS470 |
SDSCM00016106 | Counter only updates if a breakpoint is not hit | Breakpoint Manager | C5500 |
SDSCM00015403 | When the continous refresh option is activated for graph window,other realtime windows also get refreshed continuously | Debugger | F2800 |
SDSCM00015168 | CCS not working if not administrator | Code Composer IDE | All |
SDSCM00015469 | CCS should cleanup typelibrary entries that may impact CCS currently being started | Code Composer IDE | All |
SDSCM00013804 | Missing installation paths for plugins in CCSCorePlugins.xml | Code Composer IDE | All |
SDSCM00013933 | Target access error when running C6400PLUS of DaVinci board in real-time mode | Emulation | C6000 |
SDSCM00014960 | If workspace is saved when connected to target, then reloading it does not work properly | Code Composer IDE | All |
SDSCM00014995 | CC_SETUP change to manage a relationship between a processor node and a memory capable router (which is not a parent ) | Code Composer Setup | All |
SDSCM00014738 | cc_setup crashes when user modifies an existing board confi and select board data file from "specify custom board data file" | Code Composer Setup | All |
SDSCM00013374 | CCS 3.3 beta 2 takes too long to start up | Code Composer Setup | All |
SDSCM00013866 | CCS dies on run of an application with code coverage enabled. | Simulation | C6000 |
SDSCM00014829 | Merge Issue | Analysis Toolkit | All |
SDSCM00014980 | C64x+ simulator does not count the CPU.NOP simulator analysis events correctly. | Simluation | C6000 |
SDSCM00015075 | CCS will generate erroneous illegal opcode error message depending on how CCS customization options are set | Simulation | C6000 |
SDSCM00015902 | Registry entry for the DRP script processor is incorrect | Installer | All |
SDSCM00013184 | Register server changes to support new schema for xml files which speed up performance. | Register Server | All |
SDSCM00010951 | Zero value returned when reading register in IEEE format via SDK | Register Server | All |
SDSCM00014390 | Register server does not dynamically update the MajorID when it changes after connect and retains the old (pre-connect) value | Register Server | All |
SDSCM00004933 | CCScripting API CCSClose(0) closes all instances of CCS control windows | CCS Scripting | All |
SDSCM00015670 | CCS crashes when radix of more than one variable is selected in watch window and changed. | Watch Window | All |
SDSCM00015864 | Memory Window does not display min & max signed long values correctly on C64x and C64x+ | Memory Window | C6000 |
SDSCM00015338 | DSP reset on raptor causes Failed Software reset: JTAG protocol reset | Emulation | C5600 |
SDSCM00015412 | HWA Register Visibility in CCS | Emulation | C5600 |
SDSCM00014442 | C55xp functional simulator crashes | Simulation | C5600 |
SDSCM00012983 | CC3.3 Beta: Help search tab spawns an error | Documentation | All |
SDSCM00015165 | Disassembly window contents scrambled when scrolling up | Code Composer IDE | C6000 |
SDSCM00013793 | .net error is thrown on memory window | Memory Window | C6000 |
SDSCM00013980 | No FLOAT dislplay option available in the register window | Register Window | All |
SDSCM00014384 | Register window can not view ICEPick register even when ICEPick is connected | Register Window | All |
SDSCM00014545 | Breakpoint Manager is confused between a Breakpoint and a User defined group. | Breakpoint Manager | All |
SDSCM00012225 | DSK5510: Guard bits are not read properly in Register window | Register Window | C5500 |
SDSCM00013178 | Name of TMS470R2x Advanced Features plugin needs to be updated | Emulator Analysis | All |
SDSCM00015183 | Register Window does not set the correct bits for registers defined in TargetDB xml file | Register Window | All |
SDSCM00013046 | Neon register status on IDE status bar is not updated correctly | Code Composer IDE | TMS470 |
SDSCM00015286 | Profiling Setup window (Lower half) gives misleading message. | Profile Setup | All |
SDSCM00013195 | Missing help doc for TMS470R2x Advance Features | Documentation | TMS470 |
SDSCM00016008 | IDE change to manage a relationship between a processor node and a memory capable router (which is not a parent ) | Debugger | All |
SDSCM00015449 | The GEL_SetTimer function timeout interval is not correct | General Extension Language (GEL) | All |
SDSCM00014812 | The GEL_SetTimer function timeout interval is not correct in CCS3.3 | General Extension Language | All |
SDSCM00015071 | Flash programmer for 28xx does not allow programming of non-executable files | Flash Plugin | F2800 |
SDSCM00016023 | CCS_Setup throws error | Emulation | All |
SDSCM00016245 | CCS will generate erroneous illegal opcode error message depending on how CCS customization options are set | Simulation | C6000 |