Code Composer Studio ™ IDE Service
Release
These Code Composer Studio (CCStudio) release notes contain valuable information which may not be included in other product documentation. This information will assist you in the use of CCStudio. Each Service Release is a cumulative
To keep up-to-date on specific items in this list please visit our Tools and Software Bug Search site. Use the unique identifier (SDSCM number) to find what you are looking for.
Please note the content of each Service Release is cumulative: each Service Release of the content of all previous Service Releases plus the content of the new release.
Windows, Windows XP, Visual SourceSafe, and Visual C++ are all trademarks and/or registered trademarks of Microsoft Corporation.InstallShield and DemoShield are registered trademarks and service marks of InstallShield Software Corporation.
C2000, C5500, C54x, C55x, C6000, C6x, OMAP, TMS320, TMS320C54x, TMS470, Code Composer Studio, DSP/BIOS, eXpressDSP, XDS560, and XDS510 are trademarks of Texas Instruments.
Identifier |
Headline |
Component |
Target |
---|---|---|---|
SDSCM00018286 | TCI6486 Missing EDMA interrupts in config file | C6000 SIM- Configuration Files | Faraday |
SDSCM00016009 | CCS (Faraday CSP) reports invalid CIO command | SIM Internal | Faraday |
SDSCM00005306 | SRIO specific registers after address 0x02d01000 can't be modified via register or memory view. | Code Composer IDE | C64x Plus |
SDSCM00017247 | Unable to write to CP15 register on ARM968 | Emulation - Drivers | ARM968 |
SDSCM00018814 | Include info on unloaded modules in mini dump report | Code Composer IDE | ALL |
SDSCM00012099 | During the execution of GEL_AddInputFile(), though the file cannot be opened, the breakpoint is set | Code Composer IDE | C64x Plus Simulator |
SDSCM00018146 | Unable to load GEL files from command line as current directory gets changed | AET | ALL |
SDSCM00018230 | Performance--Speed of Stepping over on C64x+ Emulators is much slower than on other ISAs. | Code Composer IDE | C64x Plus Emulator |
SDSCM00018720 | Exception reporting doesn't persist through a CCS reset | Code Composer IDE | C64x Plus Emulator |
SDSCM00017768 | CCS hangs while running a CSL cache test case on TCI6482 simulator | C6000 Sim-Configuration Files | C6482 |
SDSCM00017747 | CCS Crashes when performing operations through PDM | Code Composer IDE | C64x Plus Emulator |
SDSCM00018316 | structures added to WW using GEL_WatchAdd(variable,x) do not show parents radix setting for all sub children | Code Composer IDE | ALL |
SDSCM00015665 | Profiling icon on the editor does not disappear for Ranges, even if profiling is disabled. | Code Composer IDE | ALL |
SDSCM00017843 | Inconsistent treatment of pointers in 55+ mixed-mode program from GEL | Code Composer IDE | C55x Plus |
SDSCM00014983 | Coverage should handle files with the same name, in different directory. | C6000 Sim-Features | C6416 |
SDSCM00015148 | PETL:: The .cov generation crashes on an empty .tprof file | Analysis Toolkit | C6000 |
SDSCM00017931 | PETL:: The coverage .xls CANNOT log counter values larger than 32-bits | Analysis Toolkit | C6416 |
SDSCM00015640 | PETL::Code coverage tool can NOT handle project with at least 5000 directory element (directory search string) | Analysis Toolkit | C6416 |
SDSCM00015148 | PETL:: The .cov generation crashes on an empty .tprof file | Analysis Toolkit | C6416 |
SDSCM00014985 | The coverage data generation takes a long time | C6000 Sim-Features | C6416 |
SDSCM00020034:Virtio Drivers need to be imported
Component: Code Composer IDE
Target: vpom2420
Release Note: the Virtio Drivers are visible in Setup:
ARM11 - VPOM2420 Platform Simulator
ARM7 - VPOM2420 Platform Simulator
C55x - VPOM2420 Platform Simulator
OMAP - VPOM2420 Platform Simulator
OMAP - VPOM2430 Platform Simulator
C:\CCStudio_v3.3\cc\bin\cc_setup.exe -i C:\CCStudio_v3.3\drivers\import\arm7tdmi_big.ccs -startCCS C:\Projects\arm7sim.wks
C:\ccstudio_v3.3\cc\bin\cc_app.exe .\..\gel\alais.gel
Identifier |
Headline |
Component |
Target |
---|---|---|---|
SDSCM00000949 | Conditional run statements in the Command Window are not working correctly | Documentation | C64x Plus Simulator |
SDSCM00004163 | PerfMem Himalaya AVV failure due to incorrect release semantics of data fifo | C6000 Sim-Source Components | C64x Plus Simulator |
SDSCM00011483 | Enabling Clock then Profile Event causes CCS to give clock error. | Emulation - Drivers | C5500 |
SDSCM00011552 | Required code generation tools for building XDS560 drivers. | Emulation - EPK | C6000 |
SDSCM00011586 | Register display window does not include NAND Flash registers | Emulation - TPI | C6000 |
SDSCM00011622 | tms470_helen.gel contains many errors | Emulation - Config Files | OMAP |
SDSCM00012356 | F1 Help Call on 28x emulator analysis menu item calls wrong topic | Plugins | C2800 |
SDSCM00013235 | M3 and R4 CCS simulators display ARM mode and Little Endian on the bottom | Code Composer IDE | ARM Cortex M3 |
SDSCM00014233 | Selecting "Collect Code Coverage and Exclusive Profile Data" activity causes CCS to crash on Program Run | C6000 Sim-Source Components | C6482 |
SDSCM00015207 | Global Halt command is broken for GEM | Emulation - Drivers | C64x Plus Emulator |
SDSCM00015523 | CCS gives data verification error when loading .out files built with -cr linker option | Code Composer IDE | C2400 |
SDSCM00016626 | Unable to use "View Location..." and "Break When.." features of Watch Window on structures | Code Composer IDE | ALL |
SDSCM00017025 | No longer able to view register pairs in the register window | Debug Server | C6000 |
SDSCM00018015 | bus-error warning being observed in the application which disappears when Flush Pipeline On Halt is selected | C5000 Sim-Source Components | Wrigley3G |
SDSCM00018066 | When a 5510 and a 5416 is put in the same scan chain unable to connect to both with CCS. | Emulation - Drivers | C55X |
SDSCM00018082 | Make cc_user.dat error message more explicit | Code Composer IDE | ALL |
SDSCM00018128 | Memory Server Register decoders not initialized properly from XML file | Code Composer IDE | C64x Plus Emulator |
SDSCM00018221 | Unable to set breakpoints in SDRAM for RAP3GV4 | Emulation - Drivers | C5500 |
SDSCM00018315 | Endianness check causes load symbols to fail when disconnected. | Code Composer IDE | ALL |
SDSCM00018528 | description of the parameters for the API ProjectBuild is not correct | Documentation | C64xx |
Identifier |
Headline |
Component |
Target |
---|---|---|---|
SDSCM00014073 | ARM11 help needs updating | Documentation | TMS470 |
SDSCM00015250 | DMA does not generate interrupt if CIER is enabled after transfer completion.Simulation | Simulation | C6000 |
SDSCM00014233 | Selecting "Collect Code Coverage and Exclusive Profile Data" activity causes CCS to crash on Program Run | Simulation | C6000 |
SDSCM00015249 | A single External memory access (in the midst of DMA accesses) consumes 15K cycle on c6416 CA simulator | Simulation | C6000 |
SDSCM00014827 | Code Coverage throws when merging two files. | Analysis Toolkit | C6000 |
SDSCM00017040 | 64+ emulation driver does not indicate it supports cache visibility | Emulation | C6000 |
SDSCM00015845 | CCS sometimes yields 'CIO command not recognized' error | Emulation | C6000 |
SDSCM00017999 | Profiling of single non-CPU Cycle event returns -1 for profiled data | Code Composer IDE | ALL |
SDSCM00017741 | Bubble help prevents all cores from connecting without user setting focus to bubble help | Code Composer IDE | ALL |
SDSCM00017256 | Processor mode not shown for Cortex R4 simulator | Code Composer IDE | TMS470 |
SDSCM00005321 | ATK needs stress test with large # of networked files/functions/symbols | Simulation | C6000 |
SDSCM00013866 | CCS dies on run of an application with code coverage enabled. | Simulation | C6000 |
Identifier |
Headline |
Component |
Target |
---|---|---|---|
SDSCM00014233 | Selecting "Collect Code Coverage and Exclusive Profile Data" activity causes CCS to crash on Program Run | Simulation | C6000 |
SDSCM00015249 | A single External memory access (in the midst of DMA accesses) consumes 15K cycle on c6416 CA simulator | Simulation | C6000 |
SDSCM00010856 | Grouping CPU's using <Highlighted CPU's> and giving PDM halt does not work as expected. | Simulation | C6000 |
SDSCM00015127 | .tprof file is not generated while disabling profile in Halt Collection state. | Profiler | All |
SDSCM00013608 | Addition of unintended task to the profile collector task list | Profiler | All |
SDSCM00015564 | Step out does not always work in thumb mode programs | Callstack | TMS470 |
SDSCM00015914 | Loading with program offset's affects data offsets | Object File Server | TMS470 |
SDSCM00016390 | Debug Line Information not shown correctly by CCS | Object File Server | All |
SDSCM00015611 | Unable to view values of local variables in gcc compiled executable | Object File Server | TMS470 |
SDSCM00017290 | local symbols are viewed at an incorrect sp offset | Object File Server | TMS470 |
SDSCM00016222 | Counter only updates if a breakpoint is not hit | Breakpoint Manager | C5500 |
SDSCM00016220 | Resetting counter on Run | Breakpoint Manager | TMS470 |
SDSCM00016228 | When the continous refresh option is activated for graph window,other realtime windows also get refreshed continuously | Debugger | C2800 |
SDSCM00016881 | CCS sometimes yields 'CIO command not recognized' error | Debugger | C6000 |
SDSCM00012885 | CCS 3.3 beta 2 takes too long to start up | Code Composer Setup | All |
SDSCM00016472 | No way to specify a register on the IO page in the XML schema | Register Server | C5500 |
SDSCM00002559 | Want line file to be automatically highlighted in goto | Code Composer Studio | All |
SDSCM00016671 | sizeof() returns incorrect values for sizes of structs both in Watch window and through Scripting APIs when using CCS 3.3 | General Extension Language (GEL) | All |
SDSCM00014442 | C55xp functional simulator crashes | Simulation | C5500 |
SDSCM00016551 | Page selection box is not big enough to distinguish data pages | Memory Window | All |
SDSCM00015071 | Flash programmer for 28xx does not allow programming of non-executable files | Flash Programmer | C2800 |
SDSCM00014338 | Memory leak in BTI | Project Manager | All |
SDSCM00015845 | CCS sometimes yields 'CIO command not recognized' error | Emulation | C6000 |
Identifier |
Headline |
Component |
Target |
---|---|---|---|
SDSCM00014761 | .tprof file is not generated when disabling profile in Halt Collection state. | Profiler | C6000 |
SDSCM00016161 | Cortex Disassembly window shows no labels for some particular .out files | Object File Server | TMS470 |
SDSCM00015388 | callstack only shows one entry when using gcc created executable | Object File Server | TMS470 |
SDSCM00015914 | Loading with program offsets affects data offsets | Object File Server | TMS470 |
SDSCM00015564 | Step out does not alwasy work in thumb mode programs | Object File Server | TMS470 |
SDSCM00015676 | Labels in thumb code have wrong address when compiled with TI ARM 4.4 codegen w/EABI | Object File Server | TMS470 |
SDSCM00016102 | Program load progress bar disappears before load completes | Code Composer IDE | All |
SDSCM00016041 | local variable is wrong | Object File Server | All |
SDSCM00012654 | Resetting counter on Run | Debugger | TMS470 |
SDSCM00016106 | Counter only updates if a breakpoint is not hit | Debugger | C5500 |
SDSCM00015403 | When continuous refresh option is activated for graph window, other realtime windows also get refreshed continuously | Debugger | C2800 |
SDSCM00015168 | CCS not working if not administrator | Code Composer IDE | All |
SDSCM00015469 | CCS should cleanup typelibrary entries that may impact CCS currently being started | Code Composer IDE | All |
SDSCM00013804 | Missing installation paths for plugins in CCSCorePlugins.xml | Code Composer IDE | All |
SDSCM00014960 | If workspace is saved when connected to target then reloading it does not work properly | Code Composer IDE | All |
SDSCM00014995 | CC_SETUP change to manage a relationship between a processor node and a memory capable router (which is not a parent) | Code Composer Setup | All |
SDSCM00014738 | cc_setup crashes when user modifies an existing board conig and selects board data file from "specify custom board data file" | Code Composer Setup | All |
SDSCM00013374 | CCS 3.3 beta 2 takes too long to start up | Code Composer Setup | All |
SDSCM00013866 | CCS dies on run of an application with code coverage enabled. | Simulation | C6000 |
SDSCM00014829 | Merge Issue | Analysis Toolkit | C6000 |
SDSCM00014980 | C64x+ simulator does not count the CPU.NOP simulator analysis events correct. | Simulation | C6000 |
SDSCM00015075 | CCS will generate erroneious illegal opcode error message dpending on how CCS customization options are set | Simulation | C6000 |
SDSCM00015902 | Registry entry for the DRP script processor is incorrect | Installer | All |
SDSCM00013184 | Register server changes to support new schema for xml files which speed up performance | Debugger | All |
SDSCM00010951 | Zero value returned when reading register in IEEE format via SDK | Debugger | C6000 |
SDSCM00014390 | Register server does not dynamically update the MajorID when it changes after connect and retains the old (pre-connect) value | Debugger | All |
SDSCM00004933 | CCScripting API CCSClose(0) closes all instances of CCS control windows | CCS Scripting | All |
SDSCM00015670 | CCS crashes when radix of more than one variable is selected in watch window and changed. | Watch Window | All |
SDSCM00015864 | Memory Window does not display min & max signed long values correctly on C64x and C64x+ | Watch Window | All |
SDSCM00015338 | DSP reset on raptor causes Failed Software reset: JTAG protocol reset | Emulation | C5500 |
SDSCM00015412 | HWA Register Visibility in CCS | Target Port Interface (TPI) | C5500 |
SDSCM00014442 | C55xp functional simulator crashes | Simulation | C5500 |
SDSCM00012983 | CC3.3 Beta: Help search tab spawns an error | Documentation | C6000/C5400/C5500 |
SDSCM00015165 | Disassembly window contents scrambled when scrolling up | Code Composer IDE | C6000 |
SDSCM00013793 | .net error is thrown on memory window | Code Composer IDE | All |
SDSCM00013980 | No FLOAT dislplay option available in the register window | Code Composer IDE | All |
SDSCM00014384 | Register window can not view ICEPick register even when ICEPick is connected | Code Composer IDE | OMAP |
SDSCM00014545 | Breakpoint Manager is confused between a Breakpoint and a User defined group. | Code Composer IDE | All |
SDSCM00012225 | DSK5510: Guard bits are not read properly in Register window | Code Composer IDE | C5500 |
SDSCM00013178 | Name of TMS470R2x Advanced Features plugin needs to be updated | Code Composer IDE | TMS470 |
SDSCM00015183 | Register Window does not set the correct bits for registers defined in TargetDB xml file | Code Composer IDE | All |
SDSCM00013046 | Neon register status on IDE status bar is not updated correctly | Code Composer IDE | OMAP |
SDSCM00015286 | Profiling Setup window (Lower half) gives misleading message. | Profiler | All |
SDSCM00013195 | Missing help doc for TMS470R2x Advance Features | Code Composer IDE | TMS470 |
SDSCM00015449 | The GEL_SetTimer function timeout interval is not correct | General Extension Language (GEL) | All |
SDSCM00014812 | The GEL_SetTimer function timeout interval is not correct in CCS3.3 | General Extension Language (GEL) | All |
SDSCM00015071 | Flash programmer for 28xx does not allow programming of non-executable files | F28xx Flash Programmer | F2800 |
SDSCM00016023 | CCS_Setup throws error | Emulation | All |
Identifier |
Headline |
Component |
Target |
---|---|---|---|
SDSCM00000450 | CIO break point semantics to be defined by IDE in presence of global break points | Debugger | C6000 |
SDSCM00014168 | Error when attempting to generate ATK .xls files within CCS 3.3 | Analysis Toolkit | C6000 |
SDSCM00014253 | can't open register window via context menu | Code Composer IDE | All |
SDSCM00013960 | C6x profiler sometimes calculates large profiling values after end of program breakpoint hit | Profiler | C6000 |
SDSCM00013706 | GEL_MemorySave() using COFF format generates bad COFF file | Debugger | All |
SDSCM00013822 | GEL_SystemRestoreState() does not restore Registers | General Extension Language (GEL) | C5500 |
SDSCM00005135 | CCS3.0 HSRTDX Does not work after performing Debug->Reset CPU | RTDX GUI | C6000 |
SDSCM00014352 | L2 Cache set 0, way 0 shown repeatedly | Cache Tag Ram Viewer | C6000 |
SDSCM00014353 | Not all cache lines are read | Cache Tag Ram Viewer | C6000 |
SDSCM00014356 | Cache tag ram display incorrect after increasing L2 size | Cache Tag Ram Viewer | C6000 |
SDSCM00014358 | Cache tag ram display incorrect after decreasing L2 size | Cache Tag Ram Viewer | C6000 |
SDSCM00014840 | Consultant template files need to be updated to enable codegen consultant fix. | Application Code Tuning | C6000 |
SDSCM00014181 | Help needs to state that Spectrum Digital 14 pin-CTI-20 pin adapter does not support HS RTDX | Documentation | All |
SDSCM00013236 | Problem stepping in a while loop | Target Port Interface (TPI) | TMS470 |
SDSCM00013146 | Many CST (CodeSizeTune) references in CCS tutorial files | Documentation | All |
SDSCM00014175 | CCS Memory Leak occurs when running long usage sessions | CCS Scripting | All |
SDSCM00014388 | Memory leak in Project Manager | BTI | All |
SDSCM00014493 | If global breakpoints are configured, but don't work, the IDE will wait forever | Debugger | All |
SDSCM00014487 | locals not showing up for some functions | Object File Server | All |
SDSCM00014109 | Crash when loading ELF program | Object File Server | All |
SDSCM00014803 | OFS doesn't properly extract register offset information | Object File Server | All |
SDSCM00013673 | Variable declared inside two nested loop does not hid outer variable | Object File Server | All |
SDSCM00013258 | When trying to save workspace for first time in CCS 3.3, the directory defaults to a CCS 3.1 directory | Code Composer IDE | All |
SDSCM00014731 | CCS gives error messages about ACx registers, value of thos registers is ????????. | Target Port Interface(TPI) DLL | C5500 |
SDSCM00013298 | HW breakpoint on ARM11 always perform halt action no matter what other action is set | Emulation | TMS470 |
SDSCM00013522 | Step Over executed as Step Into on ARM11 of OMAP2420 | Target Port Interface(TPI) DLL | TMS470 |
SDSCM00014040 | CC_Setup: Revert to Saved Configuration makes application exit abruptly | Code Composer IDE | All |
SDSCM00014858 | Unable to load program file that is mixed TI and RVCT object code | Object File Server | TMS470 |
SDSCM00014721 | Loading program causes - This Target Does Not Support The GEL_DriverString() Function error | Analysis Toolkit | C5500 |
SDSCM00014759 | Memory mapping conflicts in CFG and GEL | General Extension Language (GEL) | C5510 |
SDSCM00014542 | StepIn takes place instead of StepOver in ARM7 core of 2420 using XDS510 Emu | Debugger | TMS470 |
SDSCM00014548 | callstack displays incorrect data in stabs mode | Debugger | C6000 |
SDSCM00014940 | Error when attempting to program some of the C64x+ AET events | Emulation | C6000 |
SDSCM00014929 | Himilaya (GEM) AET chain breakpoint always stops at second address | Emulation | C6000 |
SDSCM00015034 | ARM ELF .bss sections are modified when loaded | Object File Server | All |
SDSCM00014756 | Faraday Trace device XML file has typo for core-2 | Trace Software | C6000 |
SDSCM00014757 | Trace Display has a bug where it behaves weird when cores are not trace programmed in order. | Trace Software | C6000 |
SDSCM00014758 | Trace control has a bug where it fails to program trace when cores are not programmed in order. | Trace Software | C6000 |
SDSCM00013565 | Runaway TraceCntrl.exe process interferes with ability to logoff/reboot Windows | Trace Software | All |
SDSCM00015278 | OMAP2230 XDS560 and XDS560 configurations of CCS 3.3.39 reference nonexistent GEL files | Emulation | OMAP |
SDSCM00015047 | 2nd AET counter job doesn't count | Emulation | C6000 |
SDSCM00015246 | Cannot launch CCS 3.3 Service Pack 3.3.39 with OMAP3430 configurations | Installer | OMAP |
SDSCM00015242 | Cannot launch CCS 3.3 Service Pack 3.3.39 with Ryujin simulators | Installer | C5500 |