AM62LX Device Group descriptions

Introduction

This chapter provides information of specific device groups(DEVGRP) that are permitted in the AM62LX SoC. These device groups are more specific grouping of devices and resources used optionally to have staged init sequence control of the SoC.

Enumeration of Device group IDs

SoC Devgrp ID Generic Devgrp ID Flag Value Description
MCU_WAKEUP DEVGRP_01 0x1U << 1U Set of MCU domain peripherals to initialize at boot and use during runtime.
MAIN DEVGRP_00 0x1U << 0U Set of Main domain peripherals to initialize at boot and use during runtime.