AM62LX Host Descriptions

Introduction

This chapter provides information on the set of HostIDs permitted in this AM62LX SoC. HostIDs uniquely identify each logically distinct high level software entity. A software entity identification number (HostID) can be assigned to an OS either native or virtualized, or a firmware/native application. The HostID is used to select the set of mailbox channels for which this software entity should use to communicate with the System Firmware.

As an example with an A53 core, then there could be 0, 1, or n number of A53 related hosts. The only limit is the number of available mailbox Channels. Typically though, an A53 core will be assigned one secure host as well as one non secure host, but may be assigned additional hosts for certain usecases. As for other cores, some will only use secure hosts, and others will only use non secure hosts. Since the hosts are tied to mailbox channels, hosts are just a way of sectioning off data for a designated purpose.

System Firmware also checks that the used HostID comes from software running on the correct core (as implied by Host Name in the below table) and with the correct security level (Security Status column).

Additionally, one of the key reasons why HostID is tied in with mailbox channels is because it prevents spoofing. When a message is received by System Firmware, the mailbox channel tied to the HostID in the message is verified against the mailbox channel on which the message was received.

Enumeration of Host IDs

Host ID Host Name Security Status Description
0 TIFS Secure Device Management and Security Control
10 A53_0 Secure Cortex A53 context 0 on Main island
11 A53_1 Secure Cortex A53 context 1 on Main island
12 A53_2 Non Secure Cortex A53 context 2 on Main island
13 A53_3 Non Secure Cortex A53 context 3 on Main island
14 A53_4 Non Secure Cortex A53 context 4 on Main island