Example 1: The following example shows how a module, named ModA,
defines a custom error type and shows how this error is raised by
the module. The module defines an Id of E_notEven in its module
specification file (in this case, ModA.xdc). The error's message
string takes only one argument. The module also defines a mayFail()
function that takes an error block. In the module's C source file,
the function checks for the error condition and raises the error if
needed.
Void ModA_mayFail(Int x, Error_Block *eb)
{
if ((x % 2) != 0) {
Error_raise(eb, ModA_E_notEven, x, 0);
...add error handling code here...
return;
}
...
}
Example 2: The following C code supplies an error block to a function
that requires one and tests the error block to see if the function
raised an error. Note that an error block must be initialized before
it can be used and same error block may be passed to several functions.
#include <xdc/runtime/Error.h>
Void myFunc(..., Error_Block *eb)
{
...
if (...error condition detected...) {
String myErrorMsg = "my custom error message";
Error_raise(eb, Error_E_generic, myErrorMsg, 0);
...add error handling code here...
return;
}
}
| const Error.NUMARGS |
 |
Maximum number of arguments supported by an error
| XDCscript usage |
meta-domain |
#define Error_NUMARGS (Int)2
| enum Error.Policy |
 |
Error handling policies
| XDCscript usage |
meta-domain |
values of type Error.Policy
const Error.TERMINATE;
const Error.UNWIND;
typedef enum Error_Policy {
Error_TERMINATE,
Error_UNWIND
} Error_Policy;
VALUES
TERMINATE
All raised errors are fatal. A call to
Error_raise will never return to the caller.
UNWIND
Errors are returned to the caller. A call to
Error_raise will return back to the caller.
DETAILS
Regardless of the current policy in use, raising an error by
calling
Error_raise will always invoke the
error raise hook function assigned to the
Error.raiseHook configuration parameter.
| typedef Error.Id |
 |
Error identifier
DETAILS
Each type of error raised is defined with a metaonly
Error.Desc.
An
Error_Id is a 32-bit target value that encodes the information
in the
Desc. Target programs use
Error_Id values to "raise" and
check for specific errors.
WARNING
Id values may vary among different
configurations of an application. For example, the addition of a
new module to a program may result in a different absolute value for
E_generic. If you need error numbers that remain
invariant, use the user definable
Desc.code field.
| struct Error.Block |
 |
Error block
typedef struct Error_Block Error_Block;
DETAILS
An opaque structure used to store information about errors once raised.
This structure must be initialized via
Error_init()
before being used for the first time.
| struct Error.Data |
 |
Error args
| XDCscript usage |
meta-domain |
var obj = new Error.Data;
typedef struct Error_Data {
} Error_Data;
DETAILS
The two arguments (arg1, arg2) passed to
raise are
stored in one of these arrays within the associated Error_Block.
To access these arguments use
getData to obtain a
pointer to the Error_Block's Data array.
SEE
| metaonly struct Error.Desc |
 |
Error descriptor
| XDCscript usage |
meta-domain |
var obj = new Error.Desc;
obj.msg = String ...
obj.code = UInt16 ...
FIELDS
msg
The error message using a printf style format string,
but limited to NUMARGS arguments.
This format string together with the two arguments passed
to Error_raise` are used to create a human readable
error message.
code
A user assignable code, 0 by default. The user may
optionally set this field during config to give the
error a well-known numeric code.
DETAILS
Each type of error is defined with an error descriptor. This
structure groups common information about the errors of this type.
| config Error.E_generic // module-wide |
 |
Generic error
| XDCscript usage |
meta-domain |
msg: "generic error: %s"
};
| config Error.E_memory // module-wide |
 |
Out of memory error
| XDCscript usage |
meta-domain |
msg: "out of memory: heap=0x%x, size=%u"
};
| config Error.maxDepth // module-wide |
 |
Maximum number of concurrent calls to raiseHook
| XDCscript usage |
meta-domain |
Error.maxDepth = UInt16 16;
extern const UInt16 Error_maxDepth;
DETAILS
To prevent errors that occur in the raiseHook function from
causing an infinite recursion, the maximum number of concurrent
calls to
raiseHook is limited by
Error_maxDepth. If
the number of concurrent calls exceeds
Error_maxDepth, the
raiseHook function is not called.
In multi-threaded systems, errors raised by separate threads may
be detected as recursive calls to raiseHook. So, setting
Error.maxDepth to a small value may - in rare instances - result in
errorHook not being called for some raised errors.
If it is important that all raised errors trigger a call to the
raiseHook function, set Error.maxDepth to an impossibly large
number (0xffff) and either ensure that the raise hook never calls a
function that can raise an error or add checks in raiseHook to
protect against "double faults".
| config Error.policy // module-wide |
 |
System-wide error handling policy
| XDCscript usage |
meta-domain |
| config Error.raiseHook // module-wide |
 |
The function to call whenever an error is raised
| XDCscript usage |
meta-domain |
VALUES
eb
non-NULL pointer to an Error_Block
Even if the client passes a NULL error block pointer, this
parameter is always non-NULL.
DETAILS
This function is always called when an error is raised, even if the
Error policy is
TERMINATE. In rare cases it is
possible that a raised error does not trigger a call to
raiseHook;
see
maxDepth.
SEE
| metaonly config Error.common$ // module-wide |
 |
Common module configuration parameters
| XDCscript usage |
meta-domain |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
| Error.check( ) // module-wide |
 |
Return TRUE if an error was raised
ARGUMENTS
eb
pointer to an Error_Block or NULL
RETURNS
If
eb is non-
NULL and
Error.policy == UNWIND and
an error was raised on
eb, this function returns
TRUE. Otherwise,
it returns
FALSE.
| Error.getCode( ) // module-wide |
 |
Get an error's code
ARGUMENTS
eb
non-NULL pointer to an Error_Block
RETURNS
getCode returns the error code associated with this error block.
SEE
| Error.getData( ) // module-wide |
 |
Get an error's argument list
ARGUMENTS
eb
non-NULL pointer to an Error_Block
RETURNS
getData returns an array of type
Data with
NUMARGS elements containing the arguments provided
at the time the error was raised.
SEE
| Error.getId( ) // module-wide |
 |
Get an error's id
ARGUMENTS
eb
non-NULL pointer to an Error_Block
WARNING
Error_Id values may vary among different configurations
of an application. For example, the addition of a new module to a
program may result in a different absolute value for
E_generic. If you need error numbers that remain
invariant, use the user definable
Desc.code field.
SEE
| Error.getMsg( ) // module-wide |
 |
Get an error's "printf" format string
ARGUMENTS
eb
non-NULL pointer to an Error_Block
SEE
| Error.getSite( ) // module-wide |
 |
Get an error's call site info
ARGUMENTS
eb
non-NULL pointer to an Error_Block
RETURNS
getSite returns a pointer to an initialized
Types.Site structure. However, in the
event that the call site was compiled with
xdc_FILE defined to
be
NULL (to minimize string space overhead) the
file
field may be set to
NULL.
SEE
| Error.init( ) // module-wide |
 |
Put an error block into its initial state
ARGUMENTS
eb
pointer to an Error_Block or NULL
If eb is NULL this function simply returns.
DETAILS
To ensure reliable error detection, clients must call init for
an Error_Block prior to any use.
If the same Error Block is used multiple times, only the last error
raised is retained.
| Error.print( ) // module-wide |
 |
Print error using System.printf()
ARGUMENTS
eb
pointer to an Error_Block or NULL
If eb is NULL this function simply returns with no output.
DETAILS
This function prints the error using System_printf(). The output
is on a single line terminated with a new line character and has the
following form:
<site>: <file>, line <line_num>: <err_msg>
where <site> is the module that raised the error, <file> and
<line_num> are the file and line number of the containing the call
site of the Error_raise(), and <err_msg> is the error message
rendered with the arguments associated with the error.
WARNING
This function is not protected by a gate and, as a result,
if two threads call this method concurrently, the output of the two
calls will be intermingled. To prevent intermingled error output,
you can either wrap all calls to this method with an appropriate
Gate_enter/Gate_leave pair or simply ensure that only one
thread in the system ever calls this method.
| Error.raise( ) // module-wide |
 |
Raise an error
ARGUMENTS
eb
pointer to an Error_Block or NULL
If
eb is
NULL or
Error.policy == TERMINATE,
this function does not return to the caller; after calling any
configured
raiseHook,
System_abort is called with the
string
"xdc.runtime.Error.raise: terminating execution\n".
id
the error to raise
This pointer identifies the class of error being raised;
the error class indicates how to interpret any subsequent
arguments passed to
raise.
arg1
error's first argument
The argument interprested by the first control character
in the error message format string. It is ignored if not needed.
arg2
error's second argument
The argument interpreted by the second control character
in the error message format string. It is ignored if not needed.
DETAILS
This function is used to raise an Error by writing call site,
error ID, and error argument information into the Error_Block
pointed to by eb.
If Error_raise is called more than once on an Error_Block object,
the previous error information is overwritten; only the last error
is retained in the Error_Block object.
In all cases, any configured
Error.raiseHook
function is called with a non-
NULL pointer to a fully
initialized
Error_Block object.
| module-wide built-ins |
 |
// Get this module's unique id
Bool Error_Module_startupDone( );
// Test if this module has completed startup
// The heap from which this module allocates memory