Defines | |
| #define | EDMA3_RM_E_BASE (-155) |
| #define | EDMA3_RM_E_OBJ_NOT_DELETED (EDMA3_RM_E_BASE) |
| #define | EDMA3_RM_E_OBJ_NOT_CLOSED (EDMA3_RM_E_BASE-1) |
| #define | EDMA3_RM_E_OBJ_NOT_OPENED (EDMA3_RM_E_BASE-2) |
| #define | EDMA3_RM_E_INVALID_PARAM (EDMA3_RM_E_BASE-3) |
| #define | EDMA3_RM_E_RES_ALREADY_FREE (EDMA3_RM_E_BASE-4) |
| #define | EDMA3_RM_E_RES_NOT_OWNED (EDMA3_RM_E_BASE-5) |
| #define | EDMA3_RM_E_SPECIFIED_RES_NOT_AVAILABLE (EDMA3_RM_E_BASE-6) |
| #define | EDMA3_RM_E_ALL_RES_NOT_AVAILABLE (EDMA3_RM_E_BASE-7) |
| #define | EDMA3_RM_E_INVALID_STATE (EDMA3_RM_E_BASE-8) |
| #define | EDMA3_RM_E_MAX_RM_INST_OPENED (EDMA3_RM_E_BASE-9) |
| #define | EDMA3_RM_E_RM_MASTER_ALREADY_EXISTS (EDMA3_RM_E_BASE-10) |
| #define | EDMA3_RM_E_CALLBACK_ALREADY_REGISTERED (EDMA3_RM_E_BASE-11) |
| #define | EDMA3_RM_E_SEMAPHORE (EDMA3_RM_E_BASE-12) |
| #define | EDMA3_RM_E_FEATURE_UNSUPPORTED (EDMA3_RM_E_BASE-13) |
| #define | EDMA3_RM_E_RES_NOT_ALLOCATED (EDMA3_RM_E_BASE-14) |
Error Codes returned by the EDMA3 Resource Manager Layer
| #define EDMA3_RM_E_ALL_RES_NOT_AVAILABLE (EDMA3_RM_E_BASE-7) |
No Resource of specified type is available
| #define EDMA3_RM_E_BASE (-155) |
Resource Manager Error Codes base define
| #define EDMA3_RM_E_CALLBACK_ALREADY_REGISTERED (EDMA3_RM_E_BASE-11) |
Callback function already registered.
| #define EDMA3_RM_E_FEATURE_UNSUPPORTED (EDMA3_RM_E_BASE-13) |
Hardware feature NOT supported
| #define EDMA3_RM_E_INVALID_PARAM (EDMA3_RM_E_BASE-3) |
Invalid Parameter passed to API
| #define EDMA3_RM_E_INVALID_STATE (EDMA3_RM_E_BASE-8) |
Invalid State of EDMA3 RM Obj
| #define EDMA3_RM_E_MAX_RM_INST_OPENED (EDMA3_RM_E_BASE-9) |
Maximum no of Res Mgr Instances already Opened
| #define EDMA3_RM_E_OBJ_NOT_CLOSED (EDMA3_RM_E_BASE-1) |
Resource Manager Object Not Closed yet. So the object cannot be deleted.
| #define EDMA3_RM_E_OBJ_NOT_DELETED (EDMA3_RM_E_BASE) |
Resource Manager Object Not Deleted yet. So the object cannot be created.
| #define EDMA3_RM_E_OBJ_NOT_OPENED (EDMA3_RM_E_BASE-2) |
Resource Manager Object Not Opened yet So the object cannot be closed.
| #define EDMA3_RM_E_RES_ALREADY_FREE (EDMA3_RM_E_BASE-4) |
Resource requested for freeing is already free
| #define EDMA3_RM_E_RES_NOT_ALLOCATED (EDMA3_RM_E_BASE-14) |
EDMA3 Resource NOT allocated
| #define EDMA3_RM_E_RES_NOT_OWNED (EDMA3_RM_E_BASE-5) |
Resource requested for allocation/freeing is not owned
| #define EDMA3_RM_E_RM_MASTER_ALREADY_EXISTS (EDMA3_RM_E_BASE-10) |
More than one Res Mgr Master Instance NOT supported. Only 1 master can exist.
| #define EDMA3_RM_E_SEMAPHORE (EDMA3_RM_E_BASE-12) |
Semaphore related error
| #define EDMA3_RM_E_SPECIFIED_RES_NOT_AVAILABLE (EDMA3_RM_E_BASE-6) |
Resource is not available
1.4.7