EDMA3 Driver Error Codes
[EDMA3 Driver Interface Definition]

Usage of EDMA3 Driver. More...

Defines

#define EDMA3_DRV_E_BASE   (-128)
#define EDMA3_DRV_E_OBJ_NOT_DELETED   (EDMA3_DRV_E_BASE)
#define EDMA3_DRV_E_OBJ_NOT_CLOSED   (EDMA3_DRV_E_BASE-1)
#define EDMA3_DRV_E_OBJ_NOT_OPENED   (EDMA3_DRV_E_BASE-2)
#define EDMA3_DRV_E_RM_CLOSE_FAIL   (EDMA3_DRV_E_BASE-3)
#define EDMA3_DRV_E_DMA_CHANNEL_UNAVAIL   (EDMA3_DRV_E_BASE-4)
#define EDMA3_DRV_E_QDMA_CHANNEL_UNAVAIL   (EDMA3_DRV_E_BASE-5)
#define EDMA3_DRV_E_PARAM_SET_UNAVAIL   (EDMA3_DRV_E_BASE-6)
#define EDMA3_DRV_E_TCC_UNAVAIL   (EDMA3_DRV_E_BASE-7)
#define EDMA3_DRV_E_TCC_REGISTER_FAIL   (EDMA3_DRV_E_BASE-8)
#define EDMA3_DRV_E_CH_PARAM_BIND_FAIL   (EDMA3_DRV_E_BASE-9)
#define EDMA3_DRV_E_ADDRESS_NOT_ALIGNED   (EDMA3_DRV_E_BASE-10)
#define EDMA3_DRV_E_INVALID_PARAM   (EDMA3_DRV_E_BASE-11)
#define EDMA3_DRV_E_INVALID_STATE   (EDMA3_DRV_E_BASE-12)
#define EDMA3_DRV_E_INST_ALREADY_EXISTS   (EDMA3_DRV_E_BASE-13)
#define EDMA3_DRV_E_FIFO_WIDTH_NOT_SUPPORTED   (EDMA3_DRV_E_BASE-14)
#define EDMA3_DRV_E_SEMAPHORE   (EDMA3_DRV_E_BASE-15)

Detailed Description

Usage of EDMA3 Driver.

Error Codes returned by the EDMA3 Driver


Define Documentation

#define EDMA3_DRV_E_ADDRESS_NOT_ALIGNED   (EDMA3_DRV_E_BASE-10)

The address of the memory location passed as argument is not properly aligned. It should be 32 bytes aligned.

#define EDMA3_DRV_E_BASE   (-128)

EDMA3 Driver Error Codes Base define

#define EDMA3_DRV_E_CH_PARAM_BIND_FAIL   (EDMA3_DRV_E_BASE-9)

The binding of Channel and PaRAM Set failed

#define EDMA3_DRV_E_DMA_CHANNEL_UNAVAIL   (EDMA3_DRV_E_BASE-4)

The requested DMA Channel not available

#define EDMA3_DRV_E_FIFO_WIDTH_NOT_SUPPORTED   (EDMA3_DRV_E_BASE-14)

FIFO width not supported by the requested TC

#define EDMA3_DRV_E_INST_ALREADY_EXISTS   (EDMA3_DRV_E_BASE-13)

EDMA3 Driver instance already exists for the specified region

#define EDMA3_DRV_E_INVALID_PARAM   (EDMA3_DRV_E_BASE-11)

Invalid Parameter passed to API

#define EDMA3_DRV_E_INVALID_STATE   (EDMA3_DRV_E_BASE-12)

Invalid State of EDMA3 HW Obj

#define EDMA3_DRV_E_OBJ_NOT_CLOSED   (EDMA3_DRV_E_BASE-1)

EDMA3 Driver Object Not Closed yet. So it cannot be deleted.

#define EDMA3_DRV_E_OBJ_NOT_DELETED   (EDMA3_DRV_E_BASE)

EDMA3 Driver Object Not Deleted yet. So it cannot be created.

#define EDMA3_DRV_E_OBJ_NOT_OPENED   (EDMA3_DRV_E_BASE-2)

EDMA3 Driver Object Not Opened yet So it cannot be closed.

#define EDMA3_DRV_E_PARAM_SET_UNAVAIL   (EDMA3_DRV_E_BASE-6)

The requested PaRAM Set not available

#define EDMA3_DRV_E_QDMA_CHANNEL_UNAVAIL   (EDMA3_DRV_E_BASE-5)

The requested QDMA Channel not available

#define EDMA3_DRV_E_RM_CLOSE_FAIL   (EDMA3_DRV_E_BASE-3)

While closing EDMA3 Driver, Resource Manager Close Failed.

#define EDMA3_DRV_E_SEMAPHORE   (EDMA3_DRV_E_BASE-15)

Semaphore related error

#define EDMA3_DRV_E_TCC_REGISTER_FAIL   (EDMA3_DRV_E_BASE-8)

The registration of TCC failed

#define EDMA3_DRV_E_TCC_UNAVAIL   (EDMA3_DRV_E_BASE-7)

The requested TCC not available


Generated on Fri Sep 28 11:47:37 2007 for EDMA3 Driver by  doxygen 1.4.7