![]() |
![]() |
#include <iaudenc.h>
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size
parameter.
The size
field must be correctly set by the caller. See http://wiki.davincidsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | encodingPreset |
XDAS_Int32 | maxSampleRate |
XDAS_Int32 | maxBitrate |
XDAS_Int32 | maxNoOfCh |
XDAS_Int32 | dataEndianness |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Encoding Preset. See XDM_EncodingPreset.
Maximum sampling frequency in Hz. For example, if the maximum sampling frequency is 44.1 kHz, this field should be 44100.
Maximum bit rate in bits per second. For example, if the maximum bit rate is 128 kbps, set this field to 128000.
Maximum Channels. See IAUDIO_ChannelId.
Endianness of output data. See XDM_DataFormat.