xDM Speech/Voice Interface


Detailed Description

This is the xDM speech/voice interface shared between the various codecs.


Enumerations

enum  ISPEECH1_NullTrafficMode {
  ISPEECH1_NULLTRAFFICMODE_OFF = 0,
  ISPEECH1_NULLTRAFFICMODE_ON = 1,
  ISPEECH1_NULLTRAFFICMODE_DEFAULT = ISPEECH1_NULLTRAFFICMODE_OFF
}
 Null traffic channel setting. More...
enum  ISPEECH1_PostFilter {
  ISPEECH1_POSTFILTER_OFF = 0,
  ISPEECH1_POSTFILTER_ON = 1,
  ISPEECH1_POSTFILTER_DEFAULT = ISPEECH1_POSTFILTER_ON
}
 Post filter setting. More...
enum  ISPEECH1_VADFlag {
  ISPEECH1_VADFLAG_OFF = 0,
  ISPEECH1_VADFLAG_ON = 1,
  ISPEECH1_VADFLAG_DEFAULT = ISPEECH1_VADFLAG_ON
}
 Voice Activity Detection (VAD) setting. More...


Enumeration Type Documentation

enum ISPEECH1_NullTrafficMode

Null traffic channel setting.

See also:
ISPHENC1_InArgs.nullTrafficChannel.
Enumerator:
ISPEECH1_NULLTRAFFICMODE_OFF  Null traffic channel frames disabled, normal speech encoding is enabled.
ISPEECH1_NULLTRAFFICMODE_ON  Null traffic channel frames enabled.
ISPEECH1_NULLTRAFFICMODE_DEFAULT  Null traffic channel frames disabled, normal speech encoding is enabled.

enum ISPEECH1_PostFilter

Post filter setting.

These values are used for enabling/disabling the post filter.

Enumerator:
ISPEECH1_POSTFILTER_OFF  Post Filter disabled.
ISPEECH1_POSTFILTER_ON  Post Filter enabled.
ISPEECH1_POSTFILTER_DEFAULT  Post Filter enabled.

enum ISPEECH1_VADFlag

Voice Activity Detection (VAD) setting.

Enumerator:
ISPEECH1_VADFLAG_OFF  Voice Activity Detection off.
ISPEECH1_VADFLAG_ON  Voice Activity Detection on.
ISPEECH1_VADFLAG_DEFAULT  Voice Activity Detection on.


Copyright 2009, Texas Instruments Incorporated