![]() |
![]() |
Data Structures | |
| struct | IVIDENC1_Obj |
| This must be the first field of all IVIDENC1 instance objects. More... | |
| struct | IVIDENC1_Params |
| Defines the creation time parameters for all IVIDENC1 instance objects. More... | |
| struct | IVIDENC1_DynamicParams |
| This structure defines the algorithm parameters that can be modified after creation via control() calls. More... | |
| struct | IVIDENC1_InArgs |
| Defines the input arguments for all IVIDENC1 instance process function. More... | |
| struct | IVIDENC1_Status |
| Defines instance status parameters. More... | |
| struct | IVIDENC1_OutArgs |
| Defines the run time output arguments for all IVIDENC1 instance objects. More... | |
| struct | IVIDENC1_MbData |
| Defines the structure that contains macroblock related encoding parameter estimates. More... | |
| struct | IVIDENC1_Fxns |
| Defines all of the operations on IVIDENC1 objects. More... | |
Defines | |
| #define | IVIDENC1_EOK XDM_EOK |
| #define | IVIDENC1_EFAIL XDM_EFAIL |
| #define | IVIDENC1_EUNSUPPORTED XDM_EUNSUPPORTED |
Typedefs | |
| typedef IVIDENC1_Obj * | IVIDENC1_Handle |
| Opaque handle to an IVIDENC1 objects. | |
| typedef IALG_Cmd | IVIDENC1_Cmd |
| Defines the control commands for the IVIDENC1 module. | |
| #define IVIDENC1_EOK XDM_EOK |
Success.
| #define IVIDENC1_EFAIL XDM_EFAIL |
General failure.
| #define IVIDENC1_EUNSUPPORTED XDM_EUNSUPPORTED |
Request is unsupported.
| typedef struct IVIDENC1_Obj* IVIDENC1_Handle |
Opaque handle to an IVIDENC1 objects.
| typedef IALG_Cmd IVIDENC1_Cmd |
Defines the control commands for the IVIDENC1 module.