xDM 0.9 Audio Decoder Interface


Detailed Description

This is the xDM 0.9 Audio Decoder Interface.

Deprecated:
This 0.9 xDM audio decoder interface has been deprecated, and superceeded by the 1.00 xDM audio decoder interface.


Data Structures

struct  IAUDDEC_Obj
 This must be the first field of all IAUDDEC instance objects. More...
struct  IAUDDEC_Params
 Defines the creation time parameters for all IAUDDEC instance objects. More...
struct  IAUDDEC_DynamicParams
 This structure defines the codec parameters that can be modified after creation via control() calls. More...
struct  IAUDDEC_InArgs
 Defines the input arguments for all IAUDDEC instance process function. More...
struct  IAUDDEC_Status
 Defines instance status parameters (read-only). More...
struct  IAUDDEC_OutArgs
 Defines the run time output arguments for all IAUDDEC instance objects. More...
struct  IAUDDEC_Fxns
 Defines all of the operations on IAUDDEC objects. More...

Defines

#define IAUDDEC_CID   "ti.xdais.dm.IAUDDEC"
#define IAUDDEC_ERUNTIME   XDM_ERUNTIME
#define IAUDDEC_EOK   XDM_EOK
#define IAUDDEC_EFAIL   XDM_EFAIL

Typedefs

typedef IAUDDEC_ObjIAUDDEC_Handle
 Opaque handle to an IAUDDEC objects.
typedef IALG_Cmd IAUDDEC_Cmd
 Defines the control commands for the IAUDDEC module.


Define Documentation

#define IAUDDEC_CID   "ti.xdais.dm.IAUDDEC"

IAUDDEC Class ID

#define IAUDDEC_ERUNTIME   XDM_ERUNTIME

General runtime failure.

#define IAUDDEC_EOK   XDM_EOK

Success.

#define IAUDDEC_EFAIL   XDM_EFAIL

General failure.


Typedef Documentation

typedef struct IAUDDEC_Obj* IAUDDEC_Handle

Opaque handle to an IAUDDEC objects.

typedef IALG_Cmd IAUDDEC_Cmd

Defines the control commands for the IAUDDEC module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId

IAUDDEC_Fxns::control()


Copyright 2008, Texas Instruments Incorporated