![]() |
![]() |
Data Structures | |
| struct | IIMGDEC_CodecClassConfig |
| Definition of IIMGDEC codec class configurable parameters. More... | |
Defines | |
| #define | IMGDEC_EOK IIMGDEC_EOK |
| #define | IMGDEC_EFAIL IIMGDEC_EFAIL |
| #define | IMGDEC_ERUNTIME IIMGDEC_ERUNTIME |
| #define | IMGDEC_ETIMEOUT VISA_ETIMEOUT |
| #define | IMGDEC_FOREVER VISA_FOREVER |
Typedefs | |
| typedef IIMGDEC_Status | IMGDEC_Status |
| typedef VISA_Handle | IMGDEC_Handle |
| Opaque handle to a IMGDEC codec. | |
| typedef IIMGDEC_Params | IMGDEC_Params |
| This structure defines the parameters necessary to create an instance of a Image Decoder object. | |
| typedef IIMGDEC_InArgs | IMGDEC_InArgs |
| typedef IIMGDEC_OutArgs | IMGDEC_OutArgs |
| typedef IIMGDEC_Cmd | IMGDEC_Cmd |
| typedef IIMGDEC_DynamicParams | IMGDEC_DynamicParams |
Functions | |
| IMGDEC_Handle | IMGDEC_create (Engine_Handle e, String name, IMGDEC_Params *params) |
| Create an instance of an image decoder algorithm. | |
| Int32 | IMGDEC_process (IMGDEC_Handle handle, XDM_BufDesc *inBufs, XDM_BufDesc *outBufs, IMGDEC_InArgs *inArgs, IMGDEC_OutArgs *outArgs) |
| Execute the "process" method in this instance of a image decoder algorithm. | |
| Int32 | IMGDEC_control (IMGDEC_Handle handle, IMGDEC_Cmd id, IMGDEC_DynamicParams *params, IMGDEC_Status *status) |
| Execute the "control" method in this instance of a image decoder algorithm. | |
| Void | IMGDEC_delete (IMGDEC_Handle handle) |
| Delete the instance of a image decoder algorithm. | |
| XDAS_Int32 | IMGDEC_processAsync (IMGDEC_Handle handle, XDM_BufDesc *inBufs, XDM_BufDesc *outBufs, IMGDEC_InArgs *inArgs, IMGDEC_OutArgs *outArgs) |
| Perform asynchronous submission to this instance of a image decoder algorithm. | |
| XDAS_Int32 | IMGDEC_processWait (IMGDEC_Handle handle, XDM_BufDesc *inBufs, XDM_BufDesc *outBufs, IMGDEC_InArgs *inArgs, IMGDEC_OutArgs *outArgs, UInt timeout) |
| Wait for a return message from a previous invocation of IMGDEC_processAsync() in this instance of an image decoder algorithm. | |
| #define IMGDEC_EOK IIMGDEC_EOK |
Success.
| #define IMGDEC_EFAIL IIMGDEC_EFAIL |
General failure.
| #define IMGDEC_ERUNTIME IIMGDEC_ERUNTIME |
General runtime failure.
| #define IMGDEC_ETIMEOUT VISA_ETIMEOUT |
| #define IMGDEC_FOREVER VISA_FOREVER |
| typedef IIMGDEC_Status IMGDEC_Status |
Defines instance status parameters (read-only).
size parameter.
The size field must be correctly set by the caller.
| typedef VISA_Handle IMGDEC_Handle |
Opaque handle to a IMGDEC codec.
| typedef struct IIMGDEC_Params IMGDEC_Params |
This structure defines the parameters necessary to create an instance of a Image Decoder object.
| typedef IIMGDEC_InArgs IMGDEC_InArgs |
Defines the input arguments for all IIMGDEC instance process() function.
size parameter.
The size field must be correctly set by the caller.
| typedef IIMGDEC_OutArgs IMGDEC_OutArgs |
Defines the run time output arguments for all IIMGDEC instance objects.
size parameter.
The size field must be correctly set by the caller.
| typedef IIMGDEC_Cmd IMGDEC_Cmd |
Defines the control commands for the IIMGDEC module.
This structure defines the codec parameters that can be modified after creation via control() calls.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller.
| IMGDEC_Handle IMGDEC_create | ( | Engine_Handle | e, | |
| String | name, | |||
| IMGDEC_Params * | params | |||
| ) |
Create an instance of an image decoder algorithm.
Instance handles must not be concurrently accessed by multiple threads; each thread must either obtain its own handle (via IMGDEC_create()) or explicitly serialize access to a shared handle.
| [in] | e | Handle to an opened engine. |
| [in] | name | String identifier of the type of image decoder to create. |
| [in] | params | Creation parameters. |
| NULL | An error has occurred. | |
| non-NULL | The handle to the newly created image decoder instance. |
In general, name is the name of the codec configured by the system integrator. However, an optional "argument string" may be appended to the codec name, to allow the codec's configured priority and/or the heaps where its memory will be allocated, to be overridden. This optional argument string is of the form ":priority", ":priority:flag", or "::flag".
priority is the new priority to create the codec with.
The flag must be either 0 or 1, and if 1, all memory allocated for the codec will be in the heap that corresponds to IALG_EXTERNAL. If flag is 0, the memory for the codec will be allocated from the heaps it has requested. For example, if a codec named "mp3" has been configured into the system, setting name to "mp3:4" would cause the codec to be created at priority 4, instead of whatever priority was configured. This feature is useful if more than one instance of the codec are to be created at different priorities.
The flag can be used to prevent the codec from using any internal memory, for example, if it is to be run at the same time as another codec that must use internal memory, and there is insufficient internal memory for both.
| Int32 IMGDEC_process | ( | IMGDEC_Handle | handle, | |
| XDM_BufDesc * | inBufs, | |||
| XDM_BufDesc * | outBufs, | |||
| IMGDEC_InArgs * | inArgs, | |||
| IMGDEC_OutArgs * | outArgs | |||
| ) |
Execute the "process" method in this instance of a image decoder algorithm.
| [in] | handle | Handle to a created image decoder instance. |
| [in] | inBufs | A buffer descriptor containing input buffers. |
| [out] | outBufs | A buffer descriptor containing output buffers. |
| [in] | inArgs | Input Arguments. |
| [out] | outArgs | Output Arguments. |
handle is a valid (non-NULL) image decoder handle and the image decoder is in the created state.| IMGDEC_EOK | Success. | |
| IMGDEC_EFAIL | Failure. | |
| IMGDEC_ERUNTIME | Internal Runtime Error. |
This is a blocking call, and will return after the data has been decoded.
The buffers supplied to IMGDEC_process() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
| Int32 IMGDEC_control | ( | IMGDEC_Handle | handle, | |
| IMGDEC_Cmd | id, | |||
| IMGDEC_DynamicParams * | params, | |||
| IMGDEC_Status * | status | |||
| ) |
Execute the "control" method in this instance of a image decoder algorithm.
| [in] | handle | Handle to a created image decoder instance. |
| [in] | id | Command id for xDM control operation. |
| [in] | params | Runtime control parameters used for decoding. |
| [out] | status | Status info upon completion of decode operation. |
handle is a valid (non-NULL) image decoder handle and the image decoder is in the created state.| IMGDEC_EOK | Success. | |
| IMGDEC_EFAIL | Failure. | |
| IMGDEC_ERUNTIME | Internal Runtime Error. |
| Void IMGDEC_delete | ( | IMGDEC_Handle | handle | ) |
Delete the instance of a image decoder algorithm.
| [in] | handle | Handle to a created image decoder instance. |
handle is a valid (non-NULL) handle which is in the created state.| XDAS_Int32 IMGDEC_processAsync | ( | IMGDEC_Handle | handle, | |
| XDM_BufDesc * | inBufs, | |||
| XDM_BufDesc * | outBufs, | |||
| IMGDEC_InArgs * | inArgs, | |||
| IMGDEC_OutArgs * | outArgs | |||
| ) |
Perform asynchronous submission to this instance of a image decoder algorithm.
| [in] | handle | Handle to a created image decoder instance. |
| [in] | inBufs | A buffer descriptor containing input buffers. |
| [out] | outBufs | A buffer descriptor containing output buffers. |
| [in] | inArgs | Input Arguments. |
| [out] | outArgs | Output Arguments. |
handle is a valid (non-NULL) image decoder handle and the image decoder is in the created state.| IMGDEC_EOK | Success. | |
| IMGDEC_EFAIL | Failure. | |
| IMGDEC_EUNSUPPORTED | Unsupported request. |
The buffers supplied to IMGDEC_processAsync() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
| XDAS_Int32 IMGDEC_processWait | ( | IMGDEC_Handle | handle, | |
| XDM_BufDesc * | inBufs, | |||
| XDM_BufDesc * | outBufs, | |||
| IMGDEC_InArgs * | inArgs, | |||
| IMGDEC_OutArgs * | outArgs, | |||
| UInt | timeout | |||
| ) |
Wait for a return message from a previous invocation of IMGDEC_processAsync() in this instance of an image decoder algorithm.
| [in] | handle | Handle to a created image decoder instance. |
| [in] | inBufs | A buffer descriptor containing input buffers. |
| [out] | outBufs | A buffer descriptor containing output buffers. |
| [in] | inArgs | Input Arguments. |
| [out] | outArgs | Output Arguments. |
| [in] | timeout | Amount of "time" to wait (from 0 -> IMGDEC_FOREVER) |
handle is a valid (non-NULL) image decoder handle and the image decoder is in the created state.| IMGDEC_EOK | Success. | |
| IMGDEC_EFAIL | Failure. | |
| IMGDEC_EUNSUPPORTED | Unsupported request. | |
| IMGDEC_ETIMEOUT | Operation timed out. |
"Polling" is supported by using a timeout of 0. Waiting forever is supported by using a timeout of IMGDEC_EFOREVER.
There must have previously been an invocation of the IMGDEC_processAsync() API.
The buffers supplied to IMGDEC_processAsync() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.