![]() |
![]() |
Defines | |
| #define | IMGDEC1_EOK IIMGDEC1_EOK |
| #define | IMGDEC1_EFAIL IIMGDEC1_EFAIL |
| #define | IMGDEC1_EUNSUPPORTED IIMGDEC1_EUNSUPPORTED |
Typedefs | |
| typedef VISA_Handle | IMGDEC1_Handle |
| Opaque handle to a IMGDEC1 codec. | |
| typedef IIMGDEC1_Params | IMGDEC1_Params |
| This structure defines the parameters necessary to create an instance of an image decoder object. | |
| typedef IIMGDEC1_InArgs | IMGDEC1_InArgs |
| typedef IIMGDEC1_OutArgs | IMGDEC1_OutArgs |
| typedef IIMGDEC1_Cmd | IMGDEC1_Cmd |
| typedef IIMGDEC1_Status | IMGDEC1_Status |
| typedef IIMGDEC1_DynamicParams | IMGDEC1_DynamicParams |
Functions | |
| Int32 | IMGDEC1_control (IMGDEC1_Handle handle, IMGDEC1_Cmd id, IMGDEC1_DynamicParams *params, IMGDEC1_Status *status) |
| Execute the control() method in this instance of an image1 decoder algorithm. | |
| IMGDEC1_Handle | IMGDEC1_create (Engine_Handle e, String name, IMGDEC1_Params *params) |
| Create an instance of an image decoder algorithm. | |
| Void | IMGDEC1_delete (IMGDEC1_Handle handle) |
| Delete the instance of an image decoder algorithm. | |
| Int32 | IMGDEC1_process (IMGDEC1_Handle handle, XDM1_BufDesc *inBufs, XDM1_BufDesc *outBufs, IMGDEC1_InArgs *inArgs, IMGDEC1_OutArgs *outArgs) |
| Execute the process() method in this instance of an image decoder algorithm. | |
| #define IMGDEC1_EOK IIMGDEC1_EOK |
Success.
| #define IMGDEC1_EFAIL IIMGDEC1_EFAIL |
General failure.
| #define IMGDEC1_EUNSUPPORTED IIMGDEC1_EUNSUPPORTED |
Request is unsupported.
| typedef VISA_Handle IMGDEC1_Handle |
Opaque handle to a IMGDEC1 codec.
| typedef struct IIMGDEC1_Params IMGDEC1_Params |
This structure defines the parameters necessary to create an instance of an image decoder object.
| typedef IIMGDEC1_InArgs IMGDEC1_InArgs |
Defines the input arguments for all IIMGDEC1 instance process() function.
size parameter.
The size field must be correctly set by the caller.
| typedef IIMGDEC1_OutArgs IMGDEC1_OutArgs |
Defines the run time output arguments for all IIMGDEC1 instance objects.
size parameter.
The size field must be correctly set by the caller.
| typedef IIMGDEC1_Cmd IMGDEC1_Cmd |
Defines the control commands for the IIMGDEC1 module.
| typedef IIMGDEC1_Status IMGDEC1_Status |
Defines instance status parameters.
size parameter.
The size field must be correctly set by the caller.
This structure defines the codec parameters that can be modified after creation via control() calls.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller.
| Int32 IMGDEC1_control | ( | IMGDEC1_Handle | handle, | |
| IMGDEC1_Cmd | id, | |||
| IMGDEC1_DynamicParams * | params, | |||
| IMGDEC1_Status * | status | |||
| ) |
Execute the control() method in this instance of an image1 decoder algorithm.
| [in] | handle | Handle to a created image decoder instance. |
| [in] | id | Command id for xDM control operation. |
| [in] | params | Runtime control parameters used for decoding. |
| [out] | status | Status info upon completion of decode operation. |
handle is a valid (non-NULL) image decoder handle and the image decoder is in the created state.| IMGDEC1_EOK | Success. | |
| IMGDEC1_EFAIL | Failure. | |
| IMGDEC1_EUNSUPPORTED | Unsupported request. |
IIMGDEC1_Fxns()control()
| IMGDEC1_Handle IMGDEC1_create | ( | Engine_Handle | e, | |
| String | name, | |||
| IMGDEC1_Params * | params | |||
| ) |
Create an instance of an image decoder algorithm.
Instance handles must not be concurrently accessed by multiple threads; each thread must either obtain its own handle (via IMGDEC1_create()) or explicitly serialize access to a shared handle.
| [in] | e | Handle to an opened engine. |
| [in] | name | String identifier of the type of image decoder. to create. |
| [in] | params | Creation parameters. |
| NULL | An error has occurred. | |
| non-NULL | The handle to the newly created image decoder instance. |
params is optional. If it's not supplied, codec-specific default params will be used.Depending on the configuration of the engine opened, this call may create a local or remote instance of the image decoder.
In general, name is the name of the codec configured by the system integrator. However, an optional "argument string" may be appended to the codec name, to allow the codec's configured priority and/or the heaps where its memory will be allocated, to be overridden. This optional argument string is of the form ":priority", ":priority:flag", or "::flag", where priority is the new priority to create the codec with. The flag must be either 0 or 1, and if 1, all memory allocated for the codec will be in the heap that corresponds to IALG_EXTERNAL. If flag is 0, the memory for the codec will be allocated from the heaps it has requested. For example, if a codec named "mp3" has been configured into the system, setting name to "mp3:4" would cause the codec to be created at priority 4, instead of whatever priority was configured. This feature is useful if more than one instance of the codec are to be created at different priorities. The flag can be used to prevent the codec from using any internal memory, for example, if it is to be run at the same time as another codec that must use internal memory, and there is insufficient internal memory for both.
| Void IMGDEC1_delete | ( | IMGDEC1_Handle | handle | ) |
Delete the instance of an image decoder algorithm.
| [in] | handle | Handle to a created image decoder instance. |
handle is a valid (non-NULL) handle which is in the created state.| Int32 IMGDEC1_process | ( | IMGDEC1_Handle | handle, | |
| XDM1_BufDesc * | inBufs, | |||
| XDM1_BufDesc * | outBufs, | |||
| IMGDEC1_InArgs * | inArgs, | |||
| IMGDEC1_OutArgs * | outArgs | |||
| ) |
Execute the process() method in this instance of an image decoder algorithm.
| [in] | handle | Handle to a created image decoder instance. |
| [in] | inBufs | A buffer descriptor containing input buffers. |
| [out] | outBufs | A buffer descriptor containing output buffers. |
| [in] | inArgs | Input Arguments. |
| [out] | outArgs | Output Arguments. |
handle is a valid (non-NULL) image decoder handle and the image decoder is in the created state.| IMGDEC1_EOK | Success. | |
| IMGDEC1_EFAIL | Failure. | |
| IMGDEC1_EUNSUPPORTED | Unsupported request. |
The buffers supplied to IMGDEC1_process() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
IIMGDEC1_Fxns()process()