USBLibAPIGuide
1.00.00.01
|
#include <usbdhidsensor.h>
Data Fields | |
const uint16_t | ui16VID |
The vendor ID that this device is to present in the device descriptor. More... | |
const uint16_t | ui16PID |
The product ID that this device is to present in the device descriptor. More... | |
const uint16_t | ui16MaxPowermA |
The maximum power consumption of the device, expressed in milliamps. More... | |
const uint8_t | ui8PwrAttributes |
const tUSBCallback | pfnCallback |
void * | pvCBData |
const uint8_t *const * | ppui8StringDescriptors |
const uint32_t | ui32NumStringDescriptors |
tUSBDSensorInstance | sPrivateData |
This structure is used by the application to define operating parameters for the HID sensor device.
const uint16_t tUSBDHIDSensorDevice::ui16VID |
The vendor ID that this device is to present in the device descriptor.
Referenced by USBDHIDSensorCompositeInit().
const uint16_t tUSBDHIDSensorDevice::ui16PID |
The product ID that this device is to present in the device descriptor.
Referenced by USBDHIDSensorCompositeInit().
const uint16_t tUSBDHIDSensorDevice::ui16MaxPowermA |
The maximum power consumption of the device, expressed in milliamps.
Referenced by USBDHIDSensorCompositeInit().
const uint8_t tUSBDHIDSensorDevice::ui8PwrAttributes |
Indicates whether the device is self- or bus-powered and whether or not it supports remote wakeup. Valid values are USB_CONF_ATTR_SELF_PWR or USB_CONF_ATTR_BUS_PWR, optionally ORed with USB_CONF_ATTR_RWAKE.
Referenced by USBDHIDSensorCompositeInit().
const tUSBCallback tUSBDHIDSensorDevice::pfnCallback |
A pointer to the callback function which is called to notify the application of general events and those related to reception of Output and Feature reports via the (optional) interrupt OUT endpoint.
Referenced by USBDHIDSensorCompositeInit(), and USBDHIDSensorInit().
void* tUSBDHIDSensorDevice::pvCBData |
A client-supplied pointer which is sent as the first parameter in all calls made to the sensor callback, pfnCallback.
const uint8_t* const* tUSBDHIDSensorDevice::ppui8StringDescriptors |
A pointer to the string descriptor array for this device. This array must contain the following string descriptor pointers in this order. Language descriptor, Manufacturer name string (language 1), Product name string (language 1), Serial number string (language 1),HID Interface description string (language 1), Configuration description string (language 1).
If supporting more than 1 language, the descriptor block (except for string descriptor 0) must be repeated for each language defined in the language descriptor.
Referenced by USBDHIDSensorCompositeInit(), and USBDHIDSensorInit().
const uint32_t tUSBDHIDSensorDevice::ui32NumStringDescriptors |
The number of descriptors provided in the ppStringDescriptors array. This must be (1 + (5 * (num languages))).
tUSBDSensorInstance tUSBDHIDSensorDevice::sPrivateData |
The private instance data for this device. This memory must remain accessible for as long as the sensor device is in use and must not be modified by any code outside the HID sensor driver.
Referenced by USBDHIDSensorCompositeInit(), USBDHIDSensorInit(), USBDHIDSensorSendReport(), and USBDHIDSensorTerm().