![]() |
![]() |
USBLibAPIGuide
1.00.00.01
|
#include <usbdhidgamepad.h>
Data Fields | |
const uint16_t | ui16VID |
The vendor ID that this device is to present in the device descriptor. More... | |
const uint16_t | ui16PID |
The product ID that this device is to present in the device descriptor. More... | |
const uint16_t | ui16MaxPowermA |
The maximum power consumption of the device, expressed in milliamps. More... | |
const uint8_t | ui8PwrAttributes |
const tUSBCallback | pfnCallback |
void * | pvCBData |
const uint8_t *const * | ppui8StringDescriptors |
const uint32_t | ui32NumStringDescriptors |
const uint8_t * | pui8ReportDescriptor |
const uint32_t | ui32ReportSize |
tUSBDGamepadInstance | sPrivateData |
This structure is used by the application to define operating parameters for the HID game device.
const uint16_t tUSBDHIDGamepadDevice::ui16VID |
The vendor ID that this device is to present in the device descriptor.
Referenced by USBDHIDGamepadCompositeInit().
const uint16_t tUSBDHIDGamepadDevice::ui16PID |
The product ID that this device is to present in the device descriptor.
Referenced by USBDHIDGamepadCompositeInit().
const uint16_t tUSBDHIDGamepadDevice::ui16MaxPowermA |
The maximum power consumption of the device, expressed in milliamps.
Referenced by USBDHIDGamepadCompositeInit().
const uint8_t tUSBDHIDGamepadDevice::ui8PwrAttributes |
Indicates whether the device is self- or bus-powered and whether or not it supports remote wake up. Valid values are USB_CONF_ATTR_SELF_PWR or USB_CONF_ATTR_BUS_PWR, optionally ORed with USB_CONF_ATTR_RWAKE.
Referenced by USBDHIDGamepadCompositeInit().
const tUSBCallback tUSBDHIDGamepadDevice::pfnCallback |
A pointer to the callback function that is called to notify the application of general events. This pointer must point to a valid function.
Referenced by USBDHIDGamepadCompositeInit(), and USBDHIDGamepadInit().
void* tUSBDHIDGamepadDevice::pvCBData |
A client-supplied pointer that is sent as the first parameter in all calls made to the pfnCallback gamedevice callback function.
const uint8_t* const* tUSBDHIDGamepadDevice::ppui8StringDescriptors |
A pointer to the string descriptor array for this device. This array must contain the following string descriptor pointers in this order: Language descriptor, Manufacturer name string (language 1), Product name string (language 1), Serial number string (language 1),HID Interface description string (language 1), Configuration description string (language 1).
If supporting more than 1 language, the descriptor block (except for string descriptor 0) must be repeated for each language defined in the language descriptor.
Referenced by USBDHIDGamepadCompositeInit(), and USBDHIDGamepadInit().
const uint32_t tUSBDHIDGamepadDevice::ui32NumStringDescriptors |
The number of descriptors provided in the ppStringDescriptors array, which must be (1 + (5 * (number of languages))).
const uint8_t* tUSBDHIDGamepadDevice::pui8ReportDescriptor |
Optional report descriptor if the application wants to use a custom descriptor.
const uint32_t tUSBDHIDGamepadDevice::ui32ReportSize |
The size of the optional report descriptor define in pui8ReportDescriptor.
tUSBDGamepadInstance tUSBDHIDGamepadDevice::sPrivateData |
The private instance data for this device. This memory must remain accessible for as long as the game device is in use and must not be modified by any code outside the HID game device driver.
Referenced by USBDHIDGamepadCompositeInit(), USBDHIDGamepadInit(), USBDHIDGamepadSendReport(), and USBDHIDGamepadTerm().