#include <usbdcdc.h>
§ ui32USBBase
uint32_t tCDCSerInstance::ui32USBBase |
§ sDevInfo
§ iCDCRxState
volatile tCDCState tCDCSerInstance::iCDCRxState |
§ iCDCTxState
volatile tCDCState tCDCSerInstance::iCDCTxState |
§ iCDCRequestState
volatile tCDCState tCDCSerInstance::iCDCRequestState |
§ iCDCInterruptState
volatile tCDCState tCDCSerInstance::iCDCInterruptState |
§ ui8PendingRequest
volatile uint8_t tCDCSerInstance::ui8PendingRequest |
§ ui16BreakDuration
uint16_t tCDCSerInstance::ui16BreakDuration |
§ ui16ControlLineState
uint16_t tCDCSerInstance::ui16ControlLineState |
§ ui16SerialState
uint16_t tCDCSerInstance::ui16SerialState |
§ ui16DeferredOpFlags
volatile uint16_t tCDCSerInstance::ui16DeferredOpFlags |
§ ui16LastTxSize
uint16_t tCDCSerInstance::ui16LastTxSize |
§ sLineCoding
tLineCoding tCDCSerInstance::sLineCoding |
§ bRxBlocked
volatile bool tCDCSerInstance::bRxBlocked |
§ bControlBlocked
volatile bool tCDCSerInstance::bControlBlocked |
§ bConnected
volatile bool tCDCSerInstance::bConnected |
§ ui8ControlEndpoint
uint8_t tCDCSerInstance::ui8ControlEndpoint |
§ ui8BulkINEndpoint
uint8_t tCDCSerInstance::ui8BulkINEndpoint |
§ ui8BulkOUTEndpoint
uint8_t tCDCSerInstance::ui8BulkOUTEndpoint |
§ ui8InterfaceControl
uint8_t tCDCSerInstance::ui8InterfaceControl |
§ ui8InterfaceData
uint8_t tCDCSerInstance::ui8InterfaceData |
The documentation for this struct was generated from the following file: