#include <usbdbulk.h>
§ ui32USBBase
      
        
          | uint32_t tBulkInstance::ui32USBBase | 
        
      
 
 
§ sDevInfo
§ iBulkRxState
§ iBulkTxState
§ ui16DeferredOpFlags
      
        
          | volatile uint16_t tBulkInstance::ui16DeferredOpFlags | 
        
      
 
 
§ ui16LastTxSize
      
        
          | uint16_t tBulkInstance::ui16LastTxSize | 
        
      
 
 
§ bConnected
      
        
          | volatile bool tBulkInstance::bConnected | 
        
      
 
 
§ ui8INEndpoint
      
        
          | uint8_t tBulkInstance::ui8INEndpoint | 
        
      
 
 
§ ui8OUTEndpoint
      
        
          | uint8_t tBulkInstance::ui8OUTEndpoint | 
        
      
 
 
§ ui8Interface
      
        
          | uint8_t tBulkInstance::ui8Interface | 
        
      
 
 
The documentation for this struct was generated from the following file: