Macros
values that can be given to the

Macros

#define COMP0_OUTPUT_PIN_PD0   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 0, 0)
 
#define COMP0_OUTPUT_PIN_PL2   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTL, 2, 0)
 
#define COMP1_OUTPUT_PIN_PD1   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 1, 0)
 
#define COMP1_OUTPUT_PIN_PL3   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTL, 3, 0)
 
#define COMP2_OUTPUT_PIN_PD2   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 2, 0)
 
#define COMP_NO_OUTPUT   (0)
 

Detailed Description

outputPin field of ComparatorMSP432E4 Hardware Attributes to select the output pin of a given comparator. Comparator 2 only has a single output option.

Macro Definition Documentation

§ COMP0_OUTPUT_PIN_PD0

#define COMP0_OUTPUT_PIN_PD0   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 0, 0)

§ COMP0_OUTPUT_PIN_PL2

#define COMP0_OUTPUT_PIN_PL2   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTL, 2, 0)

§ COMP1_OUTPUT_PIN_PD1

#define COMP1_OUTPUT_PIN_PD1   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 1, 0)

§ COMP1_OUTPUT_PIN_PL3

#define COMP1_OUTPUT_PIN_PL3   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTL, 3, 0)

§ COMP2_OUTPUT_PIN_PD2

#define COMP2_OUTPUT_PIN_PD2   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 2, 0)

§ COMP_NO_OUTPUT

#define COMP_NO_OUTPUT   (0)
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale