Modules | |
Status Codes | |
Macros | |
#define | CAN_CMD_RESERVED (32) |
#define | CAN_STATUS_RESERVED (-32) |
These CAN macros are reservations for CAN.h
#define CAN_CMD_RESERVED (32) |
Common CAN_control command code reservation offset. CAN driver implementations should offset command codes with CAN_CMD_RESERVED growing positively
Example implementation specific command codes:
#define CAN_STATUS_RESERVED (-32) |
Common CAN_control status code reservation offset. CAN driver implementations should offset status codes with CAN_STATUS_RESERVED growing negatively.
Example implementation specific status codes: