Data Structures
Here are the data structures with brief descriptions:
 C_NoRTOS_ConfigNoRTOS framework global configuration
 CADC_Config_ADC driver's custom configuration structure
 CADC_FxnTableThe definition of an ADC function table that contains the required set of functions to control a specific ADC driver implementation
 CADC_ParamsADC Parameters used with ADC_open()
 CADCBuf_Config_ADC driver's custom configuration structure
 CADCBuf_ConversionDefines a conversion to be used with ADCBuf_convert()
 CADCBuf_FxnTableThe definition of an ADCBuf function table that contains the required set of functions to control a specific ADC driver implementation
 CADCBuf_ParamsADCBuf parameters used with ADCBuf_open()
 CADCBufMSP432E4_ChannelsADCBufMSP432E4 Channel Settings
 CADCBufMSP432E4_HWAttrsV1ADCBufMSP432E4 Hardware attributes
 CADCBufMSP432E4_Object
 CADCBufMSP432E4_ParamsExtensionMSP432E4 ADCBuf_Params Parameter Extensions
 CADCMSP432E4_HWAttrsV1ADCMSP432E4 Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For SimpleLink these definitions are found in:
 CADCMSP432E4_ObjectADCMSP432 Object
 CAESCBC_Config_AESCBC Global configuration
 CAESCBC_OperationStruct containing the parameters required for encrypting/decrypting a message
 CAESCBC_ParamsCBC Parameters
 CAESCBCMSP432E4_HWAttrsHardware-specific configuration attributes
 CAESCCM_ConfigAESCCM Global configuration
 CAESCCM_OperationStruct containing the parameters required for encrypting/decrypting and authenticating/verifying a message
 CAESCCM_ParamsCCM Parameters
 CAESCCMMSP432E4_HWAttrsHardware-specific configuration attributes
 CAESCTR_ConfigAESCTR Global configuration
 CAESCTR_OperationStruct containing the parameters required for encrypting/decrypting a message
 CAESCTR_ParamsCTR Parameters
 CAESCTRDRBG_ConfigAESCTRDRBG Global configuration
 CAESCTRDRBG_ParamsAESCTRDRBG Parameters
 CAESCTRDRBGXX_HWAttrsAESCTRDRBGXX Hardware Attributes
 CAESCTRDRBGXX_ObjectAESCTRDRBGXX Object
 CAESCTRMSP432E4_HWAttrsHardware-specific configuration attributes
 CAESECB_ConfigAESECB Global configuration
 CAESECB_OperationStruct containing the parameters required for encrypting/decrypting and a message
 CAESECB_ParamsECB Parameters
 CAESECBMSP432E4_HWAttrsHardware-specific configuration attributes
 CAESGCM_ConfigAESGCM Global configuration
 CAESGCM_OperationStruct containing the parameters required for encrypting/decrypting and authenticating/verifying a message
 CAESGCM_ParamsGCM Parameters
 CAESGCMMSP432E4_HWAttrsHardware-specific configuration attributes
 CButton_ConfigButton configuration
 CButton_HWAttrsHardware specific settings for a button
 CButton_ObjectInternal to Button module. Members should not be accessed by the application
 CButton_ParamsButton Parameters
 CCAN_Config_CAN Global configuration
 Ccan_frameCAN frame structure
 CCAN_FxnTableThe definition of a CAN function table that contains the required set of functions to control a specific CAN driver implementation
 CCAN_ParamsCAN Parameters
 CCANMSP432E4_HWAttrsCANMSP432E4 Hardware attributes
 CCANMSP432E4_ObjectCANMSP432E4 Object
 CComparator_Config_Comparator driver's custom configuration structure
 CComparator_FxnTableThe definition of a comparator function table that contains the required set of functions to control a specific comparator driver implementation
 CComparator_ParamsComparator Parameters
 CComparatorMSP432E4_HWAttrsComparatorMSP432E4 Hardware attributes
 CComparatorMSP432E4_ObjectComparatorMSP432E4 Object
 CCRC_ConfigCRC Global configuration
 CCRC_ParamsStruct containing the parameters required for calculating the CRC of a data block. Default values can be set with CRC_Params_init
 CCRCMSP432E4_ObjectCRCMSP432E4 Hardware Attributes
 CCryptoKeyCryptoKey datastructure
 CCryptoKey_KeyBlobKeyblob CryptoKey datastructure
 CCryptoKey_KeyStoreKey store CryptoKey datastructure
 CCryptoKey_PlaintextPlaintext CryptoKey datastructure
 CDisplay_ConfigDisplay Global configuration
 CDisplay_FxnTableThe definition of a Display function table that contains the required set of functions to control a specific Display driver implementation
 CDisplay_ParamsDisplay Parameters
 CDisplayGrLib_Object
 CDisplayHost_HWAttrsDisplayHost Attributes
 CDisplayHost_ObjectDisplayHost Object
 CDisplaySharp_HWAttrsV1
 CDisplaySharp_Object
 CDisplaySharpColor_tForeground and background color struct, compatible with GrLib
 CDisplayUart2_HWAttrsDisplayUart2 Attributes
 CDisplayUart2_ObjectDisplayUart2 Object
 CDisplayUart_HWAttrsDisplayUart Attributes
 CDisplayUart_ObjectDisplayUart Object
 CEMACMSP432E4_HWAttrsEMACMSP432E4 Hardware attributes
 CGPIOMSP432E4_ConfigGPIO device specific driver configuration structure
 CI2C_Config_I2C driver's custom configuration structure
 CI2C_FxnTableThe definition of an I2C function table that contains the required set of functions to control a specific I2C driver implementation
 CI2C_ParamsI2C parameters used with I2C_open()
 CI2C_TransactionDefines a transaction to be used with I2C_transfer() or I2C_transferTimeout()
 CI2CMSP432E4_HWAttrsI2CMSP432E4 Hardware attributes
 CI2CMSP432E4_ObjectI2CMSP432E4 Object
 CLED_ConfigLED configuration
 CLED_HWAttrsHardware specific settings for a LED module
 CLED_ObjectLED Object structure
 CLED_ParamsLED Parameters
 CList_Elem_
 CList_List
 CNVS_AttrsNVS attributes
 CNVS_Config_NVS Global configuration
 CNVS_FxnTableThe definition of an NVS function table that contains the required set of functions to control a specific NVS driver implementation
 CNVS_ParamsNVS Parameters
 CNVSMSP432E4_HWAttrsNVSMSP432E4 attributes
 CNVSMSP432E4_Object
 CNVSRAM_HWAttrsNVSRAM Hardware Attributes
 CNVSRAM_Object
 CNVSSPI25X_HWAttrsNVSSPI25X attributes
 CNVSSPI25X_Object
 CPower_NotifyObjPower notify object structure
 CPowerMSP432E4_ConfigPower global configuration structure
 CPWM_Config_PWM Global configuration
 CPWM_FxnTableThe definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation
 CPWM_ParamsPWM Parameters
 CPWMMSP432E4_HWAttrsPWMMSP432E4 Hardware attributes
 CPWMMSP432E4_ObjectPWMMSP432E4 Object
 CPWMMSP432E4_StatusPWMMSP432E4_Status
 CRingBuf_Object
 CSD_Config_SD Global configuration
 CSD_FxnTableThe definition of a SD function table that contains the required set of functions to control a specific SD driver implementation
 CSD_ParamsSD Parameters
 CSDFatFS_ConfigSDFatFS Global configuration
 CSDFatFS_ObjectSDFatFS Object The application must not access any member variables of this structure!
 CSDSPI_HWAttrsSDSPI Hardware attributes
 CSDSPI_ObjectSDSPI Object
 CSHA2_ConfigSHA2 Global configuration
 CSHA2_ParamsSHA2 Parameters
 CSHA2MSP432E4_HWAttrsHardware-specific configuration attributes
 CSPI_Config_SPI Global configuration
 CSPI_FxnTableThe definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation
 CSPI_ParamsSPI Parameters
 CSPI_TransactionA SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK
 Cspiffs_config
 Cspiffs_DIR
 Cspiffs_dirent
 Cspiffs_stat
 Cspiffs_t
 CSPIFFSNVS_Data_SPIFFSNVS data object
 CSPIFFSNVS_Lock_SPIFFSNVS Lock
 CSPIMSP432E4DMA_HWAttrsSPIMSP432E4DMA Hardware attributes
 CSPIMSP432E4DMA_Object
 CStructRingBuf_Object
 CTimer_Config_Timer Global configuration
 CTimer_FxnTableThe definition of a timer function table that contains the required set of functions to control a specific timer driver implementation
 CTimer_ParamsTimer Parameters
 CTimerMSP432E4_HWAttrsTimerMSP432E4 Hardware Attributes
 CTimerMSP432E4_ObjectTimerMSP432E4_Object
 CUART2_Config_UART2 Global configuration
 CUART2_FxnTableThe definition of a UART2 function table that contains the required set of functions to control a specific UART2 driver implementation
 CUART2_ParamsUART2 Parameters
 CUART2MSP432E4_HWAttrsUART2MSP432E4 Hardware attributes
 CUART2MSP432E4_ObjectUART2MSP432E4 Object
 CUART_Config_UART Global configuration
 CUART_FxnTableThe definition of a UART function table that contains the required set of functions to control a specific UART driver implementation
 CUART_ParamsUART Parameters
 CUARTMSP432E4_FxnSetComplement set of read functions to be used by the UART ISR and UARTMSP432E4_read(). Internal use only
 CUARTMSP432E4_HWAttrsUARTMSP432E4 Hardware attributes
 CUARTMSP432E4_ObjectUARTMSP432E4 Object
 CUDMAMSP432E4_ConfigUDMAMSP432E4 Global configuration
 CUDMAMSP432E4_HWAttrsUDMAMSP432E4 Hardware attributes
 CUDMAMSP432E4_ObjectUDMAMSP432E4 object
 CWatchdog_Config_Watchdog Global configuration
 CWatchdog_FxnTableThe definition of a Watchdog function table that contains the required set of functions to control a specific Watchdog driver implementation
 CWatchdog_ParamsWatchdog Parameters
 CWatchdogMSP432E4_HWAttrsWatchdog hardware attributes for MSP432E4
 CWatchdogMSP432E4_ObjectWatchdog Object for MSP432E4
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale