#include <usbhostpriv.h>
§ ui32Address
uint32_t tUSBHostDevice::ui32Address |
§ ui32Interface
uint32_t tUSBHostDevice::ui32Interface |
§ bLowSpeed
bool tUSBHostDevice::bLowSpeed |
§ ui32Speed
uint32_t tUSBHostDevice::ui32Speed |
§ bConfigRead
bool tUSBHostDevice::bConfigRead |
§ ui8Hub
uint8_t tUSBHostDevice::ui8Hub |
§ ui8HubPort
uint8_t tUSBHostDevice::ui8HubPort |
§ sDeviceDescriptor
tDeviceDescriptor tUSBHostDevice::sDeviceDescriptor |
§ psConfigDescriptor
tConfigDescriptor* tUSBHostDevice::psConfigDescriptor |
§ ui32ConfigDescriptorSize
uint32_t tUSBHostDevice::ui32ConfigDescriptorSize |
§ ui32Flags
uint32_t tUSBHostDevice::ui32Flags |
The documentation for this struct was generated from the following file: