#include <usbdmsc.h>
§ ui32USBBase
uint32_t tMSCInstance::ui32USBBase |
§ sDevInfo
§ ui8ErrorCode
uint8_t tMSCInstance::ui8ErrorCode |
§ ui8SenseKey
uint8_t tMSCInstance::ui8SenseKey |
§ ui16AddSenseCode
uint16_t tMSCInstance::ui16AddSenseCode |
§ pvMedia
void* tMSCInstance::pvMedia |
§ bConnected
volatile bool tMSCInstance::bConnected |
§ ui32Flags
uint32_t tMSCInstance::ui32Flags |
§ iMediaStatus
§ pui32Buffer
uint32_t tMSCInstance::pui32Buffer[0x1000 >>2] |
§ ui32BytesToTransfer
uint32_t tMSCInstance::ui32BytesToTransfer |
§ ui32CurrentLBA
uint32_t tMSCInstance::ui32CurrentLBA |
§ ui8INEndpoint
uint8_t tMSCInstance::ui8INEndpoint |
§ ui8INDMA
uint8_t tMSCInstance::ui8INDMA |
§ ui8OUTEndpoint
uint8_t tMSCInstance::ui8OUTEndpoint |
§ ui8OUTDMA
uint8_t tMSCInstance::ui8OUTDMA |
§ ui8Interface
uint8_t tMSCInstance::ui8Interface |
§ ui8SCSIState
uint8_t tMSCInstance::ui8SCSIState |
§ psDMAInstance
The documentation for this struct was generated from the following file: